Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs IO, IO, it's off to work we go! [micro:bit].
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 20 Sep 2016 11:04 AM Date Created
  • Views 808 views
  • Likes 6 likes
  • Comments 1 comment
  • micro:bit
  • big ideas
Related
Recommended

IO, IO, it's off to work we go! [micro:bit].

jc2048
jc2048
20 Sep 2016

I am now the proud owner of a micro:bit. Yippee! I'm a bit old to be running around shouting "Yippee!" really, but why shouldn't us oldies have a bit of fun too.

 

Over on this thread,

 

https://www.element14.com/community/community/stem-academy/microbit/blog/2016/06/08/10-bbc-microbit-projects-in-10-days-day-three-making-music

 

jlucas suggested connecting an 8 ohm speaker to one of the IO pins. Instinctively, I flinched: 3.3V into 8 ohms would be a current of 413mA [if the IO pin could hold up under the strain, which it wouldn't - "Cap'n, the IO pins, they cannae take the strain"]. That would far exceed the absolute

maximum for the pin. Now that I have a micro:bit of my own I can see for myself, and the good news is that you can safely connect an 8 ohm loudspeaker. The pins have a 220 ohm resistor in series with them.

 

Here's a picture of my micro:bit driving a small speaker.

 

image

 

And here is the waveform across the speaker

 

image

 

We'd expect the amplitude to be 116mV. 8/(220+8) x 3.3V. It's slightly less than that because the IO driver (inside the chip) isn't a perfect switch and has some resistance too which adds to the 220 outside the chip.

 

The current is a modest 15mA (calculation: I didn't measure it) and the dissipation in the speaker would be a mere 1.8mW.

 

There's also a weak pull-up resistor at the edge connector, but that's difficult to measure accurately in circuit.

 

Sorry about all this - I'm doing electronics when I should be learning to code (old habits die hard). Now where's that Python book got to...

  • Sign in to reply
Parents
  • jw0752
    jw0752 over 10 years ago

    Great writing style and I am enjoying your exploration of the Microbit

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago

    Great writing style and I am enjoying your exploration of the Microbit

    John