Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Isolated DC/DC Converter TIDA-00349
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: martinvalencia
  • Date Created: 13 Aug 2015 1:51 AM Date Created
  • Views 967 views
  • Likes 4 likes
  • Comments 2 comments
  • texas-instruments
  • efficient
  • high
  • tida-00349
  • dc-to-dc
  • analog
  • isolate
Related
Recommended

Isolated DC/DC Converter TIDA-00349

martinvalencia
martinvalencia
13 Aug 2015

Introduction

My main intention today is the presentation of this excellent product launched by Texas Instruments the world, I'm excited to show the performance of TIDA-00349.

To analyze performance, I'm  using a FLUKE oscilloscope and a thermometer IR, so I can sure that the data measured is according datasheet found correct and according to specified by the manufacturer.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Description

The TIDA-00349 TI Design is an isolated DC/DC converter turn-key solution, delivering exceptionally high efficiencies up to 85% from ultra-low power up to 60mW.

Open-loop control removes the need for opto-couplers, while a primary side half-bridge topology operating at 60kHz and secondary side Schottky rectification provides low switching losses, enabling highly efficient power conversion.

image

image

image

Features:

Highly Efficient Design

– Up to 86% With 5-V Input

– Up to 82% With 3.3-V Input

 

Table N.1image

Featured Applications

• Factory Automation and Process Control

• Loop Powered 4- to 20-mA Transmitters and Other

Sensors and Field Transmitters

• Building Automation

• Portable Instrumentation

 

Schematic circuit

 

image

Bill of Materials

image

Performance test


You can see in Figure 1 and 2, the physical connection of TIDA-00349, I used the power of a TI Launchpad, on the grounds of having a highly regulated power.

image

Figure N. 1

image

Figure N. 2



Perform an oscilloscope view the output of TIDA-00349, to see if there are some kind of rizado or noise in the output by switching but the output is very stable and is within the parameters set out in Table N. 1


image

Measure to Input 3.3v

 

image

Measure to Input 5.0 v

image

The measurements were made with a 450 ohm resistive load.

 

Temperature tests (FLUKE IR THERMOMETER)


About an hour of work, TIDA temperature measurement is performed, noting that this hardly dissipated power and heat.

image

 

The working temperature always remained around 25 ° C

image

Switching Frequency


Switching frequency according to manufacturer sheet is 60KHz, and cycled dutty 50%, this is important for the maximum transfer of power in a flyback configuration occurs when the pulse width is 50%

image

 

image

 

Reference TI Design

 

Uniquely Efficient Isolated DC/DC Converter for Ultra-Low Power and Low Power Apps Reference Design - TIDA-00349 - TI To…

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 11 years ago +1
    Hi Martin, I enjoyed your presentation on this DC/DC converter. John
  • martinvalencia
    martinvalencia over 11 years ago in reply to jw0752 +1
    Thank you very much for taking your time and read the presentation, I hope to have more things to show in the future. Good day, Greetings.
Parents
  • jw0752
    jw0752 over 11 years ago

    Hi Martin,

    I enjoyed your presentation on this DC/DC converter.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 11 years ago in reply to jw0752

    Thank you very much for taking your time and read the presentation, I hope to have more things to show in the future.

    Good day, Greetings.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • martinvalencia
    martinvalencia over 11 years ago in reply to jw0752

    Thank you very much for taking your time and read the presentation, I hope to have more things to show in the future.

    Good day, Greetings.