Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Issue using Energia for the CC3200 LaunchXL
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kweber250
  • Date Created: 26 Dec 2018 8:31 PM Date Created
  • Views 1752 views
  • Likes 2 likes
  • Comments 7 comments
Related
Recommended

Issue using Energia for the CC3200 LaunchXL

kweber250
kweber250
26 Dec 2018

Hello All,

I'm trying to compile this code in Energia and I receive the error below, I receive a similar error regardless of the code, if I need to download a library to write in c, which library and where do I download it.

Thank you!

////////////////////////////////////////CODE/////////////////////////////////////////

#include <msp430.h>

 

volatile unsigned int i;

 

void main(void) {

 

WDTCTL = WDTPW | WDTHOLD;

P1DIR |= (1<<0);

P1OUT &= ~(1<<0);

 

while(1) {

P1OUT ^= (1<<0);

i = 65535;// SW Delay

while(i --!= 0);

}

//////////////////////////////////////////////////////////////////////////////////////

////////////////////////////////ERROR/////////////////////////////////////////

Build options changed, rebuilding all

test.c:1:20: error: msp430.h: No such file or directory

 

 

#include <msp430.h>

 

 

                    ^

 

 

compilation terminated.

 

 

exit status 1

msp430.h: No such file or directory

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago +3
    This does not seem to be energia code. Energia code looks and feels like arduino sketches. msp430.h is not for a cc3200 controller. You seem to try and use msp430 registers on the cc3200. These two controller…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to kweber250 +3
    You’d use an IDE such as TI’s code composer studio for non-energia projects. Energia, like the Arduino IDE, expects you to follow the sketch way of working.
  • jomoenginer
    jomoenginer over 7 years ago +2
    This might be more inline with what you are looking for. https://energia.nu/pinmaps/cc3200-launchxl/ http://energia.nu/guide/boards/ https://forum.43oh.com/forum/125-energia-tivaccc3xxx/ Is there a particular…
Parents
  • phoenixcomm
    phoenixcomm over 7 years ago

    I agree with James. the MSP4xx and the CC32xx are very different processors and ARE NOT compatible/subset/superset/etc.

    • The MSP4xx are 16-bit low power devices, with a von Neumann architecture, with a single address space for instructions and data.
    • The CC3200 are ARMRegistered CortexRegistered -M4 Core, with an Armv7E-Harvard architecture, and The Wi-Fi Internet-on-a-chip, includes embedded TCP/IP and TLS/SSL stacks, HTTP server, and multiple Internet protocols.

    You can use CCSx on both devices but remember you must use the correct libraries.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 7 years ago

    I agree with James. the MSP4xx and the CC32xx are very different processors and ARE NOT compatible/subset/superset/etc.

    • The MSP4xx are 16-bit low power devices, with a von Neumann architecture, with a single address space for instructions and data.
    • The CC3200 are ARMRegistered CortexRegistered -M4 Core, with an Armv7E-Harvard architecture, and The Wi-Fi Internet-on-a-chip, includes embedded TCP/IP and TLS/SSL stacks, HTTP server, and multiple Internet protocols.

    You can use CCSx on both devices but remember you must use the correct libraries.