Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs LM386 Audio Amplifier
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mrchunckuee
  • Date Created: 13 Feb 2016 4:14 AM Date Created
  • Views 3667 views
  • Likes 4 likes
  • Comments 11 comments
  • audio amplifier
  • lm386
  • lm386 audio amplifier
Related
Recommended

LM386 Audio Amplifier

mrchunckuee
mrchunckuee
13 Feb 2016

Greetings! My first post on Element, is a small audio amplifier using LM386 integrated.

 

For the design has been based on the one proposed in the datasheet (Gain = 200), some components and filters are added to the feed inlet (VALIM = 12V), the circuit used is this:

AMPLIFICADOR%2BDE%2BAUDIO%2BCON%2BLM386.png

Here more photos of the PCB:

buttom pcb

3%2BAMPLIFICADOR%2BDE%2BAUDIO%2BCON%2BLM386.jpg

The final PCB with all componences looks like this:

4%2BAMPLIFICADOR%2BDE%2BAUDIO%2BCON%2BLM386.jpg

Here one video of the circuit in action (video in spanish):

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

See more projects or info in my blog (in spanish)

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 10 years ago +2
    Hi Pedro, This was a very nice project. It is really good that you are open to learning. I have learned a lot of new things by listening to michaelkellett as he always has good solid advice. John
  • jc2048
    jc2048 over 10 years ago in reply to DAB +2
    Page 4 of the datasheet has a graph of Voltage Gain vs Frequency. That shows about 40kHz for the IC itself with a gain of 200 (C pin1 to pin8 = 10uF). Out of curiousity, I tried simulating the input network…
  • nick123
    nick123 over 10 years ago +1
    Welcome, cool amp, see if you can get a guitar amplified through there
  • jc2048
    jc2048 over 10 years ago in reply to DAB

    Page 4 of the datasheet has a graph of Voltage Gain vs Frequency. That shows about 40kHz for the IC itself with a gain of 200 (C pin1 to pin8 = 10uF).

     

    Out of curiousity, I tried simulating the input network (from jack socket to pin3 of the IC) and here's the response with the pot set to 100% and the input resistance of the amplifier as 50k (the typical value from the datasheet).

     

     

    image

     

    Even if the amplifier gain was less than 200 and the bandwidth of the amplifier was therefore higher, the high end -3dB point for the whole circuit would still be around 30kHz because of the action of C6 at the input. I don't know why C6 is there - possibly it is intended to filter out rf from medium wave broadcasts that might be picked up on the input leads and then get rectified by the semiconductors in the IC. Alternatively, it might be intended to reduce the possibility of oscillation at higher frequencies (even with the natural roll-off of the amplifier, the IC still has some gain at 1MHz where the possibility of capacitive coupling from the output to the input increases).

     

    For the output network, I tried simulating with a 8ohm resistor for the loudspeaker, but you should be a bit (very?) skeptical because I've just assumed the IC output is a perfect voltage source which it obviously isn't and an 8R resistor isn't a very good model for a loudspeaker. It does, however, give some idea as to what is going on and how it's going to behave.

     

     

    image

     

    Not surprisingly, the low end is dominated by the output capacitor and looks like it might be around 100Hz.

     

    So, overall we could say something like 100Hz-30kHz. That's fine for a small speaker and the kind of applications where you'd use the circuit. [It's only a simple amplifier and the distortion is more than 1% at higher frequencies, so we're not really in the realms of hi-fi here.]

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mrchunckuee
    mrchunckuee over 10 years ago in reply to nick123

    Yes nick123, I've used couché paper and heat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mrchunckuee
    mrchunckuee over 10 years ago in reply to DAB

    DAB, I don't think that, but according to the datasheet is BW = 300 kHz but with VS = 6V and pin 1 and 8 open. In the circuit i used VS>11V also c16 and c17 , I suppose that this should change some things, but not be the exact data.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mrchunckuee
    mrchunckuee over 10 years ago in reply to jw0752

    Of course jw0752, it is always good to hear recommendations from people with more experience, so i learn more

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nick123
    nick123 over 10 years ago

    Did you hand etch that board?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>