Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Makevember : Wire Frame Christmas Trees
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 11 Nov 2019 12:01 PM Date Created
  • Views 3260 views
  • Likes 15 likes
  • Comments 19 comments
  • makevember
  • wire frame trees
Related
Recommended

Makevember : Wire Frame Christmas Trees

dubbie
dubbie
11 Nov 2019

For a contribution to the Makevember topic I decided to make some wire frame Christmas tree decorations. I wanted to make them to look good and to have some LEDs on them. I didn't quite (yet) manage this although I have made something, see below.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I aim to try and improve more on the wire frame trees and then I will have to work out some way of attaching LEDs and getting them to light up nicely.

 

Dubbie

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +7
    Hi Dubbie, I got curious and decided to run my own experiment with some 3.16 mm ( 1/8 inch ) aluminum ground wire that I had in the shop. Here is the initial shape of the wire: I put the wire in the vise…
  • fmilburn
    fmilburn over 6 years ago in reply to dubbie +5
    I have not tried it but have seen several times where people used a drill to straighten copper wire: https://www.youtube.com/watch?v=meZRMNF-6tQ. A good idea to have eye protection and gloves while doing…
  • jw0752
    jw0752 over 6 years ago in reply to fmilburn +5
    I do a lot on things with wire as a structural material. I usually put one end of the wire in a secured vise and the other end in a drill chuck. I pull the wire as tight as I can and give it about one…
Parents
  • jw0752
    jw0752 over 6 years ago

    Hi Dubbie,

     

    I got curious and decided to run my own experiment with some 3.16 mm ( 1/8 inch ) aluminum ground wire that I had in the shop. Here is the initial shape of the wire:

     

    image

     

    I put the wire in the vise and drill and pulled as tight as I could and it looked like this. At this stage there would still be quite a bit of bend in the wire if I hadn't twisted it.

     

    image

     

    I began to twist the wire with the drill and I watched the tight bend near the center of the wire as I hoped it would totally disappear.

     

    image

     

    As you can see things did get better but the tight bend did not disappear completely. I put a lot more twists per meter of length into this wire than I usually have to. I am not sure if it was the aluminum or just the tightness of the bend I was hoping to eliminate. At some point it is prudent to stop twisting as twisting puts the same weakness into the wire that bending it back and forth would. The twisting is a compromise whereby we sacrifice some strength for the straightness. In most cases the loss of strength is inconsequential compared to the improved appearance of the finished project. If you continue the twisting, the wire will eventually twist off at its weakest point which is usually right at the point it is held in the vice or the point where it enters the drill chuck.

     

    Here is the finished wire:

     

    image

     

    I usually work with 10, 12, and 14 Gauge copper and I straighten 3 to 4 meter lengths. Usually there are no tight bends just a curve left from the coiled condition of the original packaging of the wire. In these circumstances the wire straightens almost perfectly with only minimal twisting involved.

     

    This is an aside on a non-related subject. In astrophysics the Universe has shown itself to be remarkably FLAT. This means that the geometry of Euclid applies. While I am not an expert I could sense in my readings that it was a bit if a surprise to those that are experts that this condition of FLATNESS is so precise. After working with bent wire I always wondered if there might be some analog in the early Universe to the twisting of the wire such as spinning that might have contributed to the Flatness that we observe today.

     

    John

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to jw0752

    John,

     

    I'm not sure what the problem is but I can only see the first few lines of your Blog and no pictures.  Is this something wrong with my version of the element14 web site? I would really like to see the picture.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago in reply to jw0752

    John,

     

    I'm not sure what the problem is but I can only see the first few lines of your Blog and no pictures.  Is this something wrong with my version of the element14 web site? I would really like to see the picture.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 6 years ago in reply to dubbie

    Hi Dubbie,

     

    Sorry I do not see a problem on this end. I have looked at it with two different computers and my android phone. I wonder if anyone else is having problems seeing it? If they are I hope they mention it and I will repost the pictures and a new comment on this string. I hope the problem gets resolved.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to dubbie

    I can see the pictures on a Windows 10 machine and an iPad

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to jw0752

    shabaz reported the same thing about a comment I posted a few days ago. I pasted 2 screen captures.

    I can see them on different computers in different browsers. logged in or out. cache refreshed.

    Shabaz does not see them...

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps

    Currently I'm seeing no photos and one video in the main blog, and there's a comment from Dubbie where I can see 4 photos.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to shabaz

    Hi Shabaz,

     

    I believe there is only one video in Dubbie's main blog and the only comment with 4 pictures is the one that I posted that Dubbie can't see. What you describe, at least from my perspective, is a correct characterization at this point.

     

    John