Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs MIT App Inventor creating Android App to control Arduino via Bluetooth - Corrected 18 January 2015
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: neilk
  • Date Created: 14 Jul 2014 6:14 PM Date Created
  • Views 9283 views
  • Likes 3 likes
  • Comments 29 comments
  • android
  • bluetooth
  • hc06
  • mit
  • appinventor
  • led
  • arduino
Related
Recommended

MIT App Inventor creating Android App to control Arduino via Bluetooth - Corrected 18 January 2015

neilk
neilk
14 Jul 2014

App Inventor, Bluetooth and Arduino - Part 1

 

MISSING IMAGES RESTORED 5 FEBRUARY 2016

 

I was enthused by Pieter Bok’s post  involving an iPhone App connecting to an Arduino via WiFi:

 

http://www.element14.com/community/videos/12327/l/arduino-based-automatic-irrigation-system-for-pot-plants

 

I don’t have an iPhone, or a WiFi shield, but Bluetooth was mentioned in the thread,  so I Googled around for Android, Arduino and Bluetooth, finding several links which made use of an amazing, FREE resource from MIT called App Inventor, for developing Android Apps:

 

http://appinventor.mit.edu/explore

 

This link is to version 2 of App inventor. Several of the Arduino related links, were for App Inventor version 1, which is still available, although not for long, so you are advised not to start using it.

 

App Inventor 2 is entirely web-based, and includes the ability to connect to your target Android device via Wifi and run an emulation of your App in real time - the display on your device changes as you change the design in App Inventor! If you don’t even have an Android device, you can run an emulator on your PC and App Inventor will connect to it.

 

App Inventor 2 has two screens - Design and Blocks. In Design, you drag and drop components such as buttons, labels, text boxes, sliders, etc, on to a representation of your Android device screen and arrange them as you want them to appear.

 

In the Blocks screen, you drag and drop representations of code segments which relate the display components together and ultimately generate your app. Once you get into it, it’s actually very straightforward.

 

Initially, I got a little bogged down because I tried to follow a tutorial based on version 1 of App Inventor and I couldn’t get it to work. I thought it was problem with the code, but actually it was me! Because I was new to Bluetooth, I hadn’t realised that I had to pair the devices first! I’m learning fast!

 

Using this video tutorial  for version 2, to send data to the Arduino, I launched myself:

 

https://www.youtube.com/watch?v=6o_QVlltNgM

 

This Tutorial shows how to build an App which connects to an Arduino, via Bluetooth - I used a JY-MCU HC06 board. The Arduino sketch to receive commands from the App to turn an LED on and off is also supplied.

 

There seems to be some confusion about whether the JY-MCU HC06 Bluetooth board can accept a 5v Tx signal from the Arduino into its Rx pin. My JY-MCU board is clearly marked as expecting a 3.3v signal level, so I used a couple of resistors to make a simple voltage divider.

 

It was also said to be important that you disconnect the Bluetooth board from Arduino pins 0 and 1 when uploading a sketch. However, I forgot once and it didn’t  seem to make any difference!

 

You can have the IDE Serial Monitor open whilst the Bluetooth is working and see exactly what’s happening. In fact, you can test the sketch without the Bluetooth connected, by typing in the relevant characters on the keyboard and sending via the Serial Monitor.

 

In the Design screen, below, you can see the depiction of an Android device screen:

 

image

 

On the left of the screen is a list of the components which can be dragged and dropped onto the Android screen.

To the immediate right  of the Android screen is a list of the current screen components: a ListPicker, two Buttons in a Horizontal Arrangement and a “hidden” Label, hidden because it is initially blank. There is also a non-visible bluetooth client at the bottom of the screen.

 

To the far right of the Android screen are the properties of the currently selected component - in this case the Label, Label1 is selected.

 

If we click on the Blocks Tab and then click on the ListPicker1 component on the left hand side of the screen. A scrollable list of code blocks relevant to the ListPicker1 appears. Click  on “When ListPicker1 BeforePicking” and it will be placed onto the Blocks screen area.

 

 

image



We can now select further sub-Blocks to create the first full code Block, below..

 

This allows List Picker1 to display the available (already paired) Bluetooth devices: - This next code block has been corrected 18 January 2015


image

 

The next Block allows ListPicker1 to select and connect to the desired Bluetooth device and to set the “hidden” Label, Label1 to read “CONNECTED”:

 

image

 

I’ve then set the default Text of Label1 to be “NOT CONNECTED” and the colour of Label1 to be Red in the Design Screen; clearly, Label1 is now no longer “hidden”.

 

I’ve also added a further component into the code Block, to set the Text colour of Label1 to be Green when the Bluetooth client is connected.

 

The next 2 Blocks send the text string “on” when Button1 is pressed and the text string “off” when Button2 is pressed.



image
Finally, I’ve  added a third Button in the Design screen with a Text value of “DISCONNECT”and a fifth Block of code which disconnects the Bluetooth client, sets Label1 text colour to Red and Label1 text to read “DISCONNECTED”

 

 

 


image

The Arduino sketch is  straightforward:

 

int ledPin = 13;

String readString;

 

void setup()

{

  Serial.begin(9600);

  pinMode(ledPin, OUTPUT);

}

void loop()

{

  while ( Serial.available() )

{    // While there is data in the buffer

    delay( 3 ); 

    char c = Serial.read();

    readString += c;         // build the string - “on” or “off”

}

  if ( readString.length() >0 )

   {

    Serial.println( readString );

    if ( readString == "on" )

     {

      digitalWrite( ledPin, HIGH) ;

      }

    if ( readString == "off" )

     {

      digitalWrite( ledPin, LOW );

      }

    readString="";

   }

}

 

 

 

Obviously, the sketch could be simplified if the App merely sent, say ,“1” for ON and “0” for off, instead of “on” and “off”.

 

 



Attachments:
Led_Control.zip
  • Sign in to reply

Top Comments

  • dougw
    dougw over 12 years ago +1
    Thanks for posting this tutorial Neil. App Inventor is what I used to develop the Bluetooth android app that controls the Henrietta Project. I can vouch for the ease of use and ease of learning this development…
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    A really nice initiative Neil! Congrats! I really appreciate the youtube tutorial it's very informative. The reason why I chose a Etnernet shield + nano router (equals "WIFI" shield ;-) ) is that I can…
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    G'day, Nice project, and it will be my first app. Any chance of the source aia file. Grant
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi Neil, thanks for sharing your nice tutorial. I tried to find answer to my question, but no luck. I wonder, is it possible to use MIT App Inventor 2 to create an application to control multiple Arduinos?

    I mean, you have e.g. three Arduino boards each with HC06 module. Is it possible to make an app that allow you to connect to these clients via BT and display ON/OFF buttons for actually connected clients?

    Thanks.

     

    Boris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 11 years ago in reply to e14 Contributor

    Grant - lost in translation? The link is definitely to my .aia file, and definitely from Version 2; I never used Version 1.

     

    Did it work??

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to neilk

    Neil,

    I thought that when the source file is in a dir with a ".ana"  it was for Version 1, but now I know better.

    Tks again

    Grant

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 11 years ago in reply to e14 Contributor

    Thanks, Grant

     

    You can download the .aia file from this link:

    https://drive.google.com/file/d/0B5X3MgwHbj3STmlacVpNVHBkeVk/view?usp=sharing

     

    Best wishes

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    G'day,

    Nice project, and it will be my first app. Any chance of the source aia file.

    Grant

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>