Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Modifying my Motor Winding Simulator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: three-phase
  • Date Created: 23 Oct 2019 7:07 PM Date Created
  • Views 1753 views
  • Likes 7 likes
  • Comments 2 comments
  • winding simulator
  • guard terminal
  • insulation test
Related
Recommended

Modifying my Motor Winding Simulator

three-phase
three-phase
23 Oct 2019

Those of you that have followed my insulation tester series may have noticed that I have a little winding simulator to carry out winding resistance and insulation tests on, to save going out and finding a motor. The simulator also produces consistent results that is ideal for insulation tester comparisons, instead of a motor whose insulation system can vary with moisture and humidity.

 

image

 

The winding simulator is capacitive in nature, instead of inductive, to create the charging effect of a polarisation index test. However, in its original form, it did not simulate a leakage path between windings, as would be found on a real motor.

 

In my reviews of insulation testers, I have now come across a small 1kV insulation tester that has a guard terminal fitted, so to demonstrate its use, I have modified the winding simulator to now have some optional leakage between the windings.

 

image

 

image

The original circuit has now had the two leakage resistors installed, that are circled in the schematic above. Inside the winding simulator, I have soldered one end of the resistors via a wire onto the U1, V1 and W1 terminations and crimped the other ends to connect to the studs in the end cap. I have sleeved the two resistors to protect against shorts as seen win the picture below.

 

image

 

I have chosen to add these resistors via three studs on the end of the case, so I can select wether or not to have the leakage in circuit.

 

image

 

Whilst the simulator is in use, these studs would have 500V on them, so I have made up some little threaded caps to go over them when they are not in use.

 

The studs, have been spaced so I can use the shorting links from the motor connector block to add the leakage into the circuit. The two pictures show a couple of the options I now have for adding leakage to the simulator.

 

imageimage

 

image

 

The three plots below summarise the tests carried out for different configurations. The blue line represents the PI test with the other two windings left floating and no leakage installed and naturally gives the higher readings.

 

image

The green line represents the PI test when the leakage links have been fitted to the simulator. The final orange line represents the PI test with the links fitted and the other two windings connected to earth. This would be the usual insulation tests for a large motor with access to all the winding connections. This is depicted below by the yellow insulated crocodile clip links shorting out two of the windings to earth.

 

image

 

The table below shows the results for each phase with the leakage applied between U and V Phase. Each phase was then tested at 500V whilst the other two phases were floating, then earthed and then connected to the guar terminal of the insulation tester.

 

image

The two interesting results to me are the 1 minute insulation values and the DAR values. The two plots below show these test results for easier comparison to one another.

 

image

 

With leakage only applied between U and V Phases, the tests on W Phase show the same result irrespective of the test configuration. For U and V Phases, the test configuration altered the value of the test result. With the untested phases earthed, both U and V Phases showed lower insulation resistance and DAR values. Removing the earth and repeating the test with the untested phases floating, produced a slightly higher insulation resistance, but some leakage would still be going through the leads and simulator.

 

Reconfiguring the test with the untested phases wired to the guard terminal on the insulation tester, showed the highest insulation and DAR values. The guard terminal is basically detecting any leakage into the untested phases and removing it from the result, leaving only the leakage from the tested phase to earth.

 

image

 

I am happy with the modification to the winding simulator and it now gives me more additional functionality and improves the test regime for those insulation testers that are fitted with a guard terminal. This will also act as a forerunner for a larger version of the winding simulator for higher test voltages that I would like to build.

 

I will demonstrate more in depth use of the guard terminal, and some of its uses, in the review of that specific insulation tester.

  • Sign in to reply

Top Comments

  • genebren
    genebren over 6 years ago +3
    Donald, A great write-up and a great little tool. Simulators are always a good way to test or evaluate when you do not have easy access to the real thing. At one point in my career, I developed relatively…
  • three-phase
    three-phase over 6 years ago in reply to genebren +1
    Many thanks Gene. Sounds like an impressive set up you created, I think I have a little way to go before I get anywhere near that. Yes, I do find simulators very handy for testing out concepts and general…
Parents
  • genebren
    genebren over 6 years ago

    Donald,

     

    A great write-up and a great little tool.  Simulators are always a good way to test or evaluate when you do not have easy access to the real thing.  At one point in my career, I developed relatively complex simulators to assist in testing/evaluating avionics equipment in the lab.  We would read inputs from a cockpit mock-up, and then simulate the aircraft in flight, along with other instrumentation (gyros, air data computers, etc.) and feed all of this data to the device under test.  We would then sample all of the outputs from the device under test and feed those back into the simulations.  This allowed us to fully test/prove all of our software in the lab, before we moved onto the real airframe.  This saved us from the cost of air time, and allow us to insert faults and out of bounds data into the device to better test our code.

     

    P.S.  I really like the screwdriver in your second image.  I have one on my desk/workbench and it is one my favorite tools.

     

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 6 years ago

    Donald,

     

    A great write-up and a great little tool.  Simulators are always a good way to test or evaluate when you do not have easy access to the real thing.  At one point in my career, I developed relatively complex simulators to assist in testing/evaluating avionics equipment in the lab.  We would read inputs from a cockpit mock-up, and then simulate the aircraft in flight, along with other instrumentation (gyros, air data computers, etc.) and feed all of this data to the device under test.  We would then sample all of the outputs from the device under test and feed those back into the simulations.  This allowed us to fully test/prove all of our software in the lab, before we moved onto the real airframe.  This saved us from the cost of air time, and allow us to insert faults and out of bounds data into the device to better test our code.

     

    P.S.  I really like the screwdriver in your second image.  I have one on my desk/workbench and it is one my favorite tools.

     

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • three-phase
    three-phase over 6 years ago in reply to genebren

    Many thanks Gene. Sounds like an impressive set up you created, I think I have a little way to go before I get anywhere near that. Yes, I do find simulators very handy for testing out concepts and general functionality of devices. Most of the ones I have previously built in my professional capacity, were to enable faults to be identified and function checks carried out after repairs.

     

    The Nanch screwdriver set is very nice indeed. I find it a very good quality driver and bits. The extension out of the driver is very useful and the slightly longer bits than the usual ones in precision screwdriver sets are very handy. As with all kits though, I always find some bits missing that I would like.

     

    imageimage

     

    Nanch screwdriver on Amazon

     

    I plan to do a review of all of my tools in my tear down kit, when I have got my current set of insulation testers in for review out of the way.

     

    Kind regards.