Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Molex Antenna Adventures starring a RPi4
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 18 Nov 2020 2:41 AM Date Created
  • Views 5284 views
  • Likes 11 likes
  • Comments 6 comments
  • wifi
  • molex
  • molex_webinar
  • raspberrypi4
  • umc
  • antenna
Related
Recommended

Molex Antenna Adventures starring a RPi4

wolfgangfriedrich
wolfgangfriedrich
18 Nov 2020

Some time ago, I received a Molex Antenna Kit consisting of a boatload of different antenna types. A big thanks to E14, Avnet and Molex.

 

These are the contents:

 

{gallery}Molex Antenna Kit

image

Antenna Kit: Molex Sample Kit

image

Antenna Kit: Cellular Antennas

image

Antenna Kit: Combo Antennas

image

Antenna Kit: GNSS Antennas

image

Antenna Kit: ISM Antennas

image

Antenna Kit: NFC Antennas

image

Antenna Kit: UWB Antennas

image

Antenna Kit: BT/WiFi Antennas

image

Antenna Kit: Selection of WiFi Antennas

 

 

 

As a leftover from a previous roadtest, I am also the proud owner of a PaspberryPi4 B. This mighty little computer did have bad WiFI performance in the basement, with the router being one floor up and across the house.

= imageimage

 

A close look at the board shows a very interesting layout for the PCB antenna. I don't even want to start thinking about, what is going on there in the RF domain.

image

 

The part that interested me most, was the empty footprint at the feed trace and the single contact, suggesting a mounting option for an UMC connector. The antenna Kit did contain a nice selection of dual band 2.4/5 GHz WiFi/Bluetooth antennas with UMC connections as well. One Digikey order later, a fitting part ended up on my desk. In the spirit of the giveaway, it is a Molex UMC receptable 50 Ohm SMD, part number 073412-0110.

image

A banana for scale would not work very well, so I used my EEVblog measuring stick.

The next steps are: cut trace, add wire bridge, scrape scrape scrape, solder connector in place, plug in antenna, done.

image

image

image

One of the camera connector slots in the housing is a perfect feed-through to get the antenna out. And there is 'plenty' of room to stick it somewhere to secure it.

image

image

A quick test, did reveal an improvement in WiFi signal strength.

= image.image

I am sure, there is some programs around to give more detailed WiFi signal strength information, but I am happy as it is. So no 'apt get ..........' session tonight, that would take longer than the hardware upgrade.

 

The End.

 

PS: I probably should scratch the FCC/CE mark off the board now...

  • Sign in to reply

Top Comments

  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to wolfgangfriedrich +3
    jkutzsch : I have some more results: as expected, unplugging the new antenna really kills the Wifi range. It detects the network up to 2 meters away from the router in line of sight or through a thin North…
  • colporteur
    colporteur over 5 years ago +3
    I sit here on Friday night with two Coors Light beers in my gullet and think WOW! I doff my hat for your initiative. I have no fortitude for putting a Pi at risk by hacking to the level you have ventured…
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago +2
    It looks like the RPi Foundation went with my idea for their compute module: Must be a fancy RF switch. From: https://www.raspberrypi.org/products/compute-module-4-antenna-kit/?resellerType=home
Parents
  • jkutzsch
    jkutzsch over 5 years ago

    Interesting wolfgangfriedrich, any idea if you were to remove the external wire now how much different your reception would be from the original setup?  As in did the previous "builtin" really provide much?  Makes me wonder about some type of on board connector that would allow you to use a generic antenna option so you could switch out from omni to directional.  Seems like some people just go to an external USB option to allow for antenna swapping but if the chipset is good enough on board this could be interesting.  Ty for sharing!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to jkutzsch

    Hello jkutzsch.

    It never occurred to me to test the RPI without antenna at all. I will do this and report back. I would imagine the feed trace + connector will not have a lot of gain. Using a generic connector like an edge-mount SMA looks possible, when you don't mind losing the mounting hole. The PCB antenna (and my setup probably too) is definitely very directional. Thanks,

    - W.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to jkutzsch

    Hello jkutzsch.

    It never occurred to me to test the RPI without antenna at all. I will do this and report back. I would imagine the feed trace + connector will not have a lot of gain. Using a generic connector like an edge-mount SMA looks possible, when you don't mind losing the mounting hole. The PCB antenna (and my setup probably too) is definitely very directional. Thanks,

    - W.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to wolfgangfriedrich

    jkutzsch:

    I have some more results: as expected, unplugging the new antenna really kills the Wifi range. It detects the network up to 2 meters away from the router in line of sight or through a thin North-american wall with the router right next to the wall. Everything further away ends up with a un-connected RPi.

     

    And I learnt another Linux command:

    sudo iwlist wlan0 scan

    outputs a lot of stats about the network including signal strength in dB.

    This can be useful to characterized WiFi coverage.

    The output is in the form of:

    Channel:157
    Frequency:5.785 GHz (Channel 157)
    Quality=45/70  Signal level=-65 dBm  
    Encryption key:on
    ESSID:"FibreOP444-5"
    Bit Rates:6 Mb/s; 9 Mb/s; 12 Mb/s; 18 Mb/s; 24 Mb/s
              36 Mb/s; 48 Mb/s; 54 Mb/s

     

    This is going to help for some future tests. Now let's build a turn table or source the lazy Susan from the kitchen cabinet.

     

    - W.

    • Cancel
    • Vote Up +3 Vote Down