Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs MSP432 with BOOSTXL-K350QVG-S1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jomoenginer
  • Date Created: 23 Feb 2017 7:11 AM Date Created
  • Views 1337 views
  • Likes 3 likes
  • Comments 4 comments
  • boostxl-k350qvg-s1
  • msp432
Related
Recommended

MSP432 with BOOSTXL-K350QVG-S1

jomoenginer
jomoenginer
23 Feb 2017

For my Safe Sound Hearing Guard System project I plan to use a  BOOSTXL-K350QVG-S1 with a TI MSP432 for the base unit The QVGA TFT will be used for user input to the system to set dB thresholds and view data collected from the noise sampling from the Personal Noise Sensor and Room Unit I did not find the  BOOSTXL-K350QVG-S1 example in MSPWare v3.x so I resorted back to a v2.x of MSPWare and Code Composer 6.x since the older MSPWare example fails the build process in CCS 7(At the time the video was made I did not try the MSP-EXP432P401RGrLibExample located in MSPWare v3.60.00.10

 

Hardware:

BOOSTXL-K350QVG-S1

MSP432P401R LaunchPad   (Black)

Software:

Code Composer Studio 6.1.1.00022

MSPWare - Version 2.40.00.37

BOOSTXL-K350QVG-S1_GrlibExample_MSP432P401R

 

The example I found for the MSP432 was in the MSPWare 2.40.00.37 but when compiled in Code Composer 7 it produces 100 errors. However, with CCS 6.1.1.00022 this compiled without issue. My plans are to implement this in to TI RTOS, so we'll see if the IDE rev is a factor at that time.

 

So from Code Composer Studio to get to the TI Resource Explorer go to View Resource Explorer(Examples Once this has been selected the TI Resource Explorer will appear in the IDE right window If MSPWare 6.1.1.00022 is not installed it can be searched and then imported on to the Desktop After this the individual devices such as MSP432 or  BOOSTXL-K350QVG-S1 GRLib Example can be searched for by adding BOOSTXL in the search field

 

image

 

Then click on “Step 1: Import the example project into CCS.

 

image

 

This will add the "BOOSTXL-K350QVG-S1_GrlibExample_MSP432P401R" example to the Project Explorer window.

image

 

After the example is loaded on the MSP432, this is what the demo looks like. (I did have some issues with the Touch Screen and the Calibration).

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 9 years ago

    You clicked on the right button in the video. The example behaved odd.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago

    You clicked on the right button in the video. The example behaved odd.