Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs My First Ever Crimping Experience
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 20 Nov 2020 2:54 PM Date Created
  • Views 6152 views
  • Likes 10 likes
  • Comments 34 comments
  • spade connections
  • crimping
Related
Recommended

My First Ever Crimping Experience

dubbie
dubbie
20 Nov 2020

For my Sand Based Cat Detector (Cat Detector Using Sand #2 : The Implementation ) I used a lead acid battery with spade connections. I have never properly used spade connections before (I usually use crocodile clips or solder directly) so I thought this would be a good time to start as I am working my way towards an outdoor mobile robot and robust and reliable connections are essential. Not really knowing much about making spade or crimping connections I decide that the best approach would be to buy some and just try it out. I have wanted to crimp for some time so rather than find out about it I just blundered in and bought something. I do not expect to do much crimping in the future so just looked online and bought the cheapest set I could find that seemed to do what I wanted.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I used deep learning to update my natural neural networks in my head, basically I just stuck some wire inside the crimpets (or connectors) and tried to make good connections with the wire using the crimping tool. Initially there was little success as the tool I obtained did not come with any instructions what-so-ever. The crimpets would not stay on the wire while I attempted to use the crimping tool and several crimpets were harmed in this process.

 

image

 

It took me several attempts to work out that the tool I had purchased did not do any folding of the little tabs on the crimpets. Once I had worked this out and folded over the ;little tabs using some pin nosed pliers I was able to make some good crimped connections. I'm not sure if it uses cold-welding or just mechanical interference to make a good physical and electrical connection, but they seem to work, so all is good.

 

Dubbie

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 5 years ago in reply to ajcc +8
    Hi Adrian, Probably everyone has their own recommendations, I've been quite impressed with the Multicomp HT-xxx range, I have several of them, they are about $25 ballpark. The HT-230 crimp tool HT-230…
  • shabaz
    shabaz over 5 years ago +7
    Hi Dubbie, I do the same as Doug, i.e. add some solder (after crimping) if the specific crimp tool isn't suitable. However, I think maybe your tool might do both the bare wire crimping and the insulation…
  • dougw
    dougw over 5 years ago +5
    There is a lot of science behind good crimp connections. I suspect they rely on the wire bring more springy than the crimp terminal, so after a crimp there is always force on the joint Whenever I don't…
Parents
  • ajcc
    ajcc over 5 years ago

    Neat!

    Those battery terminals sure look a lot sturdier.

     

    I didn't know those tools just finished the crimp, now I'm curious what the "better one" looks like. Because I've been thinking about getting one for crimping spade lugs, the ones you can use with some banana plugs and smaller ones for screw terminals.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to ajcc

    Hi Adrian,

     

    Probably everyone has their own recommendations, I've been quite impressed with the Multicomp HT-xxx range, I have several of them, they are about $25 ballpark.

    The HT-230 crimp toolHT-230 crimp tool works for the bare (non-insulated terminals). It does the thin gold-colored ones with ease, but the slightly thicker material crimps need a lot of force, with both hands.

    Here's a photo showing it's results, compared to a higher-end tool. The top two crimps are done with the HT-230, and the lower one is with a Knipex toolKnipex tool (£200, but it's >$400 in the USA). There's not a lot of difference, personally I think they are both acceptable, except the Knipex tool requires a lot less effort for the thick crimp terminals. But the Knipex tool is x-in-one, it has swappable crimping adapters.

     

    The photo shows 22 AWG PVC wire, and since sometimes the terminals are for thicker wire, I have folded the wire before inserting it into such crimp terminals. Probably frowned upon, but for prototypes I have no issue with this.

    image

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 5 years ago in reply to ajcc

    Hi Adrian,

     

    Probably everyone has their own recommendations, I've been quite impressed with the Multicomp HT-xxx range, I have several of them, they are about $25 ballpark.

    The HT-230 crimp toolHT-230 crimp tool works for the bare (non-insulated terminals). It does the thin gold-colored ones with ease, but the slightly thicker material crimps need a lot of force, with both hands.

    Here's a photo showing it's results, compared to a higher-end tool. The top two crimps are done with the HT-230, and the lower one is with a Knipex toolKnipex tool (£200, but it's >$400 in the USA). There's not a lot of difference, personally I think they are both acceptable, except the Knipex tool requires a lot less effort for the thick crimp terminals. But the Knipex tool is x-in-one, it has swappable crimping adapters.

     

    The photo shows 22 AWG PVC wire, and since sometimes the terminals are for thicker wire, I have folded the wire before inserting it into such crimp terminals. Probably frowned upon, but for prototypes I have no issue with this.

    image

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to shabaz

    Yep that's how a crimp should look like. Did loads when working at the DAF truck factory.

    Solder isn't good in crimp contacts except for static things. The wires break where the solder stops.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 5 years ago in reply to shabaz

    Shabaz,

     

    Good crimping, mine look nothing like as good as these.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ajcc
    ajcc over 5 years ago in reply to shabaz

    Thanks for pointing out that they're for bare non-isolated terminals, I didn't even think about that. The Multicomp crimping tool looks like a very affordable and capable tool, at least those crimps looks nice image I've only ever heard good things about Knipex, often following a story about how many decades ago said tool was purchased.