Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs My New Robot
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 26 Mar 2019 1:29 PM Date Created
  • Views 3438 views
  • Likes 10 likes
  • Comments 23 comments
  • month or robots
  • robot
  • walking robot
Related
Recommended

My New Robot

dubbie
dubbie
26 Mar 2019

Just received my latest robot called Super Fighter, already assembled which is a change for me. I was attracted to this robot as it had a reasonable price, it looked good, it was supposed to walk (which it does - sort of), fire a 'laser', speak and most importantly, fires foam disks out the front.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

It is quite an interesting design as most parts are independent of all others. The laser arm contains it's own motor and LED, the two legs have a motor in each foot, the head just contains LEDs and the infrared communications diodes and the foam disk mechanism fits into the chest. It would be relatively easy to add a motor to the second arm as this is not currently motorised, as well as adding sensors and what-knots to the head.

 

I have already disassembled it and it looks relatively easy to replace the existing controller board with an Arduino or similar. The supplied controller looks like it is some sort of custom single chip microprocessor and I doubt it could be reprogrammed. Most of the motors and LEDs seem to be driven directly from this custom PCB so if replaced it would be necessary to provide H bridge drivers or similar for three DC motors (two feet and one arm), plus transistors to drive the two motors used in the foam disk firing mechanism - these only rotate in one direction so do not need H bridge drivers.

 

There is some spare room inside the chest cavity for other sensors and radio communications. The current remote control system uses infrared. It might be necessary to remove the foam disk firing mechanism if more space were needed.

 

I wonder if I could use this for an entry into the Month of Robots competition?

 

Dubbie

  • Sign in to reply

Top Comments

  • ralphjy
    ralphjy over 7 years ago +8
    Looks like a fun toy. We should have a new competition for best toy hack.
  • fmilburn
    fmilburn over 7 years ago in reply to ralphjy +6
    tariq.ahmad great suggestion from Ralph
  • tariq.ahmad
    tariq.ahmad over 7 years ago in reply to ralphjy +6
    Have a special place in my heart for our first Project14 Techno Toys . Sounds similar to that, would be cool to have a similar competition.
Parents
  • 14rhb
    14rhb over 7 years ago

    The laser arm....

    "You have 20 seconds to comply" image

     

    Good luck with your modifications Dubbie.

     

    Rod

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to 14rhb

    Rod,

     

    I'm going to have to work out how to do the recorded voices. It cannot be that difficult as many toys now seem to come with these.

     

    Dubbie

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to wolfgangfriedrich

    Wolfgang,

     

    This Little Soundie looks exactly what I would like to use. The only drawback is the price. It is not something that could be used in several smaller items, such as a swarm of mini robots.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to dubbie

    Dubbie,

    I hear you. Those breakout boards are really useful for one-offs but anything higher quantities gets expensive quick. And Sparkfun must be selling a ton of them, as the IC alone is US$8 in qty >250. There must be cheaper audio codecs out there with similar functions.

    Cheers,

    - Wolfgang.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to dubbie

    I wonder if you could make something using a simple MCU that includes a DAC peripheral? It should be possible to make something reasonable as many simple PIC microcontrollers can manage 32MHz. If the audio was to not be changed after programming, and you only wanted a few seconds, it could reside in the program/flash memory. Reducing frequency range or bit resolution could also allow longer playback periods. [Please note, I have never done this before, so any experts at audio CODEC and the like please add comments ]

     

    Rod

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to dubbie

    Hi Dubbie,

    I have used a couple of different sound boards including this one from Adafruit.  If you want to try something less expensive there are JQ6500 boards from the usual suppliers of inexpensive products from China that play MP3 files - e.g. ebay, aliexpress.  There is a good description of how to use them, including a link to an Arduino library, here.  The one I have is the 16 pin version - video below demonstrates an Arduino Uno using it to play a "doorbell" MP3.  I have not tried the 28 pin version but it would hold many more files and have larger storage.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    I have not used this in a project yet.  Just hooked it up to see if I could get it working....

     

    Frank

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to fmilburn

    OK, found the other inexpensive one I have used - ISD1820.  It has the advantage that you can record directly to it but less capacity and lower quality.  Probably not as good for what you are considering...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 7 years ago in reply to fmilburn

    OK, found the other inexpensive one I have used - ISD1820.  It has the advantage that you can record directly to it but less capacity and lower quality.  Probably not as good for what you are considering...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 7 years ago in reply to fmilburn

    Frank,

     

    I have used ISD chips before, although not this particular one. They work well but the one's I used took some getting going as they record the audio in so they needed a good audio input filter and so on. Plus in was a big chip. I do have a child's toy that contains something similar, where you record a message and then you can change the playback frequency to make it higher or lower pitched. This works but you can only have one message!

     

    Dubbie