Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Op Amps: NIC (Negative Impedance Converter) and the Chua Oscillator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 4 May 2019 10:41 PM Date Created
  • Views 7795 views
  • Likes 11 likes
  • Comments 6 comments
  • opampsch
  • simulation
  • analog design
  • chua
  • nic
  • chaos
  • negative resistance
  • op amps
Related
Recommended

Op Amps: NIC (Negative Impedance Converter) and the Chua Oscillator

jc2048
jc2048
4 May 2019

Introduction

 

NIC stands for Negative Impedance Converter. It's one particular circuit configuration that can exhibit the

phenomena of negative resistance. I'm going to look at that first and then, once we've done that, I'm going

to use a pair of them to power a rather curious oscillator circuit due to Chua (the fun bit).

 

An Op Amp Negative Impedance Converter

 

As I'm sure you all know, a simple passive resistor has a property called resistance. The resistance is the

constant of proportionality between the current through the resistor and the voltage across the resistor and

is always positive. If we reverse the voltage, the current also reverses and so the signs cancel, leaving us

still with a positive value for the resistance. Plotted as voltage against current, the resistance is the slope of

the curve. It's not too difficult to imagine a circuit where the current falls as the voltage increases and that's

what a NIC does.

 

Here it is, as I've got it in the simulator.

 

image

Unusually, it has just one port. Most circuits we look at generally have two or more ports, at least an input

and an output, but this circuit has just one; the port serves as both the input and the output. In that, it's similar

to passive components such as resistors, capacitors, and inductors, except that one side of the port connects

to ground.

 

I'm driving the input with a very slow ramp between the negative supply voltage and the positive supply voltage

so we can see how it behaves. The resistance curve has been computed by the post-processor, after running

the simulation, by using Ohm's Law on the voltage and current measured at the input. Over quite a wide central

range, as the input voltage increases, we can see that the current falls and the computed value for the resistance

shows a value of somewhere between -3k and -4k. Not too surprisingly, that starts to fail when the op amp output

gets to within a couple of volts of either supply rail. [The messy bit in the middle is the post-processor not liking

the very small values around zero.]

 

image

Understanding how it works, in a qualitative way, is quite simple (not always the case, even with seemingly

simple op amp configurations, once we go beyond the standard amplifier circuits - the Howland current pump,

for one, seems to be messy to explain without using equations as I've just discovered). Negative feedback will

cause the amplifier to drive the output (if it is able to do that) in such a way as to bring the difference in

potential between the op amp inputs to a very small value. For an ideal op amp, with infinite gain, that difference

would be zero but for a real amplifier there has to be a small voltage there, though for this purpose we can take

it as being zero. So we can quickly see that the voltage at the circuit input will be the same as the voltage at the

top of the resistor to ground (R3). That voltage defines the current through the resistor. Since the op amp has a

high impedance input, that same current also flows in the resistor from the op amp output (R2). As the resistor

(R1) from the output to the non-inverting input has the same value as the one to the inverting input and there

is the same voltage across it, there will also be the same current flowing in that one. That current flows out

of the input to the circuit. In short, the NIC applies the voltage from the input to the resistor and then mirrors

the negative of its current back to the input. Looking into the input it then seems as though we are seeing the

negative of the resistance R3. [An obvious way to vary the circuit would be to change the ratio between the two

feedback resistors to something other than 1:1 and use that to scale the resistance.]

 

Whilst the analysis was for a resistor, if we had a capacitor or inductor in place of the resistor, the circuit would

similarly attempt the negative of the current and by doing so convert a pure capacitor into an inductor or a pure

inductor into a capacitor, though we might need to look quite carefully at how the op amp behaved stability-wise

with a reactive component, depending on the resistors doing the feedback.

 

Let the Lord of Chaos Reign

 

Now for the fun part.

 

I didn't mention it in the previous section but another feature of a negative resistance is that it no longer

dissipates power in the same way as a passive resistor does. That's because P = IV now gives a negative result.

That means it can power an oscillator circuit. Of course the power doesn't come out of thin air; the source is

the power supply, via the op amp output, but we can treat the NIC circuit as behaving as though it were a simple

negative resistor.

 

Chua published a model that he claimed exhibited chaotic behaviour. He said that it was necessary to have

at least three energy storing components and invented a component he called the Chua diode to power them.

The 'diode' was a combination of a negative resistor to power the oscillations and a non-linear element that

would act as a limiter (I'm not particularly clear about this, but I think the non-linear element positions the

attractors and prevents the circuit running off to one or other rail and just sitting there).

 

Here's the circuit I used for these experiments.

 

image

 

It derives from one published in An Analog Electronics Companion [2], though I've adapted it a little for the

particular op amps and inductor that I had to hand. The resistor shown in series with the coil (R7) is really

just that of the winding resistance: I could have included it as one of the coil's hidden parameters instead

but thought it would be better to have it there on the schematic. The resistance leads to damping of the

oscillations and will have an effect on whether the oscillator oscillates at all. The XY plot on the oscilloscope

I did by measuring the points I've labelled 'A' and 'B'. Hamilton points out in his book that there are also

interesting XY plots to be seen if you plot one of the voltages against the currents that circulate (easy to

view in the simulator, but a bit more challenging in the physical circuit).

 

Here is the circuit built on a breadboard

 

image

 

and here is the result displayed XY on an oscilloscope

 

image

 

I found that the most critical component was the resistor (R8) linking the two capacitors together. Too high

a value and not enough energy will get to the coil and capacitor (L1 and C1), from the NICs, to maintain

the oscillation. Too low a value, and the two capacitors (C1 and C2) couple tightly with the coil and the

whole thing oscillates at a single frequency, with just a phase shift between the two capacitors, giving rise

to a simple ellipse on the XY plot. Somewhere between, there's a point where the two sides are loosely

coupled and just lightly influence each other and that's where the chaotic behaviour occurs. I used a fixed

resistor of 680R, in series with a 1k pot, so that I could adjust it to find a good value. Note that it is very

unlikely to be the same as whatever value you find you need to get it going in the simulator.

 

A couple of practical points if you want to try to get it working in the simulator. I found that I had to force

the node I've labelled 'A' to zero volts at the start in order to get it to oscillate. I also had to load the analysis

parameter set that is specifically for oscillators, it didn't work with the default set.

 

Here are the waveforms that a transient analysis gives

 

image

And here it is on the virtual oscilloscope that you can access from the 'T&M' menu

 

image

 

So why did Hamilton use two NICs rather than one? As far as I can see, the answer lies in the feedback

resistors. By having high values for one of the NICs, he engineers a situation where the negative

resistance for that NIC only happens over a restricted part of the range [because the op amp output

runs out of voltage to drive it]. Once that is put in parallel with the other NIC, that then gives the non-linear

response that Chua required in addition to the negative resistance.

 

The reason for having to have at least three energy storing elements is that if there were only two

elements we wouldn't get the trace crossing - in this case, the XY plot is a projection of a trajectory

in a 3-D space.

 

Final thought: the simulation is totally deterministic and the traces are the same each and every time.

Chaotic behaviour isn't the same thing as randomness. However, the real circuit is naturally sensitive

to noise and is evidently being thrown around a good deal. The general form, with the orbits traced

around the two attractors, are very similar but the simulation won't ever match the the real results.

 

I don't claim any particular expertise with all of this (chaos or NICs) and wouldn't have got to a working

circuit without the help of Hamilton's book. If anyone out there understands the theory well, please feel

free to set me right on anything I've explained wrongly in the comments below.

 

If you found this interesting and would like to see more blogs I've written, a list can be found here: jc2048 Blog Index

 

Notes:
[1] Some of the information on negative resistance came from Handbook of Linear Integrated Electronics for Research by T.D.S Hamilton, 1977.
[2] An Analog Electronics Companion by Scott Hamilton, CUP 2003.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 7 years ago +4
    Hi Jon, I enjoyed your very interesting experiment and blog. I read a couple books a while back on chaos theory. It was interesting to see that one can produce a chaotic system electronically. While I…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz +4
    shabaz wrote: Hi Jon, Interesting circuit, and very unusual behaviour! The black hole of electronics
  • jc2048
    jc2048 over 7 years ago in reply to shabaz +4
    I believe the Chua 'diode' is quite artificial, I imagine it was just a convenience for him when he wrote his paper - it rolls into one circuit symbol all the other miscellaneous bits of the circuit so…
Parents
  • shabaz
    shabaz over 7 years ago

    By coincidence today another article on negative resistance here:

    https://hackaday.com/2019/05/08/fun-with-negative-resistance-jellybean-transistors/

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago

    By coincidence today another article on negative resistance here:

    https://hackaday.com/2019/05/08/fun-with-negative-resistance-jellybean-transistors/

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 over 7 years ago in reply to shabaz

    Thanks for the link, that was interesting. His transistor simulation of a tunnel diode curve is neat.