Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Overview
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 2 Mar 2012 12:08 AM Date Created
  • Views 1817 views
  • Likes 1 like
  • Comments 14 comments
  • model_a
  • hardware
  • pcb_design
  • pcb_fabrication
  • raspberry_pi
  • model_b
Related
Recommended

Overview

e14 Contributor
e14 Contributor
2 Mar 2012

In this blog I hope to share with you some of the more interesting way points on the journey to designing the Raspberry Pi Hardware from the ideas kicking around 6 years ago to the overwhelming (for me and a few servers!) launch on Wednesday. 

 

I was lucky enough to be with element14 in Nuremberg when the RPi arrived from the UK for the noon on-stand launch.  Mike Powell from element14 deftly cabled the RPi, but gave me the 'honour' of powering it up. As many of you will know - it's a heart stopping moment (especially in front of a crowd of enthusiasts) until the kernel boot appears on the screen - it's either command line, terminal silence or smoke!

 

There is plenty of stuff on the Web about the Foundation and it's aims so I won't be repeating it here (unless asked).  There will be little discussion about software - we have lots of talented people in the team that can talk way more sensibly about that.  There is also an equally talented team on the hardware side and I hope I can encourage them to chip in with useful comment and correct me when I go off the rails.

 

I'm very happy to be sign posted to things that interest you - so let me know, and I'm sure they can be worked in somewhere.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor +1
    coder27 - I'm not an expert on driving the Silicon but there is an 128kB L2 cache and by choosing the address range you can either use it or bypass it with the CPU. The GPU is really slated the main user…
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Pete,

    Could you explain how a SOC was selected that has no L2 cache for the CPU?  Can you recall any successful Linux computers without an L2 cache?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    coder27 -

     

    I'm not an expert on driving the Silicon but there is an 128kB L2 cache and by choosing the address range you can either use it or bypass it with the CPU.  The GPU is really slated the main user.

     

    There is some scant information in: http://www.raspberrypi.org/wp-content/uploads/2012/02/BCM2835-ARM-Peripherals.pdf

     

    At the end of the day a cache just makes things go quicker, although nowadays it is often also used to unpack/pack SDRAM burst reads / writes.  With the L1data and instruction cache and the improved branch predict over the Arm 9, I never really considered it to be an issue.

     

    Within the scope of our project the Silicon was chosen because of it's overall capability - especially in Multimedia and the richness of perhiperals and the low supporting cast of components - it was never intended to be a compute workhorse. We could have chosen something else (but check into Eben's day job).... nuff said.

     

    I would be interested to hear your comments

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    @coder27: The amount and organisation of caches really depends on the goals set by the designers.  The BCM2835 was not designed as an all-out speed demon on the CPU front, hence the descriptions of "Videocore IV with ARM bolted on the side" in some Hardware FAQ.  That said, the datasheet that PeteL pointed to says "BCM2835 provides a 128KB system L2 cache, which is used primarily by the GPU. Accesses to memory are routed either via or around the L2 cache depending on senior two bits of the bus address."

     

    So, it sounds like you can use the L2 cache from the CPU in some circumstances... is it done in the RPi Linux build at the moment?  Not sure.  Bear in mind that the datasheet was written for engineers looking at the BCM2835's suitability for embedded use - in which case the GPU would be the main user of the L2 cache.  Also, remember that the only reason an L2 cache exists in a single core system is to reduce cache miss rates for less overall (cost/latency/hit to the maximum achievable CPU frequency) than enlarging the L1 cache.  In a perfect world where you didn't have to care about such mundanities, you would just choose the L1 cache size to fit your cache miss rate for your chosen workloads.

     

    I went looking for a boot log to see if there was a mention of how big the ARM's L1 cache was - the ARM1176 architecture manual only says that L1 is between 4KB and 64KB in size - the decision is left to the licensee as to how much chip area they want to spend on the cache.  I couldn't find anything in the only dmesg output (from Paul Maunders' beta board).

     

    In any case, what are you worried about being slow in particular?  The GUI?  The boot time?  The actual programming environment?  It's got about as much memory and CPU performance as the machine I used as a staff member of a university Computer Science department in 2001... and I seem to remember being able to write a few programs with that.  Boot times can be tuned, simpler GUIs favoured, and lightweight IDEs chosen.  It's for schoolkids after all... they don't need Eclipse to write programs a few pages long; back when I was at secondary college, we thought that Turbo Pascal running on a 640KB PC was usable for what we were asked to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I'll put my old academia hat on and agree with Jason that speed is not a major concern in education, which is the motivating force for Rpi.  The CPU just needs to be "fast enough" to keep it highly responsive so that interactive development is not bogged down.

     

    Of course it's always nice to have more speed, but I think we'll have to wait for Rpi Next Gen for that.  The BCM2835's ARM11 is inherently slower than a modern Cortex-A series, so it's not the best choice of ARM core for speed merchants --- but then, that was never a requirement in this design.

     

    The other ARM licensees are probably very dismayed at Broadcom's massive PR coup with Raspberry Pi, but they have ample opportunity to compete:  make a similar board within the $25-$35 price bracket but based on a more modern core.  And if ARM Holdings needs some major pummeling to lower Cortex licensing fees if they're too high for this niche (as the BeagleBone price suggests), so be it. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    The reports we have heard so far say the RPi is "sluggish".

    Sluggish computers are not fun to use, which defeats the purpose

    of getting kids excited about programming.  Yes, you can

    minimize the problem by using light-weight versions of IDE's,

    programming languages, word processors, web browsers,

    window managers, etc., but it would be a lot better to be able

    to use more mainstream software.

     

    Modern software is quite extensive in its memory usage,

    and benefits greatly from memory caches.  My understanding

    is that although it is possible to access the L2 cache from

    the CPU, it is not practical to do so, because the L2 cache is

    directly connected to the GPU and takes longer to access

    from the CPU.

     

    Turbo Pascal was quite an anomaly, with exceptional

    performance due in large part to being written in assembly,

    which is not true of most modern software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    @coder27: yes, Turbo Pascal was a nifty bit of assembler hacking.  But the RPi is probably 100 times faster than the old 5MHz 8088 - they had pretty crappy memory systems too, you know... and their closest thing to a cache was a 4 byte instruction queue. :-)    If you want a full on compositing desktop with wibbly windows and translucent borders, it'll likely chug, but if kids get put off because the GUI isn't shiny enough then they weren't that likely to be really motivated at programming either.

     

    I've read Hennessy and Patterson, I know a fair deal about caches and CPU.  I also had an L2-lacking 300MHz Celeron which ran just fine at 450MHz and a 600MHz Duron which ran just fine at 900MHz; the fact that these chips lacked L2 meant that they tended to run cool enough and draw little enough current to run successfully at a 50% overclock, at which speed they felt pretty snappy, despite needing to hit memory more often than an equivalent Pentium III or Athlon would.  It really does depend a huge amount on the miss rate and achievable IPC of your workload as to how badly things will run with just a moderate sized L1 cache.  Would the RPi's SOC be as cheap, or run the ARM as fast, if the CPU had a bigger, better L2 cache?

     

    I will say that as a sysadmin these last 16 years, I've seen a lot of ways in which a machine can seem slow at doing one thing or another that have proved to be absolutely nothing to do with raw CPU speed; as well as some that have... looking forward to seeing this sluggish RPi for myself someday! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Jason,

      About the only thing I remember from Hennessy and Patterson was Tomasulo this and Tomasulo that.

    It sounded to me like a cross between Han Solo and Mr. Sulu.

     

      My concern isn't so much the eye candy of a fancy GUI, I am presuming the GPU can eventually be

    harnessed for that.  I'm more concerned about mundane things like reports of apt get "taking ages",

    or web pages taking a long time to load.  It's also really useful for a linux box to be able to compile linux.

     

    I don't really understand why the L2 cache in the RPi is more closely attached to the GPU

    than the CPU.  Ideally, it would be readily accessible to both.  It probably wouldn't be cost effective

    to have a separate L2 cache for each. 

     

    My recollection of celeron overclocking is that it was easier to do without cache because the

    cache SRAMs were separate chips, and they had less overclocking headroom than the cpu. 

    I don't think that has any bearing on the ARM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Jason,

      About the only thing I remember from Hennessy and Patterson was Tomasulo this and Tomasulo that.

    It sounded to me like a cross between Han Solo and Mr. Sulu.

     

      My concern isn't so much the eye candy of a fancy GUI, I am presuming the GPU can eventually be

    harnessed for that.  I'm more concerned about mundane things like reports of apt get "taking ages",

    or web pages taking a long time to load.  It's also really useful for a linux box to be able to compile linux.

     

    I don't really understand why the L2 cache in the RPi is more closely attached to the GPU

    than the CPU.  Ideally, it would be readily accessible to both.  It probably wouldn't be cost effective

    to have a separate L2 cache for each. 

     

    My recollection of celeron overclocking is that it was easier to do without cache because the

    cache SRAMs were separate chips, and they had less overclocking headroom than the cpu. 

    I don't think that has any bearing on the ARM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    @coder27: Funny you should mention apt get.  I had a low-end Ubuntu server with a dual-core Athlon part in it that was taking ages to do package updates, and I was wondering whether the CPUs were really that slow.  I realised that the version of btrfs that I had used for the root filesystem was generating much too much synchronous disk activity.  Turning on write-behind caching on the disk caused apt get to run much faster, which showed that the CPUs weren't the bottleneck.  The real fix is either to upgrade to a later Ubuntu release with better btrfs performance or reinstall with ext4 as the root partition!  This is an example of how there are more ways for computers to seem slow than just having a slow CPU.

     

    apt get to an SD card will depend very much on the SD card's small write performance.  As far as self-hosted Linux compilation, I'd guess the same thing.  A USB external HD would be a very good idea for such a workload.

     

    A correction to my last comment: my recollection of Celeron overclocking was hazy - I had a 266MHz Celeron with no cache early on that I got running at 400MHz when I couldn't afford anything better, but the Celeron 300As that I used to play with had 128KB of L2 cache on-die.  This was still a lot less than the 512KB on the contemporaneous Pentium II, but when running at 450MHz the Celeron held up fairly well against a 450MHz PII.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    agreed that there are many ways for a computer to seem slow besides a slow cpu.

    However, the RPi and SoC designers couldn't have done much about the slow

    interfaces (SD card, USB 2.0, 10/100 ethernet over USB, etc.,) within their budget,

    but it does seem like they probably could have integrated the ARM better, rather than

    just "bolting it on the side", where the L2 cache is pretty much useless to the cpu.

     

    Based on celeron benchmarks vs Pentium II, the L2 cache probably has about a

    20% effect on cpu intensive jobs.  That's what caused Intel to quickly put 128KB

    L2 cache on the celeron.