Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Power Consumption of a Wemos D1 mini ESP8266 - Long Term Test 3
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: neilk
  • Date Created: 20 Mar 2019 6:10 PM Date Created
  • Views 7721 views
  • Likes 9 likes
  • Comments 8 comments
  • wemos d1 mini
  • esp-8266
Related
Recommended

Power Consumption of a Wemos D1 mini ESP8266 - Long Term Test 3

neilk
neilk
20 Mar 2019

Having returned from my holiday in the winter sun image, I removed the battery from its holder and set about fitting the XH2-2.54mm female connector to the battery holder leads.

 

I then modified the sketch to reduce the drift in the sleep time which is evident in the chart from Long Term Test 2, repeated below:

 

image

 

I checked the battery voltage and was pleased to see that it still showed 3.74 V on my DMM. Rather than charge it, I decided to reconnect the Wemos d1 mini system and see how much longer the battery would last

 

When I terminated Long Term Test 2, the battery voltage, as monitored by the Wemos d1, was 3.64V. When I reconnected everything and restarted the sketch, the battery voltage as monitored by the Wemos was 3.8V. 

 

I assume that the improvement in the cabling between the battery and the battery shield could be making a difference. By fitting the XH2-2.54mm female connector to the battery holder leads, I have eliminated 1 pair of screw terminals, 1 pair of Dupont type connections and 2 short lengths of wire

 

First Partial Test:

image

.

 

I terminated this test run after just over 25 hours, to allow for further correction of the sleep time. At the start of this partial run, the battery voltage, as measured by the Wemos A/D was about 3.8V and at the end it was about 3.75V.

 

One observation from this first partial test is that the battery voltage appears to be noisier during the night - when the temperature drops.

 

After adjusting the sleep time correction factor, I had to leave my workspace for a while and left the Wemos still powered from my PC. When I returned, I glanced at the log file and found that the sleep time error was very different from what I expected. I wondered if this might be a function of being powered via USB, rather than by battery. Keen to fully investigate the power consumption, I decided to leave the issue of power source affecting the accuracy of sleep time on one side for now.

 

I reconnected the battery and restarted the test, to run for a further 24 hours.

 

Second Partial Test

 

image

The battery voltage at the start of this run was about 3.75V and at the end of the run it was about 3.7V - this is over approximately 24 hours. Once again, the measured voltage seems to be noisier overnight - it was colder!

 

Now that the sleep time error is much less, it's possible to discern a variation of the error with ambient temperature.

 

I made a further adjustment to the sleep time, reconnected the battery and started another test, intending to run this one until the Wemos stopped working

 

Third Partial Test

 

image

 

I stopped this partial run after about 3 days, in order to make some minor alterations, including modifying the date/time stamp to use the 24 hour clock instead of am and pm:

The voltage at the start of this partial run was about 3.71V and at the end of the run it was about 3.59V

 

I restarted the system, determined this time to leave it until the Wemos stopped working. - ie until the battery voltage has fallen below the level required to keep the battery shield delivering 5V. According to the Wemos data sheet, this should be 3.2V,

 

Fourth and Final Partial Test

 

image

 

And finally, the Wemos dies! The  final battery voltage, as measured by the Wemos A/D, was about 2.81V, after a further 3 days. This is a lot lowerr than the 3.2V stated in the Wemos data sheet.

 

In total, with interruptions, the battery lasted about 336 hours, or 14 days, far longer than originally predicted!

 

I have concatenated all the battery files together to show the whole discharge pattern - apologies for the first section, before I fitted the correct connector to the battery leads!

 

Composite Graph

 

image

The date/time axis has interruptions in it, but is set to display a value every 1440 readings. With +ve drift in the sleep time, this will be slightly more than 24 hours.

 

Conclusions

 

The 18650 Li-ion battery lasted far longer than I anticipated - a total of 14 days, with readings at 1 minute intervals. Increasing the interval between readings to 5 minutes would give a battery life of perhaps up to 70 days - plenty long enough for a remote, unattended device.

 

There is some evidence that the accuracy of the sleep time duration of the Wemos is affected by ambient temperature. In my real application - monitoring inside and outside temperature of an unheated greenhouse -  I can expect the temperature swing experienced by the Wemos to be somewhat greater than at my workspace.

 

I am also aware that the performance of the 18650 Li-ion battery is likely to be affected by ambient temperature.

 

 

Final Note

 

The  crude prototype system has been sealed up in a plastic food container and moved out to one of the greenhouses. One probe is hanging out of the window, a few inches away from the glass; the other is hanging over the potting bench, shielded from direct sunlight.

  • Sign in to reply

Top Comments

  • kiri-ll
    kiri-ll over 7 years ago +3
    Nice research:) I like that I can actually estimate the standalone lifetime of the WiFi module. May I ask you more about your application? In addition to WiFi communication, which peripherals do you have…
  • kiri-ll
    kiri-ll over 7 years ago in reply to neilk +3
    Nice, you have a very light-weight application. Do you plan more power-hungry features in future?
  • genebren
    genebren over 7 years ago +2
    Nice set of data/experiments. Hard to say that the extrapolation from 14 days to 70 days is going to work out in real life. There are a lot of issues, including internal leakage that will effect the long…
Parents
  • kiri-ll
    kiri-ll over 7 years ago

    Nice research:) I like that I can actually estimate the standalone lifetime of the WiFi module. May I ask you more about your application? In addition to WiFi communication, which peripherals do you have on board? How many mAh are in your battery?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 7 years ago in reply to kiri-ll

    Thanks, Kiri, I have 2 x DS18B20 temperature probes monitored via GPIO pin 14 of the ESP8266, which maps to pin D5 in the Arduino IDE.

     

    The 18650 li-ion battery has a nominal capacity of 2400mAh

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neilk
    neilk over 7 years ago in reply to kiri-ll

    Thanks, Kiri, I have 2 x DS18B20 temperature probes monitored via GPIO pin 14 of the ESP8266, which maps to pin D5 in the Arduino IDE.

     

    The 18650 li-ion battery has a nominal capacity of 2400mAh

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kiri-ll
    kiri-ll over 7 years ago in reply to neilk

    Nice, you have a very light-weight application. Do you plan more power-hungry features in future?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 7 years ago in reply to kiri-ll

    I am about to modify the software to send me email to alert me to adverse conditions and I am also investigating self managed OTA re-programming from my website. Checking to see if these operations need to be done and the operations themselves will undoubtedly consume more power. How much, I don't yet know.

     

    At some time in the next few months, I will have a mains supply established in the greenhouse and will be able to run the system from a mobile phone charger. Then I might consider introducing control of a small heater and an air circulation fan.

     

    That should keep me busy!

     

    Neil

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kiri-ll
    kiri-ll over 7 years ago in reply to neilk

    Ah, so, it is about the greenhouse. It was interesting for me to read, how you fight for power-saving. I thought you would continue into this direction and do some experiments with adding more HW, power-saving that, comparing the lifetime after applying different techniques, and so on

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 7 years ago in reply to kiri-ll

    Glad you found it interesting image