Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Raspberry pi Questions
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: godblessamerica
  • Date Created: 23 Sep 2016 1:47 PM Date Created
  • Views 2190 views
  • Likes 2 likes
  • Comments 14 comments
  • raspberry pi
Related
Recommended

Raspberry pi Questions

godblessamerica
godblessamerica
23 Sep 2016

I have never purchased a Raspberry pi of any sort; so I was wondering if anyone out there could answer me a few of the following questions:

 

If I were to buy a Raspberry pi zero how much money would it cost to make it as capable of doing things as the Raspberry pi 3?

 

If I did that would it run as fast as a Raspberry pi 3?

 

Would it also power the same amount of stuff?

  • Sign in to reply

Top Comments

  • fvan
    fvan over 9 years ago +2
    Hi, try to avoid posting the same question in multiple places, as people may answer on one or the other, causing things to become chaotic Same question as: The specified item was not found. and The specified…
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to godblessamerica +2
    WRT RaspPi Zero and the possible need for an OTG Cable?/USB-Hub, I received an email from Amazon.com for a RaspPi Zero Case, Case sold w/ a OTG Cable.You have to provide your Own RaspPi Zero. IDK (I Don…
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to uscdadnyc +2
    TS (Time Stamp) = 11:32PM 06OCT16. Tried my Bidal USB Hub w/ that cheapie OTG Hub? interposed between the Bidal Hub and the USB connector (on left) of the RaspPi Zero. Same problem: get into Raspian GUI…
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to uscdadnyc

    TS 03OCT16. Follow-up. I bought and Used (successfully) a Bidul USB Hub 3/0 w/ ethernet Adapter. This Bidul unit works Fine on my RaspPi 3B, but not on my RaspPi Zero. WTF? Raspian seemed to have support for these type(s) of USB 3.0 Hubs, I did not have to download any drivers.   Same version of Raspbian. Same H/W aside from a RaspPi 3B Instead of RaspPi Zero. WTF2? AAR this is a low priority project for me. So, if you Guys/Gals want anymore info, I may pick-up the Baton again.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to godblessamerica

    A low priority project of mine concerns the RaspPi Zero. BTW I also have a RaspPi 3B mounted in a SmartiPi (tm =Trademark) Case that also houses the "official" -7" RaspPi TouchScreen. With an attachable location for a Bitscope on the Case's Lego (tm) Studs.

    AAR I have booted Raspian -Jessie 2016-05-27 on the RaspPi Zero and got to the Raspian GUI Window. But the attached USB Keyboard and USB Mouse DID NOT work . These two USB Devices were connected via a cheapie Chinese OTG Hub. IDK (I Don't Know) whether it is the OTG Hub that is Bad OR What?. I am going to buy a powered USB3.0 Hub to swap-out (Trouble-shoot)

    AAR I have two Q's myself: Q1: The microUSB -B receptacle marked " J10 USB" cannot? supply +5v to any attached USB Devices? Can it? If it does, where does it come from ? The microUSB -B receptacle marked "J1 Pwr In"? Is there a Block Diagram/Schematic for the RaspPi Zero.?

    Q2; The USB3.0 Hub that I am going to Buy, has a RJ-45 Jack for Wired LAN. I know that this USB-to-RJ45 IS SUPPORTED ON WIN10. What about Raspian?

    Long Range Plan is to get the RaspPi working as a SBC (Single Board Computer) first, then when the S/W & Apps are stable, strip down to

    the bare minimum. Possible RaspPiZero w/ RTC Shim and possible BT/RF-NearField  USB Nob Adapter(s)

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • godblessamerica
    godblessamerica over 9 years ago in reply to fvan

    K

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 9 years ago

    Hi, try to avoid posting the same question in multiple places, as people may answer on one or the other, causing things to become chaotic image


    Same question as: The specified item was not found. and The specified item was not found.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<