Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Rework: Replace a QFN IC
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 12 Mar 2016 11:13 AM Date Created
  • Views 4402 views
  • Likes 8 likes
  • Comments 18 comments
  • qfn
  • rework
  • lmg5200
  • repair
  • gan
  • aoyue
  • ayoue
Related
Recommended

Rework: Replace a QFN IC

Jan Cumps
Jan Cumps
12 Mar 2016

The GaN evaluation kit I have here at home died because of a power disruption @Cumps Castle.

 

image

 

There was a power failure in the perk of Brussels where I live. Power dropped from 240V to 110.

And here's the rub: I was providing the different voltages to the evaluation board from two different power supplies. The big power from a supply that takes virtually any input voltage between 100 and 250V.

But the bias power came from a supply that's 220-240V only.

 

TL;DR the LMG5200 power driver on the board didn't survive this (as documented in its datasheet).

 

image

That chip comes in a QFN package. This is my first attempt to replace such a package

 

Baking the Chip

From the datasheet:

13.1 Package Information

The LMG5200 device package is rated as a MSL3 package (Moisture Sensitivity Level 3). Please refer to

application report SNOA550 for specific handling and process recommendations of a MSL3 package.

 

If we than check that report (our package is MLS3, 2mm thick), we're in for a long baking time.

image

I didn't bake it that long.
I used my microwave/combi oven - in the non-microwave mode - at approx 120° (all temperatures in Celsius) during 4 hours.
And I crossed my fingers.

 

Desolder Time

I'm using an Aoyue Int 968 A+  rework station. For this exercise, I used the hot air part only.
Since there are no pins on QFN packages, there's little use for a soldering iron.

 

The evaluation kit uses lead-free solder. And the LMG5200 is in the way of the heat path.
That means that you have to apply the heat to the package, and that in turn will transfer that heat to it's solder pads.

I bombed the thing with 330°, low air plow - I couldn't risk that all the surrounding parts would fly away.

It took good 2 minutes before the solder melted and the IC could be removed.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 

 

 

Solder Time

To avoid that I have to heat the pads with the new chip in place, I first pre-heated the area around the board with hot air for a few minutes.
I had the temperature set to 120°.

I then applied solder paste and put the IC in place, as good as possible.
That wasn't really easy because you don't see the pads, and the PCB didn't have an outline drawing for the chip.

 

image

 

So I placed the IC where I thought it would cover the right pads with the right pins, and pulled out the hot air nossle again.
After again a good 2 minutes, the chip pulled itself to the right position (the magic of reflow).

I let the whole thing cool down, and checked with my multimeter if there were any short-cuts.

 

When that test gave good results, I decided to put the board to the test. I powered it on and validated the circuit at the key points.

All behaves normal, and I consider this little project a success.

Customer Action Photos:

 

image

image

 

image

 

image

  • Sign in to reply

Top Comments

  • mudz
    mudz over 10 years ago +2
    I've definitely skipped this part I used my microwave/combi oven - in the non-microwave mode - at approx 120° (all temperatures in Celsius) during 4 hours. And I crossed my fingers. and used hot air to…
  • jw0752
    jw0752 over 10 years ago +2
    Hi Jan, This was a great example of saving a good project by trouble shooting and applying a calculated repair. Thank you for sharing your replacement technique. I enjoyed reading your post. John
  • mcb1
    mcb1 over 10 years ago +2
    I am presuming you needed to bake these because they were not in a hermetically sealed bag? One of the more interesting things at element14 Distribution at Leeds was the attention to detail for moisture…
Parents
  • mudz
    mudz over 10 years ago

    I've definitely skipped this part

    I used my microwave/combi oven - in the non-microwave mode - at approx 120° (all temperatures in Celsius) during 4 hours.

    And I crossed my fingers.

    and used hot air to remove and replace IC. image

    I wonder how much power is wasted in heating that for 120c for 4 hours.

     

    Thanks for sharing image

     

    mudz

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 10 years ago in reply to mudz

    Have you ever been around to see the result of not baking them? image Sometimes you get lucky, and sometimes you get a functional IC with the top blown off.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelwylie
    michaelwylie over 10 years ago in reply to mudz

    Have you ever been around to see the result of not baking them? image Sometimes you get lucky, and sometimes you get a functional IC with the top blown off.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • clem57
    clem57 over 10 years ago in reply to michaelwylie

    deleted

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 10 years ago in reply to clem57

    I must be getting old. I was expecting this one: MFW Im way too much mind blown - GIF on Imgur

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mudz
    mudz over 10 years ago in reply to michaelwylie

    Not till now, but I'm aware of the consequences. That's why I always buy spares of them. I'm doing something similar these days, maybe I'll get to see what you are saying. image

    But still I'm going to skip bake part till I make my company that bigger to afford such equipments & many more. Till then I'll follow every tricks(as an hobbyist) to save power, money and do things with only equipments I've got. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to mudz
    But still I'm going to skip bake part till I make my company that bigger

    I would be making sure that gear I build/repair is reliable.

    That will do more than pricing alone.

     

    If I understand the baking process then a simple toaster oven would suffice.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to mcb1

    A toaster oven is ok. You can even bake at 45° C. It just takes longer.

    This application note documents the required baking times for 45, 90 and 125° C.

    It has more info about this subject than just the baking profiles. It's an appnote worth reading.