Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Rotary Encoders - Part 3: Capturing Input on an Arduino
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 13 Jul 2015 9:29 AM Date Created
  • Views 4781 views
  • Likes 6 likes
  • Comments 2 comments
  • rotary_switch
  • rotary_encoder
  • arduino_uno
  • arduino
Related
Recommended

Rotary Encoders - Part 3: Capturing Input on an Arduino

Jan Cumps
Jan Cumps
13 Jul 2015

I've removed the rotary encoder from the scroll button of a defect mouse. Let's see how we can use that in a microcontroller design.

In post 1, I wired up the electronics.

In part 2, I'm capturing the encoder's info on a Cypress PSoC4.

This time, I'm checking an existing example on an Arduino UNO.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Firmware

 

Well, that was easy. I found a number of examples on http://playground.arduino.cc/Main/RotaryEncoders.

I bet the majority of the projects on that page will work. I chose rafbuff's implementation because it was clean code and uses interrupts (several examples on that page do that, but you have to make a choice).

 

It's less than 100 lines of code, provides additional in-software debouncing and doesn't require an external library.

And it works straight away.

 

image

The source is available on http://playground.arduino.cc/Main/RotaryEncoders.

Search for rafbuff.

If you think that I should have tried another implementation, post it in the comments.

 

Wiring the Hardware

 

Look back at my first post to check how to components are wired up.

Then connect the encoder with the board.

Ground to Ground, 5V to 5V,

PINA to Digital 3, PINB to Digital 2 (that's different than the code comments. My setup counted backwards when I wired it up as written in the code, but I used a different encoder).

 

Connect the Arduino, execute the program and open the Serial Monitor.

The count is logged to the monitor on every spin.

 

Content
Part 1: Electronics
Part 2: Capturing Input on Cypress PSoC4
Part 3: Capturing Input on an Arduino
Part 4: Capturing Input on a Texas Instruments Hercules LaunchPad with eQEP
Part 5: Capturing Input on an FPGA
Real World Application: Hercules LaunchPad and GaN FETs: Control Big Power with a Flimsy Mouse Scroll Wheel
  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    I've fixed the embedded video link

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago

    I've fixed the embedded video link