Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs SCITS Timer Project #3 - Timer Concept
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: three-phase
  • Date Created: 1 Feb 2018 8:15 PM Date Created
  • Views 1159 views
  • Likes 7 likes
  • Comments 6 comments
  • pickit 3
  • timer
  • scits
Related
Recommended

SCITS Timer Project #3 - Timer Concept

three-phase
three-phase
1 Feb 2018

This blog will look at the initial concept I have for building the timer.

 

When built, this timer will form part of the initial tests I do when setting up for protection relay tests to show that the apparatus is performing correctly. Testing the voltage and the current outputs is easy using a digital multimeter. A few measurements are all that is required and recorded on a check sheet that gets submitted with the report on the protection relay tests.

 

imageimage

To extend this principle, the timer unit will be utilised to verify the time recording function of the SCITS. This will then show that I have verified operation of the three basic functions of the SCITS, voltage output, current output and timing.

 

The proposal is relatively simple - The SCITS under test will be set to output a voltage that will trigger the timer module, after a preset delay, the timer module will send a pulsed output that is fed back into the SCITS trip contact circuit. The time recorded by the SCITS should then match the delay setting on the timer module. This idea is depicted below;

 

image

As well as being able to produce a delay to verify the operation of the SCITS, the timer module itself will also need to be proven. For this I aim to utilise a Keysight 53220A frequency counter / timer. The setup for this test will be similar, however, I will need the ability to manually trigger the timer module that will also send a start pulse to channel A of the frequency counter / timer, the output of the timer module will then be wired to channel B of the frequency counter / timer which will be set up to record the time interval between the two channels.

 

I have established the following needs for my SCITS timer module;

 

  • I would like the system to be battery powered
  • The input and output pulses will be TTL based as the SCITS can be set up to operate at 5V DC
  • Timer resolution can be 1ms to match the timer resolution of the SCITS
  • Maximum time delay will be 99s as I time relays up to 60 seconds
  • Timer setting will therefore be by 5 BCD thumbwheels
  • Connection to the SCITS is via 4mm safety sockets
  • Connection to the counter / timer is via BNC
  • I will need a manual trigger to verify the timer against my counter / timer
  • A reset button is always a good idea
  • Both switches will need de-bouncing, either by hardware or software

 

image

 

I haven't totally decided on the battery type yet. If the current draw is low, I may just utilise a 9V PP3 or 4 off AA batteries to a 5V regulator. If I need a larger battery capacity then I may move to a couple of 18650 cells built into the case. I have seen quite a few charger boards around for these cells, which I would hope make my build a little easier. Likewise, I haven't ruled out taking mains into the case yet and building a complete charger for it, or utilising an off the shelf AC to DC converter into a DC jack as per the diagram above. I will probably build up a test circuit first and measure the current drawn with it in operation before I decide on this.

 

To generate the time delay, I plan on using a PIC (for the first time) which will give me the TTL compatibility, but will need circa 25 I/O to read the thumbwheel switches, receive the trigger, send the output and control the indicators. I have a couple of small PIC chips to start to play with, but will have to select a more appropriate chip at a later date. I will do this when I am ready to order some of the parts.

image

 

Case wise, I will look to house it in a small desktop instrument case. I am not too concerned about the case size and would prefer something robust as the instrument will travel around with the protection testing kit. Something like the Lux was series from OKW that also has the advantage of a built in battery compartment.

 

I don't like to order cases until I am well into the build stage, as I have a very easy habit of buying cases that prove to be too small for the project.

 

 

 

 

 

 

 

Next job will be to produce the schematic, but first, I have an old PIC projects book I am currently back to reading and a PICkit 3, that I purchased some considerable time ago for a project that got shelved. This will hopefully now get some use if I can connect it up and get it working.

 

image

 

I may be gone for some time.............

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +2
    Donald, Your plans are coming along nicely. This looks pretty good. I would just make a couple of suggestions, mostly relating to the usage of li-ion batteries (should you decide to go in that direction…
  • jw0752
    jw0752 over 8 years ago +2
    Hi Donald, This looks like a very interesting build. I hope you continue to post it so we can all enjoy your success. John
  • genebren
    genebren over 8 years ago in reply to three-phase +1
    Donald, When boosting the voltage to 5V, the battery current drawn by the boost circuit is greater than the current delivered to the 5V load. It is very similar to almost any conversion, power out = power…
Parents
  • genebren
    genebren over 8 years ago

    Donald,

     

    Your plans are coming along nicely.  This looks pretty good.  I would just make a couple of suggestions, mostly relating to the usage of li-ion batteries (should you decide to go in that direction).

    My experience is that it is much simpler to design a single cell system and use a boost circuit to get your 5V (in place of your regulator).  In addition, you would want to add a monitor/shutdown circuit that would turn the boost off iv the battery voltage drops to 2.5V (or 2.7) to protect the battery.

    Good luck on your project!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 8 years ago in reply to genebren

    Many thanks Gene,

     

    I have not used a boost circuit before, being a 3 wire electrician, when a voltage is stepped up, the current goes down, is this also the case with a boost circuit?

     

    I need to run some tests on the SCITS to see what current is drawn on the digital inputs when they are triggered to see what I need to be able to supply.

     

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 8 years ago in reply to genebren

    Many thanks Gene,

     

    I have not used a boost circuit before, being a 3 wire electrician, when a voltage is stepped up, the current goes down, is this also the case with a boost circuit?

     

    I need to run some tests on the SCITS to see what current is drawn on the digital inputs when they are triggered to see what I need to be able to supply.

     

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to three-phase

    Donald,

     

    When boosting the voltage to 5V, the battery current drawn by the boost circuit  is greater than the current delivered to the 5V load. It is very similar to almost any conversion, power out = power in x efficiency. Typically these boost converters run at efficiencies around 90% (or greater).  You would need to understand your 5V max load to select the right part.  In addition to the converter, the boost circuit usually needs a small inductor and two capacitors.

     

    Assuming a current drawn of 100ma @ 5V (0.5W), the current draw from the battery would be between 205ma (Vbat = 2.7V) and 132ma (Vbat = 4.2V).

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 8 years ago in reply to genebren

    Many thanks for your advice Gene, I will do a bit of testing to see how much current is drawn on the inputs. I cannot find much technical information on the binary inputs from the manufacturer. When set to voltage measurement, they have a 1MOhm input impedance, so hopefully the current draw should be quite low.

     

    Kind regards