Products
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
Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Simple I/O control using PYNQ
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Fred27
  • Date Created: 12 May 2020 8:55 PM Date Created
  • Views 6200 views
  • Likes 7 likes
  • Comments 24 comments
  • pynq-z2
  • pynq
  • pynqstarter
Related
Recommended

Simple I/O control using PYNQ

Fred27
Fred27
12 May 2020

I really enjoyed the first PYNQ workshop and also an Embedded Hour session that was a few days later. I thought the best use of time would be to get my head around all the ways you can control the IO on the PYNQ-Z2 board.

 

We were given an example of using the pattern generator and trance analyzer to toggle a few pins and monitor what happens, but the example given just took some pin names and magically knew how to access them. This example for instance generated output on D0-D2 and monitored D17-D19:

image

 

This great if you just want the pattern generator to do the work for you, but what if you want some finer control over these pins? What if you want to communicate with a device over I2C?

 

There are overlays for a fixed set of Pmod devices but I wanted to go a little off the beaten track and use another device. Well, for this you need to jump into another area of your Jupyter notebook and get familiar with the Microblaze side of things.

 

Microblaze

Microblaze is an interesting concept. Programming FPGAs is a world away from the probably more familiar world of microcontrollers. FPGAs are really powerful but there are times when a microcontroller is better suited to the job. Now, the Zynq device on the board already has an ARM microntroller inside it, but that's busy running Linux and doing all the stuff that makes PYNQ possible. What if you just need a little bit of precedural microcontroller goodness to help you along? That's where Microblaze comes in. It's a fairly small 16-bit microcontroller that's actually created withing the FPGA fabric.

 

I must admit it took me a while to find my way around the Microblaze abilities of the PYNQ board. There are a few examples but I couldn't actually find any comprehensive documentation. Under the microblaze_programming notebook I found some useful looking sections such as this:

 

image

IO on Arduino headers

However, I decided that I wanted to mess with some pins on the Arduino-style header. There were examples for Microblade targetting PMODA and I found another for the Pi pin headers (using %%microblaze base.RPI) and a bit of guesswork lead me to the following for targetting the pins I wanted and flashing an LED attached to pin A5 of the Arduino header:

image

Now, none of this is complicated, but it required some guesswork. Not really complicated quesswork, but guesswork all the same. Considering how well PYNQ is set up to be self-documenting and easy to work with I found this odd. In particular, I found the the A5 pin is referred to as "19" buried in a comment on this page. Other than that though, it was easy enough to create a Microblaze processor and get it running some simple C code - via a Python-based notebook.

 

I2C on Arduino headers

After finding an I2C example on the Raspberry Pi headers, I thought it should be reasonably simple adapting this to some different pins. Unfortunately this wasn't the case. This is the code I came up with, and despite trying lots of variations, whenever I executed the code, it hung. I couldn't see any way to find where it had hung without some clunky pin toggling either.

image

 

Take off and nuke it from orbit. It's the only way to be sure.

To make things more frustrating it seemed impossible to rest things without powering off the board. Killing the PYNQ Kernel had no effect. In fact, even if you have successful Microblaze code running (such as blinking and LED in an endless loop) there appears to be no way to stop it.

 

Sorry this blog is not a success story, but I believe in writing things up as they are - good or bad. I'm going to keep on plugging away at this when I get the chance between work and other projects.

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 6 years ago in reply to jc2048 +2
    The 0x28 came from some working code from another device (Azure Sphere). That was a great suggestion to use 0x50 but in this case 0x28 was correct. I know some I2C libraries expect the address specified…
  • weiwei2
    weiwei2 over 6 years ago +1
    i am also trying to achieve similar, although i am still testing with other PYNQ board
  • Fred27
    Fred27 over 6 years ago in reply to weiwei2 +1
    I hope my partial success is some help to you. If you make any further progress, be sure to let us know.
Parents
  • kevin_v
    kevin_v over 6 years ago

    Thank you Fred to putting this up.

     

    For 2 weeks i have been trying to figure out how to uses the Arduino component on the pynq board. The last 4 days i was trying to get an eternal LED to turn on but couldn't figure out how to select the gpio i wanted and how to output from it.

     

    You have ended my suffering. Once again thank you!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to kevin_v

    If you wanted to, you should also be able to control the GPIO ports more directly from the PS as opposed to using the MicroBlaze Arduino Input/Output processor (IOP).

     

    If you look at the Xilinx PYNQ Workshop session 4 notebooks here:

    https://github.com/Xilinx/PYNQ_Workshop/tree/master/Session_4

    then you will find examples for PS GPIO, AXI GPIO and MMIO.

    (I've just been experimenting with the MMIO method myself after the 2nd PYNQ workshop session.)

     

    These examples assume that you have appropriate PL overlay loaded in order to connect to the required IO ports on the PYNQ-Z1/Z2 boards.

     

    I believe that you should also be able to do this even more directly using MIO as opposed to Extended MIO (EMIO) to connect the PS directly to the external package pins without any PL in the middle, however the documentation gets a little bit thin around this area.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 6 years ago in reply to kevin_v

    If you wanted to, you should also be able to control the GPIO ports more directly from the PS as opposed to using the MicroBlaze Arduino Input/Output processor (IOP).

     

    If you look at the Xilinx PYNQ Workshop session 4 notebooks here:

    https://github.com/Xilinx/PYNQ_Workshop/tree/master/Session_4

    then you will find examples for PS GPIO, AXI GPIO and MMIO.

    (I've just been experimenting with the MMIO method myself after the 2nd PYNQ workshop session.)

     

    These examples assume that you have appropriate PL overlay loaded in order to connect to the required IO ports on the PYNQ-Z1/Z2 boards.

     

    I believe that you should also be able to do this even more directly using MIO as opposed to Extended MIO (EMIO) to connect the PS directly to the external package pins without any PL in the middle, however the documentation gets a little bit thin around this area.