Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Smart Home: Party Ball, Kind of
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: djfraz
  • Date Created: 1 Jun 2018 7:44 PM Date Created
  • Views 1647 views
  • Likes 5 likes
  • Comments 7 comments
Related
Recommended

Smart Home: Party Ball, Kind of

djfraz
djfraz
1 Jun 2018

So the I have gotten the code to function as intended. So now for the hardware.

 

I started by depopulating the pcb that came with the original product. My original plan was to make an acrylic version with just the mounting holes, but realise if i flipped the pcb over, it would have the same effect.

imageimageimage

The only component which gave me any trouble was the inductor, the contacts were soldered under the ferrite core, and in the end i just snapped it off, as i was not worried about keeping the PCB traces.

 

For the neopixels iI purchased some breadboard friendly ones from ebay (same price as most online retailers and no shipping cost) and simply hot glued them into place. The was to be able to replace them if needed.

 

And that is really all the hardware, the motor was connected through a transistor with diode protection. And it was ready for its first test.

 

image

Everything appeared to be working, so I turned off the lights, closed al the blinds ready to see it in the dark, and;

image

The picture has done it some justice here, but it is very dim in person. and for comparison, I purchased another of the original for comparison, and turned them on together. All the light is from the original. I have included a short video to greater illustrate the point, this one was with the lights on.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
image

 

 

 

It is fair to say that I am a bit disappointed at the moment. I though that the Neopixels would be bright enough, any of Adafruit videos show them being very bright.

 

I think the next step is going to be looking for higher powered RGB Addressable LEDs, somewhere in the region of 1W, as i think that is the value of the ones in the original. If anyone know where i could get my hand on them it would be much appreciated. I was considering buying normal 1W RGB LEDs and the Driver IC WS2811, but i think they are surface mounted and I am not wanting to go down the road of getting a custom PCB made for this.

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 8 years ago +3
    Hi Duncan, I wouldn't say your design is a fail as titled in your video. It looks good, but from reading your article you are disappointed with the brightness - maybe this is just version 1 in development…
  • genebren
    genebren over 8 years ago +3
    Duncan, There is no such thing as a failure, if you keep trying (then it is just an experiment). You have made some great steps towards your goal, so keep moving forward. There are some good suggestions…
  • djfraz
    djfraz over 8 years ago in reply to 14rhb +3
    It has definitely been V1.0, it was not so much a fail of the design, more of my expectations. The process of designing and programming this has been rewarding in the knowledge i have gained, which i will…
Parents
  • fmilburn
    fmilburn over 8 years ago

    Hi Duncan,

     

    How many Neopixels are there? If not too many, I bought some RGB LEDs a while back mounted on aluminum star shaped PCBs.  Each LED is supposedly rated for 1W so 3W total.  I never took it all the way to 3w and suspect it might need a heat sink if you did.

    I bought mine from a small reseller in the US no longer in business but you can get them from the usual Chinese locations - just search for rgb 3W or similar.  There are also RGBW.  I don’t see them on Newark.  I used them on a project that also had Neopixels and they are considerably brighter.  The R,G, and B LED pins are separate on large pads and easy to solder.  I controlled current with resistors.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to fmilburn

    It looks (from Duncan's previous tear-down) like the case of that product is the heatsink. It would be much better with a metal-clad board, but it's nice that the heat is radiated off the exterior and not internally into the case.

     

    It's possible, looking at the board, that the person who originally designed it intended it to have an mcb and it's been subsequently cheapened (probably on the basis that something that runs for about an hour on three AA batteries probably won't be run for anything like 60,000 hours to test the LED lifetime).

     

    Once you get to 1W, there's a good case for a constant-current driver rather than resistors.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 8 years ago in reply to fmilburn

    It looks (from Duncan's previous tear-down) like the case of that product is the heatsink. It would be much better with a metal-clad board, but it's nice that the heat is radiated off the exterior and not internally into the case.

     

    It's possible, looking at the board, that the person who originally designed it intended it to have an mcb and it's been subsequently cheapened (probably on the basis that something that runs for about an hour on three AA batteries probably won't be run for anything like 60,000 hours to test the LED lifetime).

     

    Once you get to 1W, there's a good case for a constant-current driver rather than resistors.