Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs The Art of Noise
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 22 May 2021 10:41 AM Date Created
  • Views 8481 views
  • Likes 14 likes
  • Comments 36 comments
  • transistor
  • 2n3904
  • noise
  • analog
Related
Recommended

The Art of Noise

jc2048
jc2048
22 May 2021

22nd May 2021

 

image

 

I've just been playing with a very simple noise generator and that's the result.

The digital phosphor of the oscilloscope presents multiple traces of the waveform as though it were sketched with a pencil or crayon.

 

In case it's of any interest, here's the circuit:

 

image

 

The internet is full of variations, with either a Zener, reverse-biased LED, or reverse-biased base-emitter junction as the avalanche 'noise diode'.

 

image

 

 

For these traces I used a reverse-biased base-emitter junction (the transistor on the left with two pins connected - the other transistor is working as a common-emitter amplifier)

and it produced a very good level of noise out on a 12V supply.

 

At lower frequencies (the scope is AC-coupled for these), the noise looks quite noise-like. Like this:

 

image

 

but if I go back to the start and show you a single trace of the first waveform, we see this

 

image

 

so we're now looking at a time scale where we can see the avalanching stopping and starting.

 

Update 4th June 2021

 

What started as a throwaway blog about an interesting/amusing waveform seems to have taken on a life of its own.

 

Thanks for all the useful comments below. They've had the useful effect of forcing me to rethink some of this.

 

1. The original circuit that I copied had an integrator (low-pass filter) in the feedback of the common-emitter stage

[the 27k and the 10uF] to set the DC bias voltage. That means that the resulting overall transfer characteristic will

be high-pass [the inverse]. I should have considered that a bit more at the time. If I simulate it with this following

circuit (I've substituted a simple signal generator, with an 8V DC offset on it, for the 'noise diode' which is the input to the circuit)

 

image

I get this for the response

 

image

That won't be entirely right - the simulation is small-signal and the generator is working large-signal - but it lets us

see in a rough way what's happening and understand it in general terms. It falls off from a few hundred Hertz downwards.

That means I'm going to see very little of the low frequency noise as the circuit will integrate it away. Indeed, if I had wanted

to use the generator circuit for audio, it would probably have been better if I had moved the low end cut-off down by

another decade [100uF might do instead of the 10uF].

 

At the top end, that plot shows quite nicely that the response is determined largely by the amplifier transistor running

out of steam and that will depend to some extent on the individual transistor.

 

2. In my reply to Shabaz in the comments, I suggested that seeing the noise decline as I filtered it with the 'scopes

noise filtering meant that it wasn't white noise. That is quite wrong and I need to correct it. Since random noise level

is a function of bandwidth, if I restrict the bandwith, I lessen the noise seen. That doesn't mean that it's necessarily

'white' noise [equal power per unit of bandwidth], but it most certainly doesn't mean the opposite [that it's not].

 

In Motchenbacher and Fitchen, they suggest that avalanche noise is white but that there is also excess noise

in the form of multistate noise that is predominently l/f. This is in a section comparing the noise performance

of zener and avalanche diodes, though I presume a reverse-biased base-emitter junction is similar.

  • Sign in to reply

Top Comments

  • geralds
    geralds over 5 years ago in reply to shabaz +6
    shabaz wrote: Hi Jon, Very interesting blog post, I had not known noise could be generated at these levels with such a simple circuit! Yes, that's an age-old way of creating noise. Simply operate a transistor…
  • fmilburn
    fmilburn over 5 years ago +5
    By coincidence I became interested in these circuits recently, mostly with the idea of making a random number generator. Horowitz and Hill have one in the Art of Electronics but I also found a good article…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to shabaz +5
    My Tektronic TBS2xxx scope had a reasonable spectrum display. Not magic, but (almost) workable in that frequency range. I gave it away to a makerspace here in Belgium, so that avenue is closed. A SA is…
Parents
  • shabaz
    shabaz over 5 years ago

    Hi Jon,

     

    Very interesting blog post, I had not known noise could be generated at these levels with such a simple circuit!

    I wish I could remember now how it was implemented (it too was analog) but in an early job I recall that white noise was deliberately inserted in certain receiver audio paths instead of silence, when there was no received signal, to reassure the user that the system was functioning.

     

    Regarding the Art of Electronics book, I tried copying one of the circuits there, which was for pseudo-random noise, it lends itself well to programmable logic so I used a CPLD for it, here: Pseudo-Random Noise; Using it and How to Create it

     

    I recently bought some flickering LEDs from AliExpress (they are supposed to simulate candlelight) I wonder what algorithm or noise method they are using! I might try to connect a photodiode and capture the output (or the current consumption) someday out of curiosity.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • geralds
    geralds over 5 years ago in reply to shabaz

    shabaz  wrote:

     

    Hi Jon,

     

    Very interesting blog post, I had not known noise could be generated at these levels with such a simple circuit!

     

    Yes, that's an age-old way of creating noise.

    Simply operate a transistor inversely and leave the collector open. Then you have a diode with Miller capacitance in reverse operation.

    The one-transistor amplifier then amplifies the noise with its set operating point, its gain.

    The chip temperature also comes into play here. Because not every transistor is suitable as a good noise generator (all noise, but not equally good).

    It is resistance noise from the differential resistance of the transistor, not from a linear resistance like the simple resistor.

     

    If I found the old book, in that this was explained I will post here. Creating noise is a fine thing because you can learn a lot lot from each of that used electronics parts.

     

    I wish I could remember now how it was implemented (it too was analog) but in an early job I recall that white noise was deliberately inserted in certain receiver audio paths instead of silence, when there was no received signal, to reassure the user that the system was functioning.

     

    image Yes - I used it as a test method in the 1970s and 1980s to "whistle through" an amplifier.

    Most of the time you do this with an RF amplifier. You then use it to set the filters, e.g. the IF on a radio, or two-way radio, I did that.

    A second Method is with my finger, the hum signal helps with this.

    50Hz "brummmmm" and I already know whether the amplifier is working, or somewhere, for example. Ground loops, or cable breaks, or whether a transistor is working properly, etc ...

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • geralds
    geralds over 5 years ago in reply to shabaz

    shabaz  wrote:

     

    Hi Jon,

     

    Very interesting blog post, I had not known noise could be generated at these levels with such a simple circuit!

     

    Yes, that's an age-old way of creating noise.

    Simply operate a transistor inversely and leave the collector open. Then you have a diode with Miller capacitance in reverse operation.

    The one-transistor amplifier then amplifies the noise with its set operating point, its gain.

    The chip temperature also comes into play here. Because not every transistor is suitable as a good noise generator (all noise, but not equally good).

    It is resistance noise from the differential resistance of the transistor, not from a linear resistance like the simple resistor.

     

    If I found the old book, in that this was explained I will post here. Creating noise is a fine thing because you can learn a lot lot from each of that used electronics parts.

     

    I wish I could remember now how it was implemented (it too was analog) but in an early job I recall that white noise was deliberately inserted in certain receiver audio paths instead of silence, when there was no received signal, to reassure the user that the system was functioning.

     

    image Yes - I used it as a test method in the 1970s and 1980s to "whistle through" an amplifier.

    Most of the time you do this with an RF amplifier. You then use it to set the filters, e.g. the IF on a radio, or two-way radio, I did that.

    A second Method is with my finger, the hum signal helps with this.

    50Hz "brummmmm" and I already know whether the amplifier is working, or somewhere, for example. Ground loops, or cable breaks, or whether a transistor is working properly, etc ...

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +6 Vote Down