Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs The Complete 8 Bit ALU
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: timswift
  • Date Created: 13 Nov 2016 6:31 PM Date Created
  • Views 2376 views
  • Likes 3 likes
  • Comments 7 comments
  • transistor
  • alu
  • computer
  • diy
  • cpu
Related
Recommended

The Complete 8 Bit ALU

timswift
timswift
13 Nov 2016

image

I finished the ALU (all 8 bits) and the test-board yesterday. It contains 355 transistors without the test board.

In all it took less then two days to construct and trouble-shoot (not including the small boards).

It is interesting to note that the ALU only had one short while the test board had two LED's soldered in backwards and a short.

 

The back side of the ALU;

image

The 34 pin connector is wired as below;

image

The six functions are not encoded so if more then one is selected at a time the functions are calculated and the the results are OR'd together

(I don't think this property has a practical use).

 

Here is the test-board (just light's and switches);

 

image

 

And finely the block diagram;

image

 

Tim

  • Sign in to reply

Top Comments

  • andycrofts
    andycrofts over 9 years ago in reply to sek4321 +1
    I, years ago worked on a Spectrum Analyzer, using the FFT algorithm. 44-bit microcode instruction word, directly operating shift registers, ALU's etc. Total memory 44-bit by 4-kilobyte Here's a piccie…
Parents
  • clem57
    clem57 over 9 years ago

    A great job and surprisingly quick too. Where did the design come from?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 9 years ago

    A great job and surprisingly quick too. Where did the design come from?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • timswift
    timswift over 9 years ago in reply to clem57

    The six functions come from 6502 microprocessor the only difference is that on the 

    6502 the inversion is done outside of the ALU.

    after the functions were determined I simply used a MUX to select the proper function and carry out.

     

    Another clever feature of the 6502 is addition and subtraction is always done with the carry in which is set beforehand (if desired).

     

     

    Tim