Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs The Gold of the Fool and the Whiskers of the Cat
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 13 Jun 2017 1:53 PM Date Created
  • Views 3091 views
  • Likes 12 likes
  • Comments 17 comments
Related
Recommended

The Gold of the Fool and the Whiskers of the Cat

jc2048
jc2048
13 Jun 2017

Back in February, I visited one of the small museums that exist in the town where I

live. It's a natural history museum and is based in an old church. It's a lovely

place to visit, with lots of curious things to look at. In the shop, on the way out,

there was a basket with small chunks of rocks and minerals for sale and I bought a

small piece of 'fool's gold' (iron pyrites); I figured that an old fool like me

deserved a piece of gold to treasure.

 

image

 

What I didn't know back then and have only just discovered is that iron pyrites is

a semiconductor (thank you, Wikipedia!) and in the old days was sometimes used as

the 'crystal' in a point-contact diode (for demodulating radio signals in a crystal

set).

 

Well, I thought, that deserves an experiment. So here is my attempt to make a

point-contact diode, and it turned out to be surprisingly easy. I simply broke one

of the small cubes away and held it in one clip of a 'helping hand' contraption.

 

image

 

That clip I connected to the ground of a signal generator. The drive from the

generator I fed through a 10k resistor to a piece of wire-wrap wire which I arranged

to scrape across the surface of the cube. My scope then measured the output from my

improvised diode.

 

image

 

A little movement of the wire and I soon found a spot that rectified nicely [I was just

so surprised - I really didn't think that this was going to work].

 

image

 

The forward voltage looks to be a little over a volt. That's much higher than a

silicon metal-junction diode (a Schottky diode).

 

And that's it. No need to melt silica in an oven and grow it into a crystal with

99.99-whatever % purity. Instead, an instant semiconductor straight from nature.

 

Do I get a cat badge for this foolishness?

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 9 years ago +6
    The "radio" based on the crystal was the absolutely first stuff I have done when I was about 10 y.o. Synth was based on the semiconductor crystal (it was the early '70 so these stuff was not difficult…
  • jc2048
    jc2048 over 9 years ago in reply to shabaz +6
    Here's a ZN414 radio I built soon after they launched it (the ZN414 is the part that looks like a transistor, even though it's an IC). Tuning cap was a modified trimmer. Power was a small hearing-aid battery…
  • rachaelp
    rachaelp over 9 years ago +5
    Very impressive. Whatever made you think of doing this? I don't have a badge, but you can be awarded Top Cat of the day if you like?
Parents
  • dougw
    dougw over 9 years ago

    Awesome. I had no clue this was possible.

    Of course you know we are going to be asking if a transistor is possible....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to dougw

    I don't understand why it works like this. When they did the work that lead to the original point-contact transistor [after failing to build themselves a FET], they investigated point-contact diodes (the physics of how they worked) and I seem to remember they came to the conclusion that what was happening was that metal ions were diffusing into the crystal and creating a doped area. But that wasn't what happened here - it was instant as soon as I found a good spot. The good part wasn't the smooth face of the cube but an area where it was broken, so it may be where it has already reacted with some other material.

     

    I didn't think about the transistor until I was out walking after posting the blog. I imagine the answer is yes, but mechanically it would be difficult - the wires have to be very, very close to get a transistor action going - so I don't think I'll be doing it with my lash-up any time soon.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 9 years ago in reply to dougw

    I don't understand why it works like this. When they did the work that lead to the original point-contact transistor [after failing to build themselves a FET], they investigated point-contact diodes (the physics of how they worked) and I seem to remember they came to the conclusion that what was happening was that metal ions were diffusing into the crystal and creating a doped area. But that wasn't what happened here - it was instant as soon as I found a good spot. The good part wasn't the smooth face of the cube but an area where it was broken, so it may be where it has already reacted with some other material.

     

    I didn't think about the transistor until I was out walking after posting the blog. I imagine the answer is yes, but mechanically it would be difficult - the wires have to be very, very close to get a transistor action going - so I don't think I'll be doing it with my lash-up any time soon.