Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs The Gold of the Fool and the Whiskers of the Cat
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 13 Jun 2017 1:53 PM Date Created
  • Views 3072 views
  • Likes 12 likes
  • Comments 17 comments
Related
Recommended

The Gold of the Fool and the Whiskers of the Cat

jc2048
jc2048
13 Jun 2017

Back in February, I visited one of the small museums that exist in the town where I

live. It's a natural history museum and is based in an old church. It's a lovely

place to visit, with lots of curious things to look at. In the shop, on the way out,

there was a basket with small chunks of rocks and minerals for sale and I bought a

small piece of 'fool's gold' (iron pyrites); I figured that an old fool like me

deserved a piece of gold to treasure.

 

image

 

What I didn't know back then and have only just discovered is that iron pyrites is

a semiconductor (thank you, Wikipedia!) and in the old days was sometimes used as

the 'crystal' in a point-contact diode (for demodulating radio signals in a crystal

set).

 

Well, I thought, that deserves an experiment. So here is my attempt to make a

point-contact diode, and it turned out to be surprisingly easy. I simply broke one

of the small cubes away and held it in one clip of a 'helping hand' contraption.

 

image

 

That clip I connected to the ground of a signal generator. The drive from the

generator I fed through a 10k resistor to a piece of wire-wrap wire which I arranged

to scrape across the surface of the cube. My scope then measured the output from my

improvised diode.

 

image

 

A little movement of the wire and I soon found a spot that rectified nicely [I was just

so surprised - I really didn't think that this was going to work].

 

image

 

The forward voltage looks to be a little over a volt. That's much higher than a

silicon metal-junction diode (a Schottky diode).

 

And that's it. No need to melt silica in an oven and grow it into a crystal with

99.99-whatever % purity. Instead, an instant semiconductor straight from nature.

 

Do I get a cat badge for this foolishness?

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 9 years ago +6
    The "radio" based on the crystal was the absolutely first stuff I have done when I was about 10 y.o. Synth was based on the semiconductor crystal (it was the early '70 so these stuff was not difficult…
  • jc2048
    jc2048 over 9 years ago in reply to shabaz +6
    Here's a ZN414 radio I built soon after they launched it (the ZN414 is the part that looks like a transistor, even though it's an IC). Tuning cap was a modified trimmer. Power was a small hearing-aid battery…
  • rachaelp
    rachaelp over 9 years ago +5
    Very impressive. Whatever made you think of doing this? I don't have a badge, but you can be awarded Top Cat of the day if you like?
Parents
  • dougw
    dougw over 9 years ago

    This whole topic is quite intriguing.

    Now you got us thinking ..... what is the breakdown voltage? If you crank up the voltage, does it hang in there?

    Not to put you to any trouble or anything, but you might be onto something that could have real applications....image

    That smooth transition to cut-off reminds me of some holy grail audio characteristics.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to dougw

    I shouldn't have said it was rectifying before because it was actually set up as a diode clamp.

     

    Here it is as a rectifier with the 10k resistor as the load (yellow trace input, blue trace output). The signal generator only goes to 20V pk/pk, but it gives an idea of how it behaves with higher voltages.

     

    image

     

    To get a better idea of what it's doing, this one is with a triangular waveform. Rather than a true diode, it's more that it becomes non-linear in the reverse direction.

     

    image

     

    Finally, this is at 1MHz where it almost performs as well as my cheap waveform generator.

     

    image

     

    So, it's not much of a diode and it's very sensitive to mechanical vibration. I can now see why people who used cat's whiskers ended up spending all their time fiddling around with the things.

     

    The idea of selling fool's gold to audio cranks does appeal, though.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 9 years ago in reply to dougw

    I shouldn't have said it was rectifying before because it was actually set up as a diode clamp.

     

    Here it is as a rectifier with the 10k resistor as the load (yellow trace input, blue trace output). The signal generator only goes to 20V pk/pk, but it gives an idea of how it behaves with higher voltages.

     

    image

     

    To get a better idea of what it's doing, this one is with a triangular waveform. Rather than a true diode, it's more that it becomes non-linear in the reverse direction.

     

    image

     

    Finally, this is at 1MHz where it almost performs as well as my cheap waveform generator.

     

    image

     

    So, it's not much of a diode and it's very sensitive to mechanical vibration. I can now see why people who used cat's whiskers ended up spending all their time fiddling around with the things.

     

    The idea of selling fool's gold to audio cranks does appeal, though.