Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs TI Hercules LaunchPad RM42x: Supply DC Source 20v/50A Part 1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: martinvalencia
  • Date Created: 11 Jun 2015 10:28 AM Date Created
  • Views 1827 views
  • Likes 4 likes
  • Comments 6 comments
  • lcd
  • amper
  • la
  • ampl
  • amplification
  • het
  • rm42x
  • 125-p/sp4
  • dc
  • hercules
  • sp:texas_instruments
Related
Recommended

TI Hercules LaunchPad RM42x: Supply DC Source 20v/50A Part 1

martinvalencia
martinvalencia
11 Jun 2015
Leaching

Extractive Metallurgy

The process used in metallurgy, mainly for working oxidized ores. From a time now leaching of copper sulfide minerals it is done through bacterial leaching processes.

In the case of leaching of gold ores (oxides) design of the pads they are according to the morphology of the area, according to details that we will begin to select the type of pad, either reusable pad, for expandable or leaching valley type (in case of Pierina).

 

Practical Applications

Industrially leaching is used to prepare powders, for this drug (generally a medicinal plant) is sprayed is taken, and mixed with menses (alcohol) placed in a leachate and left macerating the required time.

Also it can be said leaching treatment of mineral concentrates and other materials containing metals, leaching is performed by a wet process with acid soluble minerals dissolved and recovered in a pregnant leach solution. Of practical use in mining by cyanidation of gold and other minerals.

 

 

Introduction:

 

Developing a source for purposes of working with copper plates, which act as cathodes and performing leaching, so it requires high currents in DC, for this case a DC source having a current output maximum of 50 is requested amperes y 20 volts we had many problems to implement a protection circuit and display data on the LCD.

 

Schematic:

image

                                                                                                                                  Power Board

image

                                                                                                              Control Board

Album Pics:

 

 

transformer and power transistors
image

 

Test power resistors, each of 2 ohm
image

 

 

Fisrt Try (MSP430G)

 

A first attempt with the MSP430 Texas Instruments was performed to control LCD and displayar current measurement and votaje on screen, but we find the problem that it was necessary to calculate an RMS TRUE and microcontroller had no sufiente memory ,so I decided to use Hercules RM42x, with excellent memory and designed for Industrial applications.

image

 

MSP430G
image

 

 

True RMS (Vol and Amp):

 

Somehow the current and voltage, given by the switching transistors was not linear as expected, making for a more accurate measurement is true RMS decided by applying a programming.

 

Hercules RM42x (100MHz/32bits)
image

 

image

 

Control Power by transistor

image

image

 

image

 

 

Current sensor (Current Transducer LA 125-P/SP4)

 

image

image

Last update here:
TI Hercules LaunchPad RM42x: Supply DC Source 20v/50A Part 2
  • Sign in to reply

Top Comments

  • martinvalencia
    martinvalencia over 11 years ago in reply to DAB +2
    it's just like Jan Cumps says, is for the mining industry; where high current flow is used to galvanize metals, but also has other applications but only mining applications. the circuit is a simple font…
  • DAB
    DAB over 11 years ago +1
    Nice detailed post. Is this circuit for a general design or do you have a specific application in mind? DAB
  • balearicdynamics
    balearicdynamics over 11 years ago +1
    Interesting and well detailed. Bookmarked
Parents
  • DAB
    DAB over 11 years ago

    Nice detailed post.

     

    Is this circuit for a general design or do you have a specific application in mind?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 11 years ago in reply to DAB

    it's just like Jan Cumps says, is for the mining industry; where high current flow is used to galvanize metals, but also has other applications but only mining applications.

    the circuit is a simple font but the transformer and the  wire were designed to withstand the environments of acid gases and other conditions; Today we finish the box safety

     

    image

     

    image

    to finish the work, we still require a few more days, thank you very much for your interest and greetings to you all!

     

    Martin Valencia

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago in reply to martinvalencia

    Hi Martin,

     

    I am very interested in your leaching process.

     

    I have been doing research into the atomic interactions of various materials and I have defined a new atomic model to analyze these types of problems.

     

    Do you have any documents or websites you could recommend where I can get some detailed data on the processes used?

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 11 years ago in reply to DAB

    wow, a thousand apologies for the delay, the company I work alone received specifications for the design of the fountain, in no time we had some theoretical material - chemical, the contractor "CERRO VERDE" , it is owns this type of information and the company I work for specializes in the design of industrial electronics, so we have no access to this type of information.

    thank you very much for your interest and apologize!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • martinvalencia
    martinvalencia over 11 years ago in reply to DAB

    wow, a thousand apologies for the delay, the company I work alone received specifications for the design of the fountain, in no time we had some theoretical material - chemical, the contractor "CERRO VERDE" , it is owns this type of information and the company I work for specializes in the design of industrial electronics, so we have no access to this type of information.

    thank you very much for your interest and apologize!