Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Transistors: Switching a Relay Coil
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 6 Feb 2017 11:04 PM Date Created
  • Views 7360 views
  • Likes 6 likes
  • Comments 15 comments
Related
Recommended

Transistors: Switching a Relay Coil

jc2048
jc2048
6 Feb 2017

This blog is a continuation of

 

Transistors: Vce Breakdown

 

and it's probably best to read that one first. The idea for this one came out of helpful observations made by mcb1, dougw, and D_Hersey in the comments, so read those too.

 

I'm going to look in a bit more detail at protecting a bipolar junction transistor switching a relay. In that previous blog, I was using a solenoid as the inductive load, now I'm going to use a real relay. It's a relay intended for automotive use and has a 12V coil with a resistance of 87ohms and an inductance (at rest) of 93mH. The NO (normally open) contacts can switch 20A.

 

image

 

When the relay is energised, the current through the coil will be approximately 11.8V/87ohms = 136mA.

 

1N4148 diode across coil

 

First off, I'm going to use a single 1N4148 signal diode to protect the transistor.

 

image

Here's the collector waveform at the time the transistor turns off and releases the relay coil. With a low-capacitance signal diode everything happens very fast. You can see that it's so fast that the voltage overshoots a little before the diode turns on and starts clamping it to a diode drop above the rail. The turn-on time looks to be a few nanoseconds, which is in the right sort of area for a diode like this.

 

image

 

Next is the collector voltage [yellow trace], along with the current through the protection diode [blue trace], on a much longer timescale.  The collector voltage sits at 12V plus the diode drop for about 14mS before most of the energy in the relay's coil is dissipated and the collector comes to rest back at the supply voltage. The current starts at the energised current and diminishes. There's a mysterious increase in the current halfway down the slope which wasn't there with the solenoid that I used in the previous blog.

 

image

 

Finally, here's the current and the contact waveform [I've only got a 2-channel scope, otherwise I'd show all of these together] so we can see at what point the relay is releasing the contact. Now that increase makes more sense. It looks like it's the reaction to the contact being released, breaking the magnetic circuit, and the coil having to adjust to a somewhat lower inductance. Something that's interesting is that the relay manufacturer appears to have engineered it so that the contacts don't lift off until about half a mS after the release, presumably in an effort to minimise the problem that mcb1 drew my attention to. It still looks a bit uncomfortable with a single signal diode doing the protection, though.

 

image

 

1N4004 diode across coil

 

This circuit is the same as the last except I've swapped the 1N4148 for a 1N4004 rectifier diode.

 

Here are the waveforms (same order as before):

 

image

 

image

 

 

image

 

The rise time is slower than the signal diode, because the rectifier diode has more capacitance that has to be charged, but other than that they're very similar in how they dissipate the coil's energy. That's because the forward voltages are fairly similar and they'll dissipate the coil's energy at a similar rate.

 

1N4148 and 12V zener across coil

 

image

This one is a bit different. Now I've got a signal diode and a 12V zener across the coil. The signal diode blocks the zener when it [the zener] is forward-biased and would otherwise short the coil. In theory this should be better than a single diode because the coil voltage will increase to 12.6V and the initial dissipation will be 12.6V x 130mA = 1.64W rather than 0.6V x 130mA = 78mW with a single diode.

 

Here are the waveforms

 

image

 

image

 

image

 

 

The rise time now looks a bit odd. To explain it, you'd have to think about the various device capacitances and how they get charged.

 

This is much better. Most of the energy from the coil is dissipated after 2mS and, though the contacts drop out at the same current level as before, by the time the contacts move we can hardly see the result of the change of inductance on the small current that the coil is left driving at that point.

 

MOV to ground

 

image

 

MOVs (metal oxide varistors) are used for clamping and I was feeling curious what one would do here, so I thought I'd try one. I expected that it might behave similarly to a zener, but wasn't sure. [I've used a NTC thermistor symbol on the circuit - pretend it's a MOV.]

 

image

 

image

 

image

 

The rise time is slow - the datasheet says over 2nF for the capacitance, so that's not a surprise. The clamping voltage varies as the current reduces, so it doesn't clamp as hard as a zener would, but it's not too far off what a zener does.

 

1N4148, 12V zener and 47R resistor across coil

 

image

This came from a suggestion by Doug that I consider a resistor to help dissipate the coil energy. If I put the resistor across the signal diode and the zener, then the transistor would have to drive it, so I put it across just the zener.

 

image

 

The problem here is that the resistor (because the voltage declines as the current goes down) hogs the discharge leaving the zener with nothing to do and the declining dissipation gives a result that is not a lot better than a single diode.

 

Zener to ground

 

Finally, I tried a single 30V zener to ground.

 

image

 

Here are the waveforms:

 

image

 

image

 

image

 

The zener doesn't have too much capacitance to slow the rise time and doesn't switch as fast as the signal diode, so there's more overshoot. It's probably a bit more than the 4V or so that my scope shows, but nothing too embarassing - the Vce max of the transistor is at least 5 volts above that, even very worst case. With the high terminal voltage, the dissipation is much higher than with the single diodes and it dissipates the coil energy much quicker - most of the energy is out of the coil within a millisecond. It also has the side effect that the contacts release much quicker - the contacts lift off in just under 2mS, compared to over 6mS for the single diodes. Although the kink in the voltage waveform at the point where the contacts start to go over looks alarming, in practice the current is very low and it's not going to be retarding the contact movement [I think the current has reversed at this point and we are looking at the capacitance of the zener discharging through the coil to bring it back to the rail]. Note that, technically, I'm exceeding the ratings for a 1.3W zener; for my experiment it doesn't matter, but for a commercial design you'd need to take a view on what the datasheet limits actually mean. A bonus of the zener to ground is that the device protects the collector from excursions below ground too.

 

That's it for now. I'm not going to look at the kind of snubbers that D_Hersey suggested because it's too involved and this blog is long enough already.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 9 years ago +1
    Very nice side by side comparison of the different approaches with this experiment. This information will be valuable to all of us who like to interface the electronic and mechanical worlds. Thanks for…
  • mcb1
    mcb1 over 9 years ago +1
    Nice work. The one thing that I've not seen is the diode across the transistor. Most of the transistors with back emf have this included, so a comaprison would be great. It may be they add to the release…
  • jc2048
    jc2048 over 9 years ago in reply to mcb1 +1
    I'm not understanding this. Can you draw me a diagram showing how it's arranged and I'll try it?
Parents
  • mcb1
    mcb1 over 9 years ago

    Nice work.

    The one thing that I've not seen is the diode across the transistor.

     

    Most of the transistors with back emf have this included, so a comaprison would be great.

    It may be they add to the release time.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to mcb1

    I'm not understanding this. Can you draw me a diagram showing how it's arranged and I'll try it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jc2048

    jc2048

    Sorry Jon.

     

    Some of the higher powered device have it inbuilt but I need to check which one when I get home.

    This is effectively how they are in the right side of this drawing.

    Image result for transistor with inbuilt diode

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to mcb1

    Are you sure? The diode protects against any negative voltage [which you might get if the coil and any capacitance at the coil-collector node were to ring badly] but doesn't stop the coil increasing the collector voltage to the point where the transistor breaks down [which is what we're trying to protect against], unless it's a high-voltage transistor and the diode breakdown occurs before that of the transistor. In that case, it's better to use a proper zener.

     

    You do sometimes see diode and zener symbols on power MOSFETs that are avalanche-rated, where the device itself can safely break down without permanent damage as long as you stay within the datasheet limits for energy at a particular repetition rate. I'm not familiar with high power stuff, so it's possible the same could apply to some BJTs too (my knowledge of semiconductor fabrication techniques is non-existent, I'm afraid). [In a sense, there's no difference between a diode and a zener - they are both PN junctions that break down - it's just that the zener voltage is precise and the device is constructed to survive, whereas with the diode it's a lottery as to how long it will survive and the only thing you know about the breakdown voltage is that it's above the limit set by the datasheet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jc2048

    Referring to these sorts of mosfets.

    http://www.farnell.com/datasheets/1643166.pdf

    I'm sure I have some other transistor datasheets (at home) that include the diode.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to mcb1

    I think that's just making you aware that the body diode is there [which gives you a current path you may not be expecting if you are using the device for power switching]. It's not making any claims about what happens when that diode breaks down.

     

    I was thinking of this kind of thing

     

    http://www.farnell.com/datasheets/129279.pdf?_ga=1.186747243.298976934.1443043972

     

    here the body diode is designed to avalanche in a controlled way and, in this case, they add a zener symbol. There isn't a lot of consistency - I've seen avalanche-rated parts with no symbol, a diode symbol, or a zener symbol.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jc2048

    jc2048

     

    The various manufacturers do advertise 'integrated protection'.

    As you say it's mostly to protect the device, rather than provide 'active' back emf protection.

     

    I'm still hunting, but I tripped across this which is a good read about some of the devices we use for protection.

    http://www.onsemi.com/pub_link/Collateral/TND335-D.PDF

     

    On Semiconductors have a range of 'protected' mosfets

    ON Semiconductor

     

     

    In an H bridge the only place to add the diode is across the switching devices (unless you want your motor going one way).

    In this situation they provide the necessary protection, either integrated or external.

     

    Apart from switching relays, electric power steering and electronic window controllers are big users of H bridge (or that style) techniques in Automotive use.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago in reply to jc2048

    jc2048

     

    The various manufacturers do advertise 'integrated protection'.

    As you say it's mostly to protect the device, rather than provide 'active' back emf protection.

     

    I'm still hunting, but I tripped across this which is a good read about some of the devices we use for protection.

    http://www.onsemi.com/pub_link/Collateral/TND335-D.PDF

     

    On Semiconductors have a range of 'protected' mosfets

    ON Semiconductor

     

     

    In an H bridge the only place to add the diode is across the switching devices (unless you want your motor going one way).

    In this situation they provide the necessary protection, either integrated or external.

     

    Apart from switching relays, electric power steering and electronic window controllers are big users of H bridge (or that style) techniques in Automotive use.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • D_Hersey
    D_Hersey over 9 years ago in reply to mcb1

    In some configurations, one transistor's parasitic diode protects another.  In the case of unipolar stepper drives the coil pairs autotransformer to the clamp on the transistor on the coil 180 degrees out of phase.  In the H drive it is the other Q in vertical pair

     

    In configurations where one Q is driving one coil, the parasitic diode does not protect from inductive spike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • D_Hersey
    D_Hersey over 9 years ago in reply to mcb1

    If you have back-to-back Zeners or their equivalent, you can clamp across the load