Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Using MikroE Click Boards™︎ with Microsoft Sphere
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: james.flynn
  • Date Created: 12 Jul 2019 3:59 PM Date Created
  • Views 5410 views
  • Likes 16 likes
  • Comments 14 comments
  • azure sphere
  • att
  • mikroe
  • ultra96
  • embedded
  • avnet_product
  • nxp
Related
Recommended

Using MikroE Click Boards™︎ with Microsoft Sphere

james.flynn
james.flynn
12 Jul 2019

Implementing MikroElektronika Click boardTm support on Azure Sphere MT3620

image

 

  • Implementing MikroElektronika Click boardTm support on Azure Sphere MT3620
    • Overview
    • Development Platform
    • Demonstration click-board Repository
    • Demonstration Programs
      • click_demo program
        • Barometer and Temp&Hum click board
        • OLED-B click board
      • flame_demo program
      • lcdmini_demo
      • relay_demo
      • tof_demo
    • Conclusion

 

This blog uses the Azure sphere MT3620 Starter KitAzure sphere MT3620 Starter Kit to implement support for a several MikroE Click boards.  There are actually over 650+ mikroBUS(tm) boards (referred to as click-boards) with all types of sensors (see https://www.mikroe.com/click for a complete list).  For the demonstration programs discussed in this blog, support is limited to the boards listed in the Sensor Evaluation using MikroE Click Boards blog.

 

Overview

The MT3620 Starter Kit was chosen because it supports two MikroE click-board sockets as well as several on-board sensors.  With the variety of possible sensors, the goal was to demonstrate the different I/O interfaces using standard library of ANSI C library functions.  The library I am using supports the following click-boards:

 

  1. BAROMETER ClickBAROMETER Click -- uses the I2C interface for interactions
  2. FLAME ClickFLAME Click -- uses Binary I/O for interrupt input and ADC inputs
  3. LIGHTRANGER ClickLIGHTRANGER Click -- uses the I2C interface.
  4. OLED-B Click OLED-B Click -- uses the SPI and Binary I/O interfaces.
  5. RELAY ClickRELAY Click -- uses Binary I/O interfaces
  6. TEMP&HUM ClickTEMP&HUM Click -- uses the I2C interface
  7. LCD MINI ClickLCD MINI Click -- uses a combination of SPI and Binary I/O interfaces

 

Some click-boards, like the relay-click,  are simple Binary I/O while others, like the LCD Mini click, involve multiple SPI bus and Binary I/O interactions. In the demonstration program discussions, any unique interface attributes will be highlighted. 

 

Development Platform

 

When developing for the Azure Sphere Starter Kit,  a Windows 10 (version 1607 or later) PC with Visual Studio, and the Azure Sphere SDK will be utilized.  Once the development environment is installed the Starter Kit is connected via USB.  The entire development environment is extensively discussed on on the Microsoft web-site (https://docs.microsoft.com/en-us/azure-sphere/app-development/development-environment) but to briefly mention it, you need to ensure that:

 

1. The development PC has GIT installed (https://git-scm.com/book/en/v2/Getting-Started-Installing-Git) so you can retrieve copies of the software.

2. Visual Studio is installed--can be either the Enterprise, Professional, or Community; use version 16.04 or later which can be installed from https://visualstudio.microsoft.com/

3. The Azure Sphere SDK is installed from https://docs.microsoft.com/en-us/azure-sphere/install/install.

 

In earlier releases of the Azure Sphere SDK, not all the capabilities of the MT3620 were exposed in the SDK but over time, additional capabilities have been implemented and released. To get an up-to-date status on what is currently support and what isn't, see the Microsoft support page at https://docs.microsoft.com/en-us/azure-sphere/hardware/mt3620-product-status as some click-boards may use capabilities that are not available.

 

An example of this is the Flame Click. This click-board will generate an interrupt signal when a preset threshold is passed and an analog voltage is passed to an ADC so you can determine the exact level that the IR sensor is detecting.  Only the latest Sphere SDK pre-release has support for the ADC.

 

Another aspect to be aware of is that  when developing software for Sphere you can not use C++ because the Azure Sphere SDK only supports development in C (https://docs.microsoft.com/en-us/azure-sphere/resources/release-notes-1905).  Though Visual Studio does not generate an error if you add C++ source files to an Azure Sphere project, it will not build correctly because the Sphere SDK will not support it.  This is why all the click-board library software is written in ANSI C. 

 

Demonstration click-board Repository

 

To utilize the click-board library, all you need to do is include the repository (https://github.com/Avnet/clickmodules) into your project.  The click-board demo project already has this repository included so it will include the latest version of click-board software. You can obtain the source code by cloning the project using the command:

 

git clone --recurse https://github.com/Avnet/clickboard_demos

 

The '--recurse' part of the command tells github to include the click-board library submodule.  Without it, the latest version of that submodule/library will not be pulled and the project will fail to build. 

 

Demonstration Programs

 

click_demo program

The 'click_demo' project can exercise three of the click boards--the Barometer Click, Temp&Hum Click, and OLED-B Click.

 

Barometer and Temp&Hum click board

Default operation is to utilize the Barometer and Temp&Hum clicks.  You can install these two click-boards in any order you desire because the attached boards are queried to determine who is present on the board.   When the demonstration program starts, it queries for each potential click-board and if the response is correct, that board is signaled as present and utilized with output being routed to the Visual Studio output window.

 

image

 

OLED-B click board

The OLED-B click board must be mounted in Slot #1 of the Starter Kit.  This is because Binary I/O control is tied to specific pins associated with Slot #1.  The SPI bus is routed to both sockets but the Binary I/O's are unique for each socket.  Additionally, the startup command line arguments (in app_manifest.json) must be modified to signal to the program to run the OLED-B test by setting "CmdArgs" to "-t".  After this is done and the program compiled/run, the OLED-B will display program execution:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

flame_demo program

The software for this demonstration program assumed the Flame Click board is inserted into Slot #1.  The click board only requires access to the AN (analog) and INT (interrupt) pins but I used slot #1 when developing it.  Additionally, though the Sphere SDK will eventually support the ADC, when this software was developed, it didn't so the functionality for reading the ADC hasn't been incorporated into the demo program.

 

When the program is compiled and run, it will monitor the INT pin for flame/fire detection and display a message when it is or isn't seen.  You can force the transition by varying the potentiometer that is on the Flame Click board.  When the demo is run, its output is:

 

image

 

lcdmini_demo

This demo uses the LCD mini click to continuously output values read from the LSM6DSO that is on-board the Sphere board every second.  It is required to be inserted into Slot #2 for proper operation.

 

image

In addition to the data output on the LCD mini display, it is also printed to the output window:

image

 

relay_demo

The Relay click board cycles the two on-board relays through a series of combinations on/off states. Essentially, it counts from 0 to 3 using the Relay LED's to indicate which relay is active and which is not.  For this demo program to operate correctly, the Relay-Click needs to be placed in Slot #2.  When compiled and run, the following output is provided:

image

As the program is run, you will see and hear the relays open/close and the LED indicating the relay state will either illuminate or go-dark.

 

tof_demo

The TOF (time of flight) demo uses the LightRanger 2 click-board.  This click incorporates an ST VL53L0X Time-of-Flight laser-ranging module.  The code for driving this sensor is originally provided by ST Microelectronics and was adapted.  This board uses the I2C interface for communications so it can be placed in either Starter Kit mikroBUS socket.

 

There are a number of different tests that can be run:

  1. Continuous Ranging
  2. Single Ranging
  3. High Accuracy
  4. High Speed
  5. Long Range

 

The desired test to be run is specified by editing the app_manifest.json file and placing a -1, -2, -3, -4, or -5 in the "CmdArgs" field.  You can also modify the duration of the test (it has a default time of 30 seconds). Once the test begins running, its output is similar to:

image

 

The Device Information is read from the VL53L0X device during startup and once the testing begins, the data is displayed to the user and the total duration of the run is displayed.

 

Conclusion

 

The intention of these demonstration programs is to provide a library of code that has been written such that it can be used unchanged across multiple hardware platforms.  Though the demo code in this blog is written for the Azure sphere MT3620 Starter KitAzure sphere MT3620 Starter Kit, the same code can be used on the AT&T Starter KitAT&T Starter Kit when used with Breakout CarrierBreakout Carrier,  the Ultra96 Development BoardUltra96 Development Board with the Click MezzanineClick Mezzanine, or the NXP FRDM-K64F with a click SHIELD.  In fact, the demonstration code is included in the repository for each of these platforms.

 

The only limitation to note is that the Ultra96 ability to operate with the click-boards is dependent on the PetaLinux BSP implementation.  As this is a new platform, the BSP does not currently support all the different pin functions that the click-boards utilize, so at this time, support for I2C and SPI in slot #1 of the Ultra96 Click Mezzanine is the most reliable solution. As the BSP matures, support for the second mikroBUS slot and a greater variety of click-boards can be achieved.

 

As always, please provide any feedback and/or comments.  If you have code you would like to add to this repository, we welcome your contribution, please submit a pull-request on the github repository and we will get it added. It would be ideal if we could keep this Avnet repository of click-boards growing to support all that MikroElektronika provides.

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +3
    A really interesting post. Thanks. it's good that more information is starting to come out on the Azure Sphere. For a while it sort of felt abandoned.
  • Sean_Miller
    Sean_Miller over 7 years ago +3
    Thanks for sharing your code. I've been searching the internet for example Azure Sphere libraries to use with existing I2C sensors with little luck. Your code gives me a head start to building my own solutions…
  • james.flynn
    james.flynn over 7 years ago in reply to markfoster200ok +3
    Yes, this click only requires the I2C and INT pins so it should be easily implemented. I don’t have one myself but you could probably find some code for the PN7120 (which is what the click uses) that could…
Parents
  • Sean_Miller
    Sean_Miller over 7 years ago

    I thought I'd try to leverage some code to some custom code.  So, I started by dissecting the Relay click.

     

    In that codes .h file, it has a reference to an init() function which appears to init the relay.  There is also a function named rstate that sets the relay on or off.

     

    So, my thought is that this code is used by pasting it into an existing main and including the .h in that main.  In turn, my existing main's typical include files have those functions somewhere in them - such as in azure_iot_utilities.c.  However, I could not locate them in the Solution.

     

    Where do those functions definitions actually exist?

     

    Thanks,

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • james.flynn
    james.flynn over 7 years ago in reply to Sean_Miller

    Hi Sean, actually the code for the relay exists in the clickmodules repository, in the subdirectory RELAY.  When you clone the code

    1. git clone --recurse https://github.com/Avnet/clickboard_demos

     

    the clickmodules repository will be brought in via the --recurse flag.  I have found that if I forget this flag, it creates the subdirectory 'clickmodules' but it doesn't populate the code in it.  When this directory is populated it will include all the source code for the library:

    drwxr-xr-x  3 jim jim  4096 Jun 28 15:36 BAROMETER/
    drwxr-xr-x  3 jim jim  4096 Jun 30 12:13 FLAME/
    drwxr-xr-x  3 jim jim  4096 Jun 30 12:13 HEARTRATE4/
    drwxr-xr-x  2 jim jim  4096 Jun 28 15:36 LCDMINI/
    -rw-r--r--  1 jim jim  5300 Jun 28 15:36 LICENSE
    drwxr-xr-x  4 jim jim  4096 Jun 30 12:15 LIGHTRANGER/
    drwxr-xr-x  2 jim jim  4096 Jun 28 15:38 LSM6DSL/
    drwxr-xr-x  3 jim jim  4096 Jun 28 15:36 OLED-B/
    -rw-r--r--  1 jim jim  1555 Jun 28 15:36 README.md
    drwxr-xr-x  3 jim jim  4096 Aug  3 14:10 RELAY/
    drwxr-xr-x  3 jim jim  4096 Jun 28 15:36 TEMP_HUM/
    drwxr-xr-x  2 jim jim  4096 Jun 28 15:36 UART_I2CSPI/

     

    The 'init' is actually a function that you supply to performs any initialization needed for interacting with the relay board.  It is called during the 'relay_open' call.  You are correct, the rstate function sets/clears the relay. It is located in relay.c in the clickmodules/RELAY directory.  I'm guessing though that you may have forgot the '--recurse' flag and didn't get the library source.

     

    /Jim

     

    this repository will be brought in

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • james.flynn
    james.flynn over 7 years ago in reply to Sean_Miller

    Hi Sean, actually the code for the relay exists in the clickmodules repository, in the subdirectory RELAY.  When you clone the code

    1. git clone --recurse https://github.com/Avnet/clickboard_demos

     

    the clickmodules repository will be brought in via the --recurse flag.  I have found that if I forget this flag, it creates the subdirectory 'clickmodules' but it doesn't populate the code in it.  When this directory is populated it will include all the source code for the library:

    drwxr-xr-x  3 jim jim  4096 Jun 28 15:36 BAROMETER/
    drwxr-xr-x  3 jim jim  4096 Jun 30 12:13 FLAME/
    drwxr-xr-x  3 jim jim  4096 Jun 30 12:13 HEARTRATE4/
    drwxr-xr-x  2 jim jim  4096 Jun 28 15:36 LCDMINI/
    -rw-r--r--  1 jim jim  5300 Jun 28 15:36 LICENSE
    drwxr-xr-x  4 jim jim  4096 Jun 30 12:15 LIGHTRANGER/
    drwxr-xr-x  2 jim jim  4096 Jun 28 15:38 LSM6DSL/
    drwxr-xr-x  3 jim jim  4096 Jun 28 15:36 OLED-B/
    -rw-r--r--  1 jim jim  1555 Jun 28 15:36 README.md
    drwxr-xr-x  3 jim jim  4096 Aug  3 14:10 RELAY/
    drwxr-xr-x  3 jim jim  4096 Jun 28 15:36 TEMP_HUM/
    drwxr-xr-x  2 jim jim  4096 Jun 28 15:36 UART_I2CSPI/

     

    The 'init' is actually a function that you supply to performs any initialization needed for interacting with the relay board.  It is called during the 'relay_open' call.  You are correct, the rstate function sets/clears the relay. It is located in relay.c in the clickmodules/RELAY directory.  I'm guessing though that you may have forgot the '--recurse' flag and didn't get the library source.

     

    /Jim

     

    this repository will be brought in