Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Walking Robots #2 : Tobbie is Completed
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 24 Jan 2019 6:37 PM Date Created
  • Views 5818 views
  • Likes 9 likes
  • Comments 23 comments
  • mobile robots
  • tobbie
  • walking robot
Related
Recommended

Walking Robots #2 : Tobbie is Completed

dubbie
dubbie
24 Jan 2019

Continuing with my investigation of walking robots I have completed making Tobbie, as illustrated in the video below. I am very impressed with the mechanical engineering and design of this product and I think it is a great robot. I am sure that there is much more that can be done with this than just playing with it's supplied functions.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The walking mechanism is fascinating. It uses alternating sets of three legs to move forwards or backwards. It uses three legs because it is always stable so while one set of three legs is on the ground Tobbie is stable, so that the other three can be moving forwards or backwards. I'm not entirely sure how it turns yet, maybe some vector type combination of the two sets of legs.

 

It seems perfectly feasible to replace the existing electronics in Tobbie's head with an Arduino Nano or similar. I might even have a go at this myself.

 

Dubbie

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +5
    Nice little robot. The hexapod approach is very stable, so you have a nice platform to mount sensors on. It would be interesting to see a wifi microcontroller in this chassis to see how well you could…
  • danielw
    danielw over 7 years ago +5
    That looks Awesome. I might have to start saving up my pocket money! There's so much scope there for modding.
  • three-phase
    three-phase over 7 years ago +4
    Actually looks like a good quality robot given the price of it. Interesting walking method and looks very stable compared to other methods. Kind regards.
Parents
  • danielw
    danielw over 7 years ago

    That looks Awesome.  I might have to start saving up my pocket money! There's so much scope there for modding.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to danielw

    Daniel,

     

    It does seem as if Tobbie might make a good platform for some interesting experiments in walking mobile robots. I obtained mine from Amazon where one seller was much cheaper than all thee others. Seemed to be a good seller as it came quickly and was complete.  I think it is a good quality design, but it is important to remember than it is still a toy made from plastic and probably quite easy to break. Good fun though so far.

     

    Th box states it being suitable for 8 year olds but they would have to be pretty aware mechanically and very careful in order to construct it properly. I took three days to put it together as I wasn't in a rush and I carefully removed all the burrs from the injection moulded parts. Some steps were difficult to understand, especially towards the end - six legs do kind of get in the way!

     

    If MyTobbie works out I might even buy some more.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • danielw
    danielw over 7 years ago in reply to dubbie

    I can imagine it now... A Tobbie swarm!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to danielw

    Daniel,

     

    At some point I do want to make a swarm of robots. So far I have just been thinking about making very small ones as they would be cheaper and more manageable. However, imagine a whole host of Tobbies wandering about, although they do seem to be restricted to smooth surfaces which could be a problem, a bit like Daleks in Dr Who.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • danielw
    danielw over 7 years ago in reply to dubbie

    How is it that after seeing Tobbie Last week, I saw this hellish monstrosity at the weekend!

    https://youtu.be/uAWDtXoDmqg

     

    Dan.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to danielw

    Daniel,

     

    That is quite one of the weirdest things I have seen. However, I do like the walking chassis, which is obviously based on the same approach as Tobbie. It looks more substantial though. I wonder where you can get them.

     

    The laser might be a bit over the top. Probably not allowed in this Country.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • danielw
    danielw over 7 years ago in reply to dubbie

    I'd imagine that laser is restricted in our country.  I wonder if he's kitbashed something like a tobbie with additional parts from other models or 3d printed bits? it does look like a well presented model.

     

    Dan,

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • danielw
    danielw over 7 years ago in reply to dubbie

    I'd imagine that laser is restricted in our country.  I wonder if he's kitbashed something like a tobbie with additional parts from other models or 3d printed bits? it does look like a well presented model.

     

    Dan,

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 7 years ago in reply to danielw

    Daniel,

     

    The chassis for this walking robot is an Attacknid made by Combat Creatures. It is quite old now and doesn't seem to be available to buy, except via ebay. It's reliability doesn't get rave reviews but if you only want the chassis it might be OK.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • danielw
    danielw over 7 years ago in reply to dubbie

    Dubbie,

    Who knew there was such a thing as a combat spider, or Attacknids! I spent some time last night looking at different websites which finally led me to this.

    https://www.thingiverse.com/thing:1704879

    As soon as I've finished upgrading the Z axis on my printer, I'm doing one of these! 

     

    Dan.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to danielw

    Daniel,

     

    It does look good. I might have a go although there are many different parts to print. I'd prefer something simpler but that might not exist.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • danielw
    danielw over 7 years ago in reply to dubbie

    Would you say Tobbie is simpler?  Or are you thinking of a simpler method of drive?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to danielw

    Dsniel,

     

    I think that Tobbie has fewer different types of parts but some of them do need to be printed multiple times, such as the legs. I'm not very good at the 3D CAD stuff. I've tried using actual drawing CAD packages several times, but somehow I just never seem to grasp the concepts. I currently use TinkerCAD which is a block based 3D CAD package which I can just about manage as I used to make quite complex drawings using the drawing tools within Word, which I find similar. I can understand the grouping, copying and so on this approach uses. I am also happy to use nuts and bolts to make the joins which I think should also simplify the design. I have no idea how to make gears in TinkerCAD so I might have to borrow someone else's designs for that.

     

    Dubbie