Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Walking Robots #4 : I have complete control!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 31 Jan 2019 12:10 PM Date Created
  • Views 1588 views
  • Likes 10 likes
  • Comments 6 comments
  • tobbie
  • walking robot
  • arduino
Related
Recommended

Walking Robots #4 : I have complete control!

dubbie
dubbie
31 Jan 2019

I have now connected both of the motors within Tobbie to the Arduino that I have used to replace the provided control PCB, The DRV8833 PCB that I am using has two H bridge drivers so I just connected the second motor for rotating the head, to the second channel. No other additional connections ere necessary. I then set it to walk for one second, rotate clockwise for one second and then repeat this process. This was just an initial trial programme to ensure that everything was working correctly but it was interesting to see how the steering works.

the steering mechanical parts are obviously independent of the orientation of the legs which is good to know as I want to try and design my own walking mechanism. Whichever direction the head is pointing in that is then the direction that Tobbie takes.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

My next step will be to add a Bluetooth link for serial communications so that I can control Tobbie directly and then maybe think about some sensors and make it look a bit tidier.

 

Dubbie

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 7 years ago +4
    Very nice project and well executed. John
  • genebren
    genebren over 7 years ago +3
    Very cool! That looks like it has worked out quite nicely. You are well on your way to controlling your robot. Well done! Gene
  • dubbie
    dubbie over 7 years ago in reply to genebren +3
    Gene, I wasn't really thinking of trying to process the image from the camera but to just use the image for teleremote operation. I've always wanted to have a go at this so see what it is like. I've done…
Parents
  • jw0752
    jw0752 over 7 years ago

    Very nice project and well executed.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to jw0752

    John,

     

    Thanks for the support. I hope to make it better as I have just managed to ge the Bluetooth comms link working.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago in reply to jw0752

    John,

     

    Thanks for the support. I hope to make it better as I have just managed to ge the Bluetooth comms link working.

     

    Dubbie