Personal Blogs
  • Community Hub
  • More
Personal Blogs
Clem Martins's Blog Why passwords are important...
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: clem57
  • Date Created: 3 Oct 2019 1:45 PM Date Created
  • Views 4810 views
  • Likes 8 likes
  • Comments 47 comments
  • keepass
  • password-based encryption
  • change password
Related
Recommended

Why passwords are important...

clem57
clem57
3 Oct 2019

     I know a lot of you are thinking, why bother about passwords? Well let me clue you in. Many passwords we use are very weak. Let me list a few and show how long it would take to break with modern computers.

 

        • password     This is in the top 5 common list of passwords used.
        • pickles         This is in the top 2160 common list of passwords used
        • milkbad        This would take 800 milliseconds because just letters and short
        • mIlkBaD       This would take 2 minutes because short and only letters
        • m1ln2aD      This would take 6 minutes. Now we have numbers and mixed letters, but too short and no symbols
        • m1$k3a%     This would take 1 minutes. Ops, not enough to fix the problem. Too short.
        • qwerty12345asdf    Wow! finally one that would take 701,000 years to brute force attack.
        • qw$rty12#45as*f     Adding in the symbols we get 130,000,000 years to brute force attack.

 

So in conclusion, it takes the following things to make a password strong.

  1. More than 8 characters or even  more than 16 characters.
  2. Upper and lower case. This helps double the choices from 26 to 52.
  3. Add in numbers and symbols. One without the other can weaken the password.
  4. Finally, use a password generator and stored database like KeePass for instance.

 

If you wish to play around with your choices, I found this great site https://www.comparitech.com/privacy-security-tools/password-strength-test/#password-test-tool .

Give it a spin and comment below on your experience. I would like to know what is the toughest password using the above tool?

Anyone up to the challenge. Oh a password generator does not count! image

  • Sign in to reply

Top Comments

  • BigG
    BigG over 6 years ago in reply to Gough Lui +6
    In my opinion, the correct message is that users need long passwords more so than say short "complex" ones. The way I teach my kids about passwords is to type out a long sentence without spaces. It is…
  • glennvanderveer
    glennvanderveer over 6 years ago +5
    There has to be a tradeoff of entropy and usability. If you make the rules to stringent, no one will be able to remember their password. I always think of this comic when someone starts taking about password…
  • Gough Lui
    Gough Lui over 6 years ago +5
    Users need complex passwords - we know that much. Users need to avoid reuse as well - in case any password is compromised. But on the server side, administrators need to do their part as well. For one…
Parents
  • dougw
    dougw over 6 years ago

    It is all very confusing to me.

    I assume the quoted time is related to the maximum number of possible different passwords or the maximum number of tries it would take to ensure the password was tried, but presumably it could get it right on the first try. In practice, it will never take the maximum possible time to guess a password.

    Also every password system has a minimum time allowed between tries, even if it is just communications bandwidth, which would make fast computers irrelevant in computing more possible passwords. And some systems increase the time after every try or every few tries, sometimes the minimum time gets to be a very long period. Sometimes it goes to infinity.

    These extending times are often used when the password is a 4 digit pin.

    Without knowing the timing of allowed tries, computing a time to crack a password seems a bit arbitrary.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to dougw

    Even if you expect the computer to give so many tries and slow them down, you have to deal with stolen information. This is one technique of of 10 total.

    7. Offline cracking

    It’s easy to imagine that passwords are safe when the systems they protect lock out users after three or four wrong guesses, blocking automated guessing applications. Well, that would be true if it were not for the fact that most password hacking takes place offline, using a set of hashes in a password file that has been ‘obtained’ from a compromised system.

    Often the target in question has been compromised via a hack on a third party, which then provides access to the system servers and those all-important user password hash files. The password cracker can then take as long as they need to try and crack the code without alerting the target system or individual user.

    From: https://www.alphr.com/features/371158/top-ten-password-cracking-techniques

    Clem

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 6 years ago in reply to clem57

    I hadn't thought of that angle!

    Thanks for the enlightenment, Clem image

     

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 6 years ago in reply to clem57

    I hadn't thought of that angle!

    Thanks for the enlightenment, Clem image

     

    -Nico