Personal Blogs
  • Community Hub
  • More
Personal Blogs
Clem Martins's Blog Why passwords are important...
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: clem57
  • Date Created: 3 Oct 2019 1:45 PM Date Created
  • Views 4798 views
  • Likes 8 likes
  • Comments 47 comments
  • keepass
  • password-based encryption
  • change password
Related
Recommended

Why passwords are important...

clem57
clem57
3 Oct 2019

     I know a lot of you are thinking, why bother about passwords? Well let me clue you in. Many passwords we use are very weak. Let me list a few and show how long it would take to break with modern computers.

 

        • password     This is in the top 5 common list of passwords used.
        • pickles         This is in the top 2160 common list of passwords used
        • milkbad        This would take 800 milliseconds because just letters and short
        • mIlkBaD       This would take 2 minutes because short and only letters
        • m1ln2aD      This would take 6 minutes. Now we have numbers and mixed letters, but too short and no symbols
        • m1$k3a%     This would take 1 minutes. Ops, not enough to fix the problem. Too short.
        • qwerty12345asdf    Wow! finally one that would take 701,000 years to brute force attack.
        • qw$rty12#45as*f     Adding in the symbols we get 130,000,000 years to brute force attack.

 

So in conclusion, it takes the following things to make a password strong.

  1. More than 8 characters or even  more than 16 characters.
  2. Upper and lower case. This helps double the choices from 26 to 52.
  3. Add in numbers and symbols. One without the other can weaken the password.
  4. Finally, use a password generator and stored database like KeePass for instance.

 

If you wish to play around with your choices, I found this great site https://www.comparitech.com/privacy-security-tools/password-strength-test/#password-test-tool .

Give it a spin and comment below on your experience. I would like to know what is the toughest password using the above tool?

Anyone up to the challenge. Oh a password generator does not count! image

  • Sign in to reply

Top Comments

  • BigG
    BigG over 6 years ago in reply to Gough Lui +6
    In my opinion, the correct message is that users need long passwords more so than say short "complex" ones. The way I teach my kids about passwords is to type out a long sentence without spaces. It is…
  • glennvanderveer
    glennvanderveer over 6 years ago +5
    There has to be a tradeoff of entropy and usability. If you make the rules to stringent, no one will be able to remember their password. I always think of this comic when someone starts taking about password…
  • Gough Lui
    Gough Lui over 6 years ago +5
    Users need complex passwords - we know that much. Users need to avoid reuse as well - in case any password is compromised. But on the server side, administrators need to do their part as well. For one…
Parents
  • glennvanderveer
    glennvanderveer over 6 years ago

    Although the article does not say how the first break in happened, it could have been as simple as a visualbasic script that installed a key logger.  It doesn't matter what password rules you follow, key loggers record everything.  At the time of the article, VB scripts where a plague on Microsoft Windows and Office platforms.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to glennvanderveer

    If you worry about key loggers, I suggest you read https://keepass.info/help/v2/autotype_obfuscation.html . They use a method to stop that:

     

    The Auto-Type feature of KeePass is very powerful: it sends simulated key presses to other applications. This works with all Windows applications and for the target applications it's not possible to distinguish between real key presses and the ones simulated by Auto-Type. This at the same time is the main disadvantage of Auto-Type, because key loggers can eavesdrop the simulated keys. That's where Two-Channel Auto-Type Obfuscation (TCATO) comes into play.

     

    Clipboard spies don't work either, because only parts of the sensitive information is transferred on this way.

     

    Anyway, it's not perfectly secure (and unfortunately cannot be made by theory). None of the currently available key loggers or clipboard spies can eavesdrop an obfuscated auto-type process, but it is theoretically possible to write a dedicated spy application that specialises on logging obfuscated auto-type.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 6 years ago in reply to glennvanderveer

    If you worry about key loggers, I suggest you read https://keepass.info/help/v2/autotype_obfuscation.html . They use a method to stop that:

     

    The Auto-Type feature of KeePass is very powerful: it sends simulated key presses to other applications. This works with all Windows applications and for the target applications it's not possible to distinguish between real key presses and the ones simulated by Auto-Type. This at the same time is the main disadvantage of Auto-Type, because key loggers can eavesdrop the simulated keys. That's where Two-Channel Auto-Type Obfuscation (TCATO) comes into play.

     

    Clipboard spies don't work either, because only parts of the sensitive information is transferred on this way.

     

    Anyway, it's not perfectly secure (and unfortunately cannot be made by theory). None of the currently available key loggers or clipboard spies can eavesdrop an obfuscated auto-type process, but it is theoretically possible to write a dedicated spy application that specialises on logging obfuscated auto-type.