Personal Blogs
  • Community Hub
  • More
Personal Blogs
Don Bertke's Blog Why I want to speed up Global Warming!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: DAB
  • Date Created: 16 Feb 2014 10:29 PM Date Created
  • Views 3143 views
  • Likes 4 likes
  • Comments 27 comments
  • CO2
  • global
  • geology
  • levels
  • atmospherics
  • climate
  • warming
Related
Recommended

Why I want to speed up Global Warming!

DAB
DAB
16 Feb 2014

As some of you have seen in past posts, I completely reject the current effort to concern the public about global warming.

 

Mostly I object to the blatant scare tactics and lack of any scientific information that supports their position that we should work to stop it.  This last point is the really ludicrous goal.  When you do the math, we mortal humans have very few options when it comes to altering a natural planetary cycle.

 

So I went to the impeachable data source, the Geologic Record.  The data is very clear.  The earth has alternated between cold earth and warm earth states for the last 2.5 BILLION years.

When you add the Ice Core data, it shows that the cycle has been running about every 100,000 years for the last 700,000 to 800,000 years.

Almost all of the cycles have repeated like clockwork completely without any HUMAN involvement at all.

This last part is key.  The anti-global warming faction want to blame the industrial development by humans as the cause for the latest cycle.  rubbish!

 

The eco faction claims that burning the rain forest and burning fossil fuels has increased the amount of CO2 in the atmosphere and that is the cause of global warming.  Unfortunately, the math just does not work for this claim.

First of all, they are trying to use the Ice Core data as their source for comparing the CO2 levels.  They only made one tiny mistake.  The Ice trapped the CO2 level at about 10,000 feet (3000 meters) or higher.  They then want to compare those values to the current CO2 levels as measured at sea level.  When you look at the atmosphere density numbers, you would need to read twice or three times that sea level data to match the expected CO2 levels trapped in the ice.

 

Note, all of this data is in a paper published by a Polish Geologist who correctly measured the physical process of how the CO2 is first trapped and then dissolved into the water crystals as the weight of the ice compresses each snow level into glacial ice.  His research shows a very clean natural cycle by which the CO2 is removed from the atmosphere on the onset of global cooling.  Over the 50,000 years of the cycle, the CO2 levels are slowly reduced until they reach their minimum levels at the peak of the Ice age, some 12-14,000 years ago.

 

As the planet naturally warms, the ice releases the trapped CO2 until the levels reach their peak in about another 35,000 years from now.  No magic, no Human involvement, just a clean well defined natural cycle.

The latest NASA satellite measured the CO2 accumulations around the planet.  They confirmed that you have the highest concentrations of CO2 in the areas where we see melting ice.  In the high mountains and on both poles.  There were no abnormal CO2 levels in ANY of the industrial centers around the world.  So stopping the use of fossil fuels is not going to have ANY affect on the global warming cycle.

 

Now lets talk about the consequences of global warming.  The Eco factions have claimed that we will all drown as the sea levels rise as the ice melts.  That's not what the Geologic record says.

Yes, the ice will release a lot of water, BUT, ice takes up 10% more volume than water!  So we should se a net reduction in sea levels as the ice melts.

As for the land locked ice, yes it will add some additional water, but they are overlooking one important fact.  As the earth warms, there will be a tremendous absorption of water into the atmosphere.  One clear normal cycle is that warm air can hold a lot more water than cold air.  So as the earth warms, we will see a significant rise in humidity into the upper latitude regions that are currently very dry.

 

When we look into the Geologic Record, we see that a warm earth creates a huge amount of arable land up to the 70 degree latitude level.  That means we will get a huge amount of land to grow crops and support the population.  I do not see that result as being bad for humans.

 

We have also been told that the warming earth will create huge mega storms.  Again, science shows a much different result.  As the seas and the atmosphere warms, it will actually get MORE stable.  Why?  Storms are caused by the mixing of cold dry air and warm moist air.  With warm areas up to the 70 degree latitude area, the amount of cold dry air will be reduced by over 60%.  Most of the earth will experience the afternoon rain forest effect where we will get a short down pour in the late afternoon with just localized thunderstorms.  No mega hurricanes or typhoons, just consistent rain fall.  Most importantly, we will see rising humidity into areas that are now dry arid regions.  The deserts will bloom again!

 

As for living conditions, we will need much less energy to keep warm.  We should also need almost no cooling as the temperature will stabilize at about 85 degrees F for year round temperatures.

With the constant rain fall, we should have plenty of fresh water falling from the sky, so we can provide clean drinking water just about everywhere.  Hydro power can dominate the reduced energy needs of the population and we can use canals and small boats for efficient transportation.

 

I do not know about you, but I am not finding anything to fear here.

 

Plus we have a lot of time to prepare for the event.  We are currently about 13,000 years into the 50,000 year global warming cycle.  So there is absolutely no need to panic.  Yes, we will have some localized flooding along the way, but we have those every year anyway.

 

So while I am sitting in my home with the outside temperature at 30 degrees F, and oh by the way, we have spent much of the last six weeks below that temperature, I find it very desirable to have an early global warming cycle.  So I plan to burn fossil fuels, increase my carbon foot print and put as much CO2 into the atmosphere that I can and I urge all of you to do the same.

Plus I plan to beat any Eco person I meet with a stick, just to get warm. image

 

So I say enough with this Chicken Little doom and gloom propaganda about global warming.  The SCIENCE says don't panic, common sense says don't panic and the Eco people have not provided one shred of supportable data that says we should panic.  So just say "I want Global Warming and I want it NOW!" and join me in silencing these worry warts who know nothing of value.

 

Just my opinion,

DAB

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    In general I would say to DAB - I can see why you think you might be onto something here, but as I understand it the science does not support your argument. A lot of people who are concerned about the…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB +1
    "Ecologists are not scientist. Their predictions should not be considered as science. Its just their opinions and all opinions are only worth a bucket of warm spit!" Thats a very unscientific opinion Don…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB +1
    Actually, probably not! CO2 is plant food
Parents
  • vsluiter
    vsluiter over 12 years ago

    Yes, the ice will release a lot of water, BUT, ice takes up 10% more volume than water!  So we should se a net reduction in sea levels as the ice melts.

    That 10% is sticking out of the water, as Archimedes has explained. The sea level will thus stay -kind of- the same if we depend on sea ice melting.

     

    I don't know what to make of the climate change discussion; I do however think that ít's foolish to waste resources and ruin nature only because other generations will probably find a solution. Even if CO2 is not the cause of evil, we may still think about what we're doing to our environment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to vsluiter

    Hi Victor,

     

    I agree in principle, but we have a lot of efforts going way too far in the name of "saving" the planet.

    Regardless of what we do, the planet will continue to develop over time.  What is really meant by our environment is its ability to support human life.  That is my point.  What good is it to arbitrarily ban industries and energy sources and put millions of humans out of work if the result will have no effect on the lives of most of the population?

    I also agree that we need to develop efficient and low polluting energy sources, but they will not be used until the lower cost alternatives are used up.

    The current push on Carbon Capture is the most insane approach I have yet seen to "save" the planet.  CO2 is very beneficial to the plants and animals of the planet.  Why are we sequestering something that is GOOD for us?

     

    I am just trying to bring science back into the discussions.  Just about everything the Ecologists are saying is wrong or based upon unsubstantiated theories.  Worse, they have convinced politicians to make life altering decisions based upon an unobtainable utopian view of life.  A lot of people are being adversely affected by these idealized decisions.

    I think that we should stop hurting people today on an unobtainable goal for tomorrow.

     

    Ecologists are not scientist.  Their predictions should not be considered as science.  Its just their opinions and all opinions are only worth a bucket of warm spit!

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB

    "Ecologists are not scientist.  Their predictions should not be considered as science.  Its just their opinions and all opinions are only worth a bucket of warm spit!"


    Thats a very unscientific opinion Don. Actually all scientific opinion is only opinion, but opinion backed up by hypothesis, experiment, data, expert analysis, conclusions and informed argument by peer review. Ecology is no different. I work with agronomists, agriculturalists and horticulturalists all of whom recognise the vital importance of the natural systems which keep you and me alive.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB

    "Ecologists are not scientist.  Their predictions should not be considered as science.  Its just their opinions and all opinions are only worth a bucket of warm spit!"


    Thats a very unscientific opinion Don. Actually all scientific opinion is only opinion, but opinion backed up by hypothesis, experiment, data, expert analysis, conclusions and informed argument by peer review. Ecology is no different. I work with agronomists, agriculturalists and horticulturalists all of whom recognise the vital importance of the natural systems which keep you and me alive.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 12 years ago in reply to e14 Contributor

    Well Tom, what do you call people who use scare tactics and pseudo science to harm millions of people world wide?

    The Ecologists have harmed more people than any level of global warming we have experienced to date.

    I have no problem with them studying the environment and measuring changes in conditions and its effect on plants and animals.  This is science.  I only object to their screaming the "sky is falling" without any verifiable science and mathematics to support their concern.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB

    I'm curious to know exactly how you, as a scientist, diverge from the consensus.

     

    Do you reject IPCC5, and if so on what specific grounds? Can you point me to a peer reviewed paper which supports your dissent? I'm advised by colleagues that there has not been any dissenting paper published for a long time, and that most of the old ones have not survived scrutiny.

     

    Or are you planning to write one, and if so where are you intending to publish?

     

    Did you visit the site I linked to? https://www.skepticalscience.com/ That is expert opinion of a very high level of competence, I hope you will admit, and if not I would be interested to know why.

     

    All the scientists I know endorse, to a large extent, the scenario you ascribe brusquely to 'Ecologists'. It is all a matter of percentage risks. The worst case scenarios are genuinely terrifying, the best case scenarios would almost allow for business as usual, if it were not for the resource scarcity and other 'planetary boundary' issues - which I assume you must reject outright - (though on what grounds I would be interested to know). Planetary boundaries    - Stockholm Resilience Centre

     

    There are many variables, some to do with incomplete data and understanding, others to do with future decisions around mitigation, so we can't predict precisely what is going to happen. But the evidence for catastrophic damage is growing. I suspect you'll reject this, but if so it would make me I wonder from whence you are getting your information.

     

    Your anger suggests to me that you have some other reason to reject the consensus. I'm sure that as a scientist you would be careful to ensure that no non-scientific ideological influences would cloud your thinking, so I'm curious to know where you are getting your information on the latest science from, and how it supports your hypothesis outlined here.

     

    Thanks

     

    Tom