Personal Blogs
  • Community Hub
  • More
Personal Blogs
Douglas Wong's Blog Strip Board - Is it the best prototyping board?
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 23 Aug 2021 3:17 AM Date Created
  • Views 11285 views
  • Likes 20 likes
  • Comments 27 comments
  • veroboard
  • doug wong
  • track cutter
  • spotface cutter
  • strip board
  • proto board
Related
Recommended

Strip Board - Is it the best prototyping board?

dougw
dougw
23 Aug 2021

image

Veroboard

Spoiler alert - for me strip board is generally the best proto-board. But why?

Well, when it comes to circuit cards, I have a compulsion to make them clean, neat and orderly (PCB-OCD).

I have all these rules and objectives that I use when laying out circuit cards that have little to do with circuit functionality and everything to do with my concept of an aesthetically pleasing layout.

I have no idea what courses teach with regards to layout aesthetics since I never took such a course, but some of my rules come from the days before CAD when I was laying out PCBs using translucent red and blue tape.

For example I try hard to minimize the number of vias because every drilled hole increases costs.

I also try to ensure the maximum number of straight line connections since making a corner with tape takes at least twice as much time.

Re-spinning cards was (and is) a big no-no since it doubles costs and causes big delays. If you have ever had to rip up layers of tape to fix a layout issue, you know how painful it can get and why I have such an aversion to it.

In the past 400 or so PCBs I have designed, approximately 1 card needed to be re-spun (due to an idiotic assumption about pin assignments).

Approximate because I have re-spun some cards, but usually to add new features or because I wanted to improve the circuit. However I also design PCBs to allow circuit improvement without spinning a new card.

So what does this have to do with strip board?

The alternative proto boards to strip board all seem to end up with higglety-pigglety point-to-point wiring that for some reason offends my sense of propriety, even though they work perfectly well.

To digress for one point, the big promise of double sided PCBs is that all connections can be 100% routed without requiring any jumpers, even if different nets need to cross each other without touching. The simple paradigm is that all traces on one side of the card run in the same direction and all traces on the other side of the card run at 90 degrees. This allows traces to cross each other without touching simply by using vias to get to the other side of the card and hop over the track.

Strip board implements this paradigm by including all the traces on the bottom of the card running in the same direction and has all the vias pre-drilled to allow jumper connections across traces. In practice, through-hole components bridge between traces, so very few jumpers are actually needed. Basically all nets have a horizontal trace or section of a trace on the bottom of the card and all components are installed vertically between these nets. It can end up looking as neat and almost as dense as a custom double-sided PCB. It takes some planning to efficiently use the horizontal traces on the bottom and minimize vertical jumpers, but the result can be a very clean circuit card. For example the power and ground nets are generally horizontal traces that run the length of the card. Many components directly connect to these  bus bars. Also if there are busses involved they are already built into the strip board.

Individual nets may only have a few components connected, so they only need to occupy a short trace on the copper side. The trace is cut using a spot-face cutter so that the next section of the same trace can be used for another net.

Example Circuit

Here is a simple schematic of a quad op-amp chip with 19 other components implementing standard topologies for an amplifier, a filter and a comparator.

image

Here is top-view with transparency of what it might look like wired on a stripboard. The white squares are where the tracks get cut on the copper side. You can see it keeps point-to-point wiring clutter to a minimum.

After Jon Clift pointed out that there were connection errors, I made a new version with a bunch of changes....Incidentally, these changes could have been made on a real card without any change to the final look.

image

Here is the old one for those who are curious:

image

 

Newark carries lots of different sizes of stripboard or VeroBoard and they even carry a tool to cut the trackstool to cut the tracks.

image

As you use stripboard more, you discover lots of ways to make your prototyping easier and better looking. For example it lends itself well to be used with wire-wrap sockets and 0.1" pitch headers.

There are lots of breakout cards for SMT devices that use 0.1" pitch headers that work well with stripboard.

It would even directly connect to my BBC-PCBs which provide a variety of interface connectors.

I have developed several techniques to plan stripboard layouts using either graph paper, a spreadsheet or my regular CAD software. They are not really complete enough to be full solutions since I use them in conjunction with all my knowledge, but they help me to avoid getting jammed with not enough space.

I toyed with the idea of making a stripboard CAD program that would simplify the process, but I no longer do enough stripboard to make that exercise worthwhile.

Stripboards can even connect some difficult to connect parts like this big H-bridge that do not use 0.1" pitch for their pins - this one just needs to be placed at 45 degrees and each pin ends up on a different track, assuming you cut the appropriate tracks between pins.

image

Summary

I don't use a lot of prototyping cards now, but I have in the past and when I need to use prototyping cards, my go to style is stripboard. Hands down I find it to be easier to work with and the resulting circuit board looks better.

I haven't ever seen a course on how to effectively use stripboard, but it is something that can benefit makers if they take time to learn how to incorporate it into their workflows.

There are a few YouTube videos on stripboard, but from what I've seen they don't cover all the benefits (this blog doesn't either).

If you have a preferred style of prototyping card, explain it in the comments below.

  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 5 years ago +9
    I can spot two errors in your stripboard layout, if anyone wants to try practising their fault-finding skills. You were lucky with the transparent red and blue tape: the first company I worked for was…
  • shabaz
    shabaz over 5 years ago +9
    Also I guess people are familiar with the Eloi/Morlock capability with these boards : ) Like the lower stripboard only seems to have about 6 parts.. But on the underside there's at least another 16 components…
  • 14rhb
    14rhb over 5 years ago +7
    A great blog reminding me of when I got started in electronics mid 80's. Unfortunately some interesting modern devices don't come with 0.1" friendly pin outs, although a small SMT/SOIC etc breakout can…
Parents
  • colporteur
    colporteur over 5 years ago

    Your commentary on early board layout has parallels to programming. In the early days of programming I feel there was greater emphasis on efficient coding. Like electronics there were limited resources, they were expensive and not readily available. Practices that increased your chances of doing it right the first time were important. You learned those early and they became the foundation for future work.

     

    There is a vast difference comparing how you designed a PC board using early technology compared to today. Those constraints in early design reduced cost but also provided a better product. Those same cost don't exists today so motivating people to invest in the design because it improves the product is a hard sell. "yeah it cheaper and easier if I do it this way."

     

    When I worked in system engineering for a telecommunication company, I tried to anticipate the future when new systems were implemented to replace old. I referred to them as doors to the future. Not build and framed but the layout could accommodate the door. The response I would get from project managers was, it not in the requirements. Years of working from a ground level position to engineering convinced me, designing for future doors was important. It was easier to just do it and not have to convince people that it needed to be done.

     

    I support many of your suggestions in design. I'm also old and not relevant anymore.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to colporteur

    colporteur  wrote:

     

    ... In the early days of programming I feel there was greater emphasis on efficient coding. Like electronics there were limited resources, they were expensive and not readily available. Practices that increased your chances of doing it right the first time were important. You learned those early and they became the foundation for future work. ...

    That constraint is still there. But it's time and humans that are the constrained resource now, more than memory and clock speed.

    In general, we make way more complex applications with the same - adapted for inflation - budget as in the days when memory, storage and frequency were the limiter.

    They aren't as optimised for resources as in the days. But in general an average compiler optimises better than an average developer.

    And you can bring in new average developers with average costs, that can pick up in a reasonable time. Because we now don't optimise anymore until you had to split the bits in half..

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to Jan Cumps

    Jan Cumps No, since I do mostly wire-wrapRegistered So the strips don't really help me. so I prefer a Vector or Augat board. it has 2x22 pins so they can be plugged in a backplane of sorts. also, It leaves me room for by-pass caps. image

    ~~Cris

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to phoenixcomm

    phoenixcomm  wrote:

     

    ... since I do mostly wire-wrapRegistered So the strips don't really help me. so I prefer a Vector or Augat board. it has 2x22 pins so they can be plugged in a backplane of sorts. also, It leaves me room for by-pass caps...

    Isn't that too niche and obsolete to be considered as generic advise for a 2021 audience?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago in reply to Jan Cumps

    My 2 cents...

    Wire-wrap clearly isn't the usual choice for an SMT production PCB, but it has not been discontinued, it is still widely available, and pins compatible with wire-wrap are used extensively throughout the industry. It is still a very effective and low-cost way to make connections for many applications. I still use it when it is the best solution and I think it is unfortunate that not everyone has the opportunity to take advantage of its benefits.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to Jan Cumps

    Jan Cumps LOL, ?niche? I bet you want it. if you dont use SMT. (ME)

    ~~Cris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to Jan Cumps

    Jan Cumps LOL, ?niche? I bet you want it. if you dont use SMT. (ME)

    ~~Cris