I have used right angle LED indicators on a number of projects in the past and have a small collection of them.
The problem with such things, even were I to have a larger collection, is I never seem to have the right one when I need it. In the past I have had to make do with the wrong color, wait on an order, or even just bend LEDs over without a fixture. But now I have a 3D printer that needs warming up so I decided to see if I could print a fixture. The specifications I set for the trial are:
- 5mm LED
- 2.54 mm (0.1") lead spacing
- Sized to fit together in a row if desired on regular 0.1" perfboard or breadboard
This would seem easy enough but actually it is on the edge of what my little printer can do. I had to tweak hole size and such for a while to finally get something that works. Here is what the model looks like:
And here is what it looks like after slicing:
It is simple to assemble... Insert the LED and bend the leads :-)
And here are several in a breadboard lined up and working:
It would be easy to print a 2, 3, or 4 gang horizontal fixture or even stack them. If needed, the height, LED size, etc. can be modified. They don't look as nice as the commercial ones of course and are a bit clunkier. They are quick and easy however and only take about 3 minutes to print. So next time I only need a couple and don't have a full order ready, no problem.





Top Comments
-
dubbie
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
dubbie
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children