Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog 3D Printed Right Angle LED Indicators
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 8 Jun 2019 4:27 AM Date Created
  • Views 3674 views
  • Likes 9 likes
  • Comments 19 comments
  • 3d printer
  • right-angle-led-socket
  • led
  • right angle led
Related
Recommended

3D Printed Right Angle LED Indicators

fmilburn
fmilburn
8 Jun 2019

I have used right angle LED indicators on a number of projects in the past and have a small collection of them.

image

The problem with such things, even were I to have a larger collection, is I never seem to have the right one when I need it.  In the past I have had to make do with the wrong color, wait on an order, or even just bend LEDs over without a fixture. But now I have a 3D printer that needs warming up so I decided to see if I could print a fixture.  The specifications I set for the trial are:

 

  • 5mm LED
  • 2.54 mm (0.1") lead spacing
  • Sized to fit together in a row if desired on regular 0.1" perfboard or breadboard

 

This would seem easy enough but actually it is on the edge of what my little printer can do.  I had to tweak hole size and such for a while to finally get something that works.  Here is what the model looks like:

image

And here is what it looks like after slicing:

image

It is simple to assemble...  Insert the LED and bend the leads :-)

image

And here are several in a breadboard lined up and working:

image

It would be easy to print a 2, 3, or 4 gang horizontal fixture or even stack them.  If needed, the height, LED size, etc. can be modified.  They don't look as nice as the commercial ones of course and are a bit clunkier.  They are quick and easy however and only take about 3 minutes to print.  So next time I only need a couple and don't have a full order ready, no problem.

  • Sign in to reply

Top Comments

  • gam3t3ch
    gam3t3ch over 7 years ago +7
    What size nozzle are you using? one thing I noticed is the layer height there you might be able to lower it to get some better results as well. did you put the design file or stl on thingiverse or anything…
  • shabaz
    shabaz over 7 years ago +6
    They look great! It's an excellent use-case for a 3D printer.. making mounts for LEDs, switches, PCBs, etc.
  • shabaz
    shabaz over 7 years ago in reply to genebren +4
    Hi Gene, Is it possible to have transparent/translucent filament plastic? If so, light pipes could be possible. I feel it could be a great use-case if it works.
Parents
  • genebren
    genebren over 7 years ago

    Frank,

     

    Great looking results.  Nice use of your 3D printer!  I was looking for a similar product for surface mount LEDs.  On my PiCasso project, I was using an RGB surface mount LED to in normal orientation and I was looking for some right angle LEDs with similar specifications to provide side illumination, but I was unable to find a suitable match.  In the process I was thinking that it would be cool if someone made an adapter that would could switch the normal orientation into right angle (much easier with leads).

     

    Nice work!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to genebren

    Hi Gene,

     

    Is it possible to have transparent/translucent filament plastic? If so, light pipes could be possible. I feel it could be a great use-case if it works.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to shabaz

    Hello Shabaz,

     

    There is translucent filament available, it diffuses the light a lot because the end result won't be transparent 100% mostly because of the material properties itself and because the 3D printing technology will add a lot of texture, also the end result may require some isolation (like paint, darker plastic part) because the light leaks everywhere. But in short it does work but requires a bit of extra work.

     

    Luis

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • luislabmo
    luislabmo over 7 years ago in reply to shabaz

    Hello Shabaz,

     

    There is translucent filament available, it diffuses the light a lot because the end result won't be transparent 100% mostly because of the material properties itself and because the 3D printing technology will add a lot of texture, also the end result may require some isolation (like paint, darker plastic part) because the light leaks everywhere. But in short it does work but requires a bit of extra work.

     

    Luis

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 7 years ago in reply to luislabmo

    Hi Luis,

     

    Ahh, I see. Thanks for the info!

    I'm also wondering if 3D printers lend themselves to making molds. For example, a mold where transparent liquid epoxy could be poured in. Overkill for a single LED, but useful for interesting lamp projects.

    I once made a moon lamp, using transparent epoxy deliberately clouded, with several high-power LEDs embedded. It worked, but it was really difficult to make the mold. The texture could be an issue for that too, but maybe acceptable if a new mold is printed each time (i.e. destructively removed).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    I have seen several videos on using 3D printers for molds.  The print come out kind of rough due to layers but can be smoothed.  There is even a "lost PLA" method for casting metal.  Haven't tried it myself yet though.

    • Cancel
    • Vote Up +3 Vote Down