Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog 3D Printed Right Angle LED Indicators
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 8 Jun 2019 4:27 AM Date Created
  • Views 3696 views
  • Likes 9 likes
  • Comments 19 comments
  • 3d printer
  • right-angle-led-socket
  • led
  • right angle led
Related
Recommended

3D Printed Right Angle LED Indicators

fmilburn
fmilburn
8 Jun 2019

I have used right angle LED indicators on a number of projects in the past and have a small collection of them.

image

The problem with such things, even were I to have a larger collection, is I never seem to have the right one when I need it.  In the past I have had to make do with the wrong color, wait on an order, or even just bend LEDs over without a fixture. But now I have a 3D printer that needs warming up so I decided to see if I could print a fixture.  The specifications I set for the trial are:

 

  • 5mm LED
  • 2.54 mm (0.1") lead spacing
  • Sized to fit together in a row if desired on regular 0.1" perfboard or breadboard

 

This would seem easy enough but actually it is on the edge of what my little printer can do.  I had to tweak hole size and such for a while to finally get something that works.  Here is what the model looks like:

image

And here is what it looks like after slicing:

image

It is simple to assemble...  Insert the LED and bend the leads :-)

image

And here are several in a breadboard lined up and working:

image

It would be easy to print a 2, 3, or 4 gang horizontal fixture or even stack them.  If needed, the height, LED size, etc. can be modified.  They don't look as nice as the commercial ones of course and are a bit clunkier.  They are quick and easy however and only take about 3 minutes to print.  So next time I only need a couple and don't have a full order ready, no problem.

  • Sign in to reply

Top Comments

  • gam3t3ch
    gam3t3ch over 7 years ago +7
    What size nozzle are you using? one thing I noticed is the layer height there you might be able to lower it to get some better results as well. did you put the design file or stl on thingiverse or anything…
  • shabaz
    shabaz over 7 years ago +6
    They look great! It's an excellent use-case for a 3D printer.. making mounts for LEDs, switches, PCBs, etc.
  • shabaz
    shabaz over 7 years ago in reply to genebren +4
    Hi Gene, Is it possible to have transparent/translucent filament plastic? If so, light pipes could be possible. I feel it could be a great use-case if it works.
  • dubbie
    dubbie over 7 years ago

    Frank,

     

    This is a great idea, I might have to have a go myself. I use white ABS so I'm not sure if they would look better or worse.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    Nice work.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago

    They look great!

    It's an excellent use-case for a 3D printer.. making mounts for LEDs, switches, PCBs, etc.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gam3t3ch
    gam3t3ch over 7 years ago

    What size nozzle are you using?  one thing I noticed is the layer height there you might be able to lower it to get some better results as well.

     

    did you put the design file or stl on thingiverse or anything?

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
<