Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog AIS Alarm - PCB Version 0.2 Tested
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 6 Mar 2018 3:13 AM Date Created
  • Views 1877 views
  • Likes 8 likes
  • Comments 11 comments
  • fram
  • daisy
  • ais
  • buzzer
  • msp430
  • pcb design
Related
Recommended

AIS Alarm - PCB Version 0.2 Tested

fmilburn
fmilburn
6 Mar 2018

Project Objective: Develop an open source AIS Alarm that alerts sailors that a new marine vessel with AIS is within range

 

Two boards have been populated and tested now and everything seems to be working.  This update will cover thoughts on the PCB, faceplate design for the enclosure, and an update on the firmware.

 

I am satisfied with the PCB for the most part now but will decrease the drill hole size for the LED as the fit is a little loose.  Three different buzzers were tested and while all were satisfactory the one with the highest pitch seemed the most annoying and so that is the one I will use.

 

Here is the design for the enclosure face plate:

image

I had an extra dAISy blank plate for the enclosure and made a prototype with my drill press to make sure the dimensions were correct.  The plates will be fabricated by the PCB manufacturer.

 

The firmware features have now been tested individually but not completely integrated.  My chosen process is to add features one at a time and test before moving on.

 

Next up:

  • Order faceplates, parts, and PCBs for a run of 10 or so boards
  • Continue work on firmware

 

Past Posts from this Project:

AIS Alarm

AIS Alarm - The Process

AIS Alarm - Prototype Hardware

AIS Alarm - Timers and GPIO

AIS Alarm - Prototype Code Outline

AIS Alarm - UART

AIS Alarm - First AIS Messages

AIS Alarm - First FRAM Storage

AIS Alarm - Debouncing Momentary Button Switches

AIS Alarm - FRAM Ring Buffer

AIS Alarm - Schematic

AIS Alarm - PCB Version 0.1

AIS Alarm - PCB Version 0.1 Arrived

AIS Alarm - PCB Version 0.2

AIS Alarm - PCB Version 0.2 Populated

 

References and Links:

WEGMATT LLC - dAISy AIS Receiver - low cost AIS receiver

Texas Instruments MSP430FR2xx FRAM Microcontrollers - Post No. 4

TI MSP430FR2111

Maximize the Sound from a Buzzer

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +5
    Frank, What a clever idea, using a PCB as a face plate. I have struggles in the past, trying to come up with an affordable and clean face plate for products, so this is a real eye opener. How cool, in…
  • three-phase
    three-phase over 8 years ago +5
    I too hadn't thought of using a PCB for a faceplate. In the past I have printed out the faceplate onto paper and then covered with a clear stick plastic sheet available from hobby shops in the UK, as per…
  • mcb1
    mcb1 over 8 years ago +3
    Hadn't thought of using a PCB house to make face plates. Great idea and lends itself to lots of possibilities. Mark
Parents
  • three-phase
    three-phase over 8 years ago

    I too hadn't thought of using a PCB for a faceplate. In the past I have printed out the faceplate onto paper and then covered with a clear stick plastic sheet available from hobby shops in the UK, as per the resistance test box, or I have reversed the image and printed onto a transparent film and then stuck that onto the plate as per the other boxes.

     

    image

    The bottom box was a black plastic faceplate, so I tried printing yellow onto the transparent film, but that one didn't turn out too good.

     

    Look forward to seeing a fully built AIS Alarm.

     

    Kind regards.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 8 years ago in reply to three-phase

    Those look really nice!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 8 years ago in reply to three-phase

    Those look really nice!