Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gene Breniman's Blog Kitchen lighting system - take 2
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 3 Jan 2018 11:57 PM Date Created
  • Views 2243 views
  • Likes 13 likes
  • Comments 15 comments
Related
Recommended

Kitchen lighting system - take 2

genebren
genebren
3 Jan 2018

Upon moving into our 'new' home in Texas (5/2016), we noticed an under-cabinet lighting system was in place in our kitchen.  We thought cool, this will help brighten up our kitchen.  I found the remote, tried all the buttons, but nothing happened.  I then noticed that the light pucks were all battery powered.  This might make for an easy install, but wow, that is a lot of batteries (3 AAA batteries per unit x 8 units).  So after settling in a bit I decided to convert the system to use a wall wart for power and modify the system to slave itself to the under-cabinet microwave's surface lighting system (nice two level control button on the microwave front panel, i.e. not added switches). The idea was to install a small circuit into the microwave, connected in series with the lighting system, which would be powered by the controller board, and would return the current flowing to the lights.  The controller would read the A/C waveform for the current and determine the light setting level (off, low or high) and then transfer a light level to the modified light pucks via a four wire cable (+5, ground and an I2C bus). 

 

This all worked well for a while, but the current sensor was also picking up crazy readings when the microwave was in use, or when the microwave door was opened or closed.  I tried various modifications to the reading of the currents, but nothing was rock solid.  Either the lights would come on randomly or not come on at all.  I had adapted the algorithms to use filtering, modified the baseline and thresholds programmatically, moved the limits around, but nothing seemed to work quite the way I wanted.

 

Here are some pictures of the various components (original and modified):

imageimageimage

This is the original unit back, front (light on) and controller (as best as I can tell, this was a home depot distributed product).

 

 

imageimageimage

After cutting out the old battery compartment, I mounted the universal PCB (at left, configured as a end-point light fixture, center, configured as the controller and at right, the original electronics).  I used a Atmel, ATtiny85 as the processor for the light pucks and the controller boards (the opposite of this boards as the three LEDs mounted). In all, a very simple replacement PCB, designed around the mounting holes of the original unit.

 

So fast forward to the present.  After having recently completed a PIR based system for a client, I began to think that maybe I should convert my kitchen lighting to a PIR motion turn on/off system.  My wife agreed and I started planning on a very simple implementation.  Using a simple SparkFun PIR sensor, that I connected in place of my current sensor board (+5V, ground and input), I could and a 'motion detect' signal to my controller. My idea was simple, on motion detect, turn on the lights and set a timer.  Any time motion is detected, the timer is reset.  When the timer times out, the lights are turned off.  The modification to the controller was very simple, rip out all of the current sensing, replace it with a simple motion detect (high going logic level) and add a simple timer (1 to 120 minutes). Even with my dominant (right) arm in a sling, I was able to code and test the changes in a little less than a day.  Hopefully I can finish the installation tomorrow.

 

We will see how long this system work!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago in reply to mcb1 +4
    Hi Mark, I suspect you're right. They are a bit ancient now (perhaps coming up to 10 years), and due to the permanence of how I mounted them (I cut slots into the cabinet underside, and glued them flush…
  • genebren
    genebren over 8 years ago +4
    I finished the installation of the PIR board and the upgraded controller board. Everything looks like it is working well. I still need to verify delayed power down, but as I have already tested in on the…
  • mcb1
    mcb1 over 8 years ago in reply to genebren +3
    I always enjoy looking through the lights at IKEA I'm sticking to the catalogue from now on ... it will be quicker.
Parents
  • mcb1
    mcb1 over 8 years ago

    Nice solution in the end.

     

    On a trip to Australia we made the mistake (only because it was 4hrs later we got out) of visiting an IKEA shop ... and their under cabinet lighting range was rather good.

    Unlike our Asian friends they included decent looking profiles to either guide the light, or at least obscure the light source.

    NORRFLY LED light strip - 36 " - IKEA

    This is one example but they did have others ...

     

    We were looking at them to place under a cabinet and above a work desk. They needed to be shielded as the user was affected by direct light source even in her periferal vision.

     

     

    shabaz

    I suspect your leds are suffering from either overdriving, or what I've seen on many other LED products, a lack of proper current regulation to each LED.

    The expoxy is probably not helping with heat dissapation.

     

    You could always try NeoPixel strips, that way you can regulate the light and the colour if you want.

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    Hi Mark,

     

    I suspect you're right. They are a bit ancient now (perhaps coming up to 10 years), and due to the permanence of how I mounted them (I cut slots into the cabinet underside, and glued them flush) they're a lost cause, so one day I'll fit something surface-mounted over them. They are very unevenly lit due to the dead and faded LEDs. In the second pic you can see the mounting, basically I cast into a long rectangular block (water-clear epoxy) and glued it into the cabinet. A funny story, even architects get lighting wrong : ) a friend of a friend worked for a very well-known architect firm, and when I visited their kitchen, they had upward wash lights in the floor in the kitchen against the sides, but they were incandescent , maybe halogen : ) toasty feet if you were bare-foot : ) To be fair that was about 10 years ago too, so before LEDs were super popular for residential, but still... : )

     

    image

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to shabaz

    shabaz

    I suspect you can remove these ... with a bit of persuasion.

     

    I'd try drilling and taping into the resin in a couple of places at one end.

    Screw in a couple of threaded rods and fit a u shaped Ie a piece of wood with a slot, over the led strip.

    You should be able to tighten on the thread and effectively wind it out by breaking the glue.

     

    The image below is the best I could find ... yes it's not great. Most pullers pull the outer section over the inner item.

    http://3.bp.blogspot.com/-ADkTFQTXnaE/U0M4agpJP3I/AAAAAAAAHCs/BcRmLhvwRBc/s1600/2014-04-07+19.33.57.jpg

    Imagine that the threaded rod is much smaller and the white plastic is your LED strip.

     

     

    The other option is to remove the cabinet and route them out, or at least route the middle effectively splitting them.

     

     

    You can replace them and use double sided tape this time image

    I'd be inclined to leave an air gap so any heat can dissipate, or simply use a strip of acrylic flush with the cabinet base and have the LED strip in behind it.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    Neat trick! That would work : ) I should have used tape, or maybe magnets to have them removable. I like that there are lots of practical options for under-cabinet LED lighting such as the ones Gene is using. I'm using some in the shed/workshop to illuminate some areas for tools storage, but will re-do the lighting in the next couple of months (painting the floor and sorting out the walls first).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    Neat trick! That would work : ) I should have used tape, or maybe magnets to have them removable. I like that there are lots of practical options for under-cabinet LED lighting such as the ones Gene is using. I'm using some in the shed/workshop to illuminate some areas for tools storage, but will re-do the lighting in the next couple of months (painting the floor and sorting out the walls first).