Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gough Lui's Blog A Modern Digital Etch-a-Sketch
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 11 Jan 2020 8:31 AM Date Created
  • Views 6830 views
  • Likes 15 likes
  • Comments 18 comments
  • RoadTest
  • bk
  • kids
  • b_and_k_precision
  • chart recorder
  • b&k
  • heart
  • etch
  • data acquisition system
  • etch-a-sketch
  • sefram
  • das240-bat
  • recorder
  • b&k precision
  • data acquisition
  • multi_channel
  • bk precision
  • holidayspecial19ch
  • data_acquisition_systems
  • b&k_precision
  • presents
  • project14
  • art
  • bk_precision
  • multi-channel
  • toy
  • data_acquisition
  • das240
Related
Recommended

A Modern Digital Etch-a-Sketch

Gough Lui
Gough Lui
11 Jan 2020
image

Holiday Special 19

Enter Your Holiday Season Project for a Chance to Win Over $20,000 Worth of Prizes and Gifts to Give!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

When I posted my projects for the RF Project 14 in November, I mentioned that things might get busy, meaning I would not have much of a chance to post more projects. Well guess what? I was right! The Christmas-New Year period was exceedingly busy as I blogged on my own personal blog and tried to finish a few different projects that I have always wanted to do. Seeing that the Holiday Special Project14 deadline is coming up, I thought I'd do my best to cobble together a short project.

 

When I think of holiday periods, I think of gifts. When I was a child, one of the toys that people would play with is an Etch-a-Sketch - a board with some magnetic material that turns dark on the action of the magnet, which is suspended by cords along two axes with two controls on the front that control the X and Y axis motions independently. Using this, one could draw some rather simple images without needing paper, or pens. I never had an Etch-a-Sketch as a child, but then again, I was never really artistic anyway.

 

But then, just as the holiday season approached, I got news that I was awarded the B&K Precision / Sefram DAS240-BAT RoadTest review. Just two days before new year, the unit arrived, which got me thinking ... could this become an expensive modern digital Etch-a-Sketch? The answer was yes!

 

Building the System

Lucky for me, the DAS240-BAT supports direct measurement of resistance as it has an internal bias generator and the unit is capable of plotting in X-Y mode. All I have to do is supply the resistance.

image

Rummaging in my junk box, I found two new 500-ohm linear carbon-track long-stem potentiometers. I soldered a wire to one end of the track and the wiper and covered the connection in heatshrink. I then wired it to the input pluggable terminal block with the resistance across the +/- connections and the bias tied into the negative side as instructed by the manual.

image

I twisted the wires for some noise suppression, while plugging it into the 20-channel input module. Using some Blu-Tack, I stuck the potentiometers down to the table so they could be manipulated safely and then grabbed the camera.

 

In Action

I'm not much of an artist, nor have I used an Etch-a-Sketch before, but I tried my best to do a project with heart, by literally drawing a heart. Then I decided to try and draw my name ... I guess I don't have much finesse when it comes to turning pots ... as you'll see in the video

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

But I suppose it could be improved if I had used higher-quality 10-turn potentiometers as the 270-degree range of these pots combined with the mechanical backlash means that it's hard to get it to move precisely. The same sort of set-up can be used with a voltage source and infinite persistence in X-Y mode to do the same thing on an oscilloscope.

 

Conclusion

It's portable, it has an X and Y control and it draws an image. But it's not an Etch-a-Sketch ... it's a sophisticated, expensive piece of test equipment being tested in a rather whimsical manner. It's a pretty expensive way to get Etch-a-Sketch-style functionality, but it does work and it took all of about an hour to complete (from ideation through to uploading the blog and video). A project with heart? Maybe. A holiday project? Definitely.

 

It's also a bit of an experiment of mixing a Project14 with a RoadTest - within the next month or so, the full RoadTest review for the B&K Precision / Sefram DAS240-BAT should be complete and published, so I hope you look out for it as there's been a lot of interesting findings to say the least.

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 6 years ago +7
    Hi Gough, What a fun project; a heart is a very tricky shape for just X and Y input. I'm sure you can also print the output (which the original Etch-a-Sketch could not). It makes me now think of two things…
  • Gough Lui
    Gough Lui over 6 years ago in reply to beacon_dave +5
    Well, if I was doing that, I might as well get myself a two-channel arb waveform generator and draw everything with vectors ... but I think that's cheating . I could do it (slowly) with the multi-channel…
  • beacon_dave
    beacon_dave over 6 years ago in reply to Gough Lui +5
    yes, (drum roll) it's a 'fine line' (cymbal clash) I seem to recall several attempts with stepper motors attached to real Etch-a-Sketch tablets, and I think one even was connected up to a R-Pi camera so…
Parents
  • 14rhb
    14rhb over 6 years ago

    Hi Gough,

     

    What a fun project; a heart is a very tricky shape for just X and Y input. I'm sure you can also print the output (which the original Etch-a-Sketch could not). It makes me now think of two things:

     

    (1) You've a bit of practice needed to beat Elf (in the film Elf) !

    image

    [External Source: https://movies.stackexchange.com/questions/105478/how-was-the-etch-a-sketch-art-of-mona-lisa-made-for-elf  ]

     

    (2) I saw this recently, which is an Etch-a-Sketch for a woodwork router.

    image

    [External Youtube video: https://www.youtube.com/watch?v=ulblySFElo4  ]

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 6 years ago in reply to 14rhb

    I suppose with some more patience and gearing-down the pots, I might have a shot still ... but alas, I'm not looking to migrate my career to competitive Etch-a-Sketching ... so I guess I'm doing alright image. Indeed, we can take a screenshot and print it out, but alas, I don't think it quite has the resolution necessary for those near-halftone greys ... you win some, you lose some?

     

    - Gough

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 6 years ago in reply to Gough Lui
    You're doing very well IMO.
    ...competitive Etch-a-Sketching

    Something I hadn't even thought about, do people do that? I'm 50:50 wondering if I should Google the term to see but worried I might end up liking it so much and taking part image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 6 years ago in reply to Gough Lui
    You're doing very well IMO.
    ...competitive Etch-a-Sketching

    Something I hadn't even thought about, do people do that? I'm 50:50 wondering if I should Google the term to see but worried I might end up liking it so much and taking part image

    • Cancel
    • Vote Up +4 Vote Down