Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gough Lui's Blog Click MR16 LED Globe Failure Post-Mortem
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 1 Jun 2016 5:59 AM Date Created
  • Views 3066 views
  • Likes 5 likes
  • Comments 20 comments
  • fail
  • analysis
  • lighting
  • failure
  • led
  • led lighting
  • teardown
Related
Recommended

Click MR16 LED Globe Failure Post-Mortem

Gough Lui
Gough Lui
1 Jun 2016

One of my regular blog readers submitted an LED globe for post-mortem analysis, having failed well before the expected lifetime. I take a look inside, determine the configuration and analyze the relatively "anonymous" product which seems to show several design shortcomings which I discuss and think might be relevant to other readers at the element14 community.

 

The article is posted at http://goughlui.com/2016/06/01/failed-click-ltmr5w3k-5w-led-mr16-replacement-globe/

 

What really gets me is that many products are still designed using multiple-parallel LEDs without any current balancing mechanisms (e.g. remember emitter feedback resistors when paralleling BJTs?) and that leads to potential for a single string to be overstressed continually, fail early, and begin the cascade of failure as other LEDs are forced to soak up current in excess of their ratings, and operate in less efficient regimes resulting in greater heat production and degradation of the semiconductor material. Of course, if you went all-series, you would have an all or nothing situation and require higher voltage driver electronics, but I personally would gravitate to this arrangement for reliability reasons, or go with multiple independent channels if reliability is demanded.

 

Any comments, or stories related to LED globes or LED light designs are very much welcome.

 

- Gough

  • Sign in to reply

Top Comments

  • Dudley
    Dudley over 10 years ago in reply to Gough Lui +3
    We have absolutely no problem with you or anyone else posting links to blogs on external sites, as long as: It's of interest to engineers It's not spam Obviously we'd rather you blogged here, but we're…
  • jw0752
    jw0752 over 10 years ago in reply to shabaz +3
    Over the years I have become used to working under (4) 150 Watt incandescent flood lights. Yes they were hot and probably cost a couple $ a month to operate but I needed to see the cracks and problems…
  • jw0752
    jw0752 over 10 years ago +2
    Hi Gough, I am hoping that they do as good of a job figuring out what went wrong with me when I stop ticking as you performed on the LED globe. This is a great learning experience to follow your dis-assembly…
Parents
  • shabaz
    shabaz over 10 years ago

    We should have a section at element 14 for discussing different lighting product experiences and feedback. Although a lot of home lighting experience could be subjective though, so hard to compare.

    Much like mcb1 I too am in no hurry to swap conventional lighting at home for LED. But kind-of giving LEDs a trial currently in one room. The previous lights were incandescent, 40W or 60W (depending on what is available off-the-shelf - the 60W are getting rare in the DIY stores) x 5 lamps, which reflect off walls, not down spotlights.

    I went for these ones, the R50 version in the photo below: RefLED Blown Reflector | Sylvania Lighting Solutions

    image

    These ones are not perfect for all rooms, they are not suitable for dimming with an incandescent lamp dimmer.

    The feedback so far is semi-neutral to positive depending on who I speak to.

    The consensus is basically it is definitely brighter. Those who are neutral overall say the color feels too white/unnatural, and the color or effect (could be CRI related or color temperature related, I can't decide) has a slight feel of ugliness like some economy CFLs have. I can see that too.

    I get the feeling that without mixing LED colors*, this problem would be hard to get rid of. I'm not sure though, and will try some more lamps.

    I might also swap back to incandescent for a bit, and see what the feedback is then..

     

    * maybe separate color lamps, e.g. dimmable red, to mix with white LED lamps could be an option too, to try to correct things. More awkward though.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to shabaz

    Lots of opinions out there, and lots of different quality. The majors tend to do it okay, but the consumer level products of some brands are merely rebadged products OEMed from some company in China (e.g. Leedarson OEMs for Ikea, OSRAM (Sylvania) Lightify (Tunable White only) and Belkin WeMo for example).

     

    On the whole, I won't say I'm "in a hurry" but I've got more than a few LED globes. Almost half the house is LED globes, and soon, even more will be LED purely because I dislike some of CFL's disadvantages (mainly cycle life, warm-up time). The light quality indeed is poorer for many of the economy LEDs and they boil down to the CRI being on the high 70's to low 80's. The better ones score top out at a CRI of about 85 at the most when it comes to those which use white LEDs because of the physics of using ~460nm blue + a phosphor mix to give yellows and reds which still leaves a nice gap in the greens.

     

    An improvement in CRI seems to be from the tunable RGBW multicolour globes that use a discrete red (623nm), blue (460nm) and green (525nm) LED to create white. The downside is that these globes are mainly expensive home automation/Zigbee control units, and they're also generally lower on output because of the added complexity of three independent control channels. But in return, you get CRIs of >85 (e.g. OSRAM Lightify) and tunable colour temperature ... and while it could be even better than that, I suspect they decided to "stop short of a technical barrier" purely because a consumer is unlikely to need CRIs greater than 90-somethings.

     

    The mixing LED colours business seems a rather interesting approach, and the tunable white globes generally achieve their tunability by "fading" two channels to mix 2700k warm white LEDs with 6500k daylight LEDs to give the "complete" range. This works but of course, the CRI doesn't necessarily improve even when choosing an intermediate colour temperature.

     

    So far, I've had one early life failure in a personally purchased and deployed globe that boiled down to a driver failure (unidentified due to the physical construction being impossible to take apart), but the remainder are going on well. Dimming with these globes where they are supported requires trailing edge dimmers, and many existing dimmers are leading edge and won't function correctly or will cause premature failure as well. Even a universal dimmer is no guarantee - I have one on the test bench at the moment which has caused me no end to frustration because it has a 10VA load minimum and even a 15W LED globe won't allow it to run stably.

     

    I suppose, environmentally, the lower energy consumption and lack of mercury gets my tick as well.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 10 years ago in reply to shabaz

    Lots of opinions out there, and lots of different quality. The majors tend to do it okay, but the consumer level products of some brands are merely rebadged products OEMed from some company in China (e.g. Leedarson OEMs for Ikea, OSRAM (Sylvania) Lightify (Tunable White only) and Belkin WeMo for example).

     

    On the whole, I won't say I'm "in a hurry" but I've got more than a few LED globes. Almost half the house is LED globes, and soon, even more will be LED purely because I dislike some of CFL's disadvantages (mainly cycle life, warm-up time). The light quality indeed is poorer for many of the economy LEDs and they boil down to the CRI being on the high 70's to low 80's. The better ones score top out at a CRI of about 85 at the most when it comes to those which use white LEDs because of the physics of using ~460nm blue + a phosphor mix to give yellows and reds which still leaves a nice gap in the greens.

     

    An improvement in CRI seems to be from the tunable RGBW multicolour globes that use a discrete red (623nm), blue (460nm) and green (525nm) LED to create white. The downside is that these globes are mainly expensive home automation/Zigbee control units, and they're also generally lower on output because of the added complexity of three independent control channels. But in return, you get CRIs of >85 (e.g. OSRAM Lightify) and tunable colour temperature ... and while it could be even better than that, I suspect they decided to "stop short of a technical barrier" purely because a consumer is unlikely to need CRIs greater than 90-somethings.

     

    The mixing LED colours business seems a rather interesting approach, and the tunable white globes generally achieve their tunability by "fading" two channels to mix 2700k warm white LEDs with 6500k daylight LEDs to give the "complete" range. This works but of course, the CRI doesn't necessarily improve even when choosing an intermediate colour temperature.

     

    So far, I've had one early life failure in a personally purchased and deployed globe that boiled down to a driver failure (unidentified due to the physical construction being impossible to take apart), but the remainder are going on well. Dimming with these globes where they are supported requires trailing edge dimmers, and many existing dimmers are leading edge and won't function correctly or will cause premature failure as well. Even a universal dimmer is no guarantee - I have one on the test bench at the moment which has caused me no end to frustration because it has a 10VA load minimum and even a 15W LED globe won't allow it to run stably.

     

    I suppose, environmentally, the lower energy consumption and lack of mercury gets my tick as well.

     

    - Gough