Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gough Lui's Blog Woefully Insecure: Remote Control 433Mhz Power Sockets
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 10 Apr 2016 3:04 AM Date Created
  • Views 2614 views
  • Likes 4 likes
  • Comments 15 comments
  • 433.92mhz
  • remote control
  • wireless
  • power switch
  • 433
  • remote
Related
Recommended

Woefully Insecure: Remote Control 433Mhz Power Sockets

Gough Lui
Gough Lui
10 Apr 2016

It's been a while since I've had the time to post anything around here. Luckily, I had recently just submitted my PhD thesis so that gives me a chance to take a short break and do some of the stuff that I like.

 

Recently, I came across a bunch of cheap remote controlled 433Mhz power sockets which I decided to pick up, tear down and reverse engineer on my blog site. Because of the recent discussions regarding remote control that I've been a part of on this forum, I thought it would be rather interesting to some of the people here as well. What I found was most intriguing - a fixed code system with no checksum/CRC, a 3-bit address space and 1-bit switch command for 4 variable bits in a 25-bit message, and hard coded broadcast-to-all switches including fresh un-learned switches out of the box.

 

I think it's probably worth a read as I go through the whole process from start to finish, and now I have an Ethernet bridge to the 433Mhz system built out of my efforts. It doesn't improve security, but it does improve usability. However, it's a key point that even if a system has a "learning" button and doesn't seem to respond to "other" codes that it's not necessarily secure by design. It may just give the impression of security.

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 10 years ago in reply to clem57 +2
    Thanks for the comment clem57 . When I looked at the wholesale listings on made-in-china.com , they claimed that they do export market to USA, which I suppose means that they do have US-standard plug versions…
  • shabaz
    shabaz over 10 years ago +2
    Hi Gough! Great post and relevant information. To be honest most consumer remote power strips are insecure here too. Although the ones I have seen have been built to a higher quality and using more reliable…
  • Gough Lui
    Gough Lui over 10 years ago in reply to shabaz +2
    Agreed on your views there shabaz , although I'd have to say that given the cost of rolling code "replacement" remotes for garage doors from China not being much, the cost of using a rolling code chip…
Parents
  • shabaz
    shabaz over 10 years ago

    Hi Gough!

     

    Great post and relevant information. To be honest most consumer remote power strips are insecure here too.

    Although the ones I have seen have been built to a higher quality and using more reliable modulation schemes and at least did have a functioning learning capability. But insecure nevertheless, nothing that someone with a $10 SDR dongle and laptop couldn't grab and replay again and again.

     

    It isn't great, but the thinking goes along the lines of:

    (a) Question: what is the value of the impact to the "thing" that is to be secured?

          --> Answer: probably a few pennies/cents if the "thing" is remote controlled home lighting where malicious switching-on will result in a slightly higher power bill

    (b) Question: what is a reasonable amount to do in order to provide reasonable protection from the risk of that impact (the impact being a few pennies in this case)

          --> Answer to date from most manufacturers: not publish the bitstream

     

    It all breaks down of course if our answer to (a) is slightly different, such as if we use such remote control power sockets to operate (say) electric security gates or kettles that could run dry etc or if the particular lighting is visible from outside and causes a security issue for users.

    Not disagreeing that manufacturers could do more (or at least publish guidelines on what the recommended use-cases for their products are based on a security perspective, because the average non-technical user may mistakenly presume such products are secure for all practical purposes which as you've shown clearly they are not).

     

    Sad to say, but possibly the sort of thing that might need legislation so that such products meet a minimum published security standard (there will still be products that flout it of course) or declared in plain language on the packet, but today there is no legal requirement in the UK with respect to wireless security for home remote control products as far as I am aware (I could be totally wrong - not my main knowledge area!!).

    Of relevance to (b), the ability to do reverse-engineering and replay attacks at low cost has changed dramatically in the past few years because of the availability of cheap SDR (not blaming SDR! just stating that some will misuse it).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to shabaz

    Agreed on your views there shabaz, although I'd have to say that given the cost of rolling code "replacement" remotes for garage doors from China not being much, the cost of using a rolling code chip on both ends is probably trivial. It's not going to be as simple as a non-receiver-module based plug, but it's still not much more expensive, especially compared to two-way remotes which are much more sophisticated.

     

    I think the issue is not only to do with what is "lost" in case that someone breaks the system - it's more so the user experience and usability. With a more complex chipset comes a better reliability - through either having more independent group controls, better verification of sent codes, more robust error correction for greater range or perhaps, less possibility of interference from a neighbour especially if you happen to accidentally discover they have the same system too and neither of you are willing to sacrifice it, meaning that neither can use it reliably without a virtual RF war.

     

    Energy bills aside, as energy is pretty cheap, I've seen some sites actually sell this unit claiming it's good for remote switching of woodwork equipment. Ultimately, if consumers were informed and took the risk themselves, that would be fine, but consumers are none the wiser and throwing these things in even though they might be making their standby power bills worse and costing them money to buy it in the first place which is somewhat unforgivable.

     

    The cost of reverse engineering has indeed gone down - my use of RTL-SDR was not the only (cheap) option - all OOK/ASK devices are trivial bypasses by looking at the output of a <$3 ASK/OOK receiver. If I was really trying to minimise my outlay, I would probably go and take the D-pin from the transmit module on the SMARTBox and voltage divide it into my soundcard to record the code. Once the timing is known, a <$3 ASK/OOK transmitter and an Arduino (as I have done) is all I'd need ... a similar approach to how I used to emulate IR signals using Arduino.

     

    It's scary when the "primitive" radio technology used doesn't really need a radio to analyze it if you're willing enough ... and with the hard-coded all-unit broadcast, it could really become a nuisance. Of course, I'm still running the sockets, and I think the risk is low enough for my lighting uses, but I'm mindful that anything could happen at any time.

     

    I suppose if it inspires others to check on theirs and maybe repurpose their switches and unshackle them from the limited push-button remote to open up scripting/schedule possibilities, that would be nice, and is part of the reason I did mine. What better way to share control of common area house lighting with the family than by making it network-controllable image.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 10 years ago in reply to shabaz

    Agreed on your views there shabaz, although I'd have to say that given the cost of rolling code "replacement" remotes for garage doors from China not being much, the cost of using a rolling code chip on both ends is probably trivial. It's not going to be as simple as a non-receiver-module based plug, but it's still not much more expensive, especially compared to two-way remotes which are much more sophisticated.

     

    I think the issue is not only to do with what is "lost" in case that someone breaks the system - it's more so the user experience and usability. With a more complex chipset comes a better reliability - through either having more independent group controls, better verification of sent codes, more robust error correction for greater range or perhaps, less possibility of interference from a neighbour especially if you happen to accidentally discover they have the same system too and neither of you are willing to sacrifice it, meaning that neither can use it reliably without a virtual RF war.

     

    Energy bills aside, as energy is pretty cheap, I've seen some sites actually sell this unit claiming it's good for remote switching of woodwork equipment. Ultimately, if consumers were informed and took the risk themselves, that would be fine, but consumers are none the wiser and throwing these things in even though they might be making their standby power bills worse and costing them money to buy it in the first place which is somewhat unforgivable.

     

    The cost of reverse engineering has indeed gone down - my use of RTL-SDR was not the only (cheap) option - all OOK/ASK devices are trivial bypasses by looking at the output of a <$3 ASK/OOK receiver. If I was really trying to minimise my outlay, I would probably go and take the D-pin from the transmit module on the SMARTBox and voltage divide it into my soundcard to record the code. Once the timing is known, a <$3 ASK/OOK transmitter and an Arduino (as I have done) is all I'd need ... a similar approach to how I used to emulate IR signals using Arduino.

     

    It's scary when the "primitive" radio technology used doesn't really need a radio to analyze it if you're willing enough ... and with the hard-coded all-unit broadcast, it could really become a nuisance. Of course, I'm still running the sockets, and I think the risk is low enough for my lighting uses, but I'm mindful that anything could happen at any time.

     

    I suppose if it inspires others to check on theirs and maybe repurpose their switches and unshackle them from the limited push-button remote to open up scripting/schedule possibilities, that would be nice, and is part of the reason I did mine. What better way to share control of common area house lighting with the family than by making it network-controllable image.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 10 years ago in reply to Gough Lui

    Agree, yours don't need an SDR since there is no learning, so anyone who knew they owned the same ones as yours could figure out the encoding scheme, so yours are less secure.

    Mine would need for someone to have either physical access to my hardware, or (say) an SDR (since mine do have a unique number, but no rolling code), so slightly more secure but not much!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to shabaz

    Just out of interest - do you know how many bits of the message for yours are "unique" material? If the search space isn't too big, I've known for some people to emulate the protocol and avoid the retransmissions to speed up brute-force attempts - so if it's only a few "variable" unique bits, it still might not be "enough" if you know what I mean. I've seen some older systems with DIP-switch set fixed codes from 4 to 16 bits long depending on the device - at the low end, it's trivial, at the upper end, it's not too bad for security.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to Gough Lui

    I wrote some notes on the one that I used here:

    Energenie Experiments – Remote Power Control for the Home

    Basically about 1M combinations, so perhaps at max a week worth of continuous effort at a guess. It uses an off-the-shelf chip (Holtek I think, they usually offer such low-cost chips).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to shabaz

    I did some work on these during my Forget me Not.

    Forget Me Not :  eLDERmon  Hardware Hacking #3

     

    The code is 24 bit and they utilise bit 21 as ALL ON or ALL OFF.

     

     

    You are right about the lack of security, but even if you explained that to someone, would they actually consider it.

    Many people can even be bothered changing the password on their router, despite the warnings, hints and notes that tell them to.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to mcb1

    Like me for internal test routers.