Personal Blogs
  • Community Hub
  • More
Personal Blogs
Hardware Camera Location and Mounting
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mcb1
  • Date Created: 25 Aug 2013 11:29 AM Date Created
  • Views 3563 views
  • Likes 3 likes
  • Comments 19 comments
  • wifi
  • raspberryp-pi
  • raspberry_pi_camera
  • solar
  • temperature_measurement
Related
Recommended

Camera Location and Mounting

mcb1
mcb1
25 Aug 2013

This is part of my project to fit a solar powered RaspberryPi webcam at Mt Lyford that starts here

 

An excuse for a field trip (to a skifield) on a nice day, is not to be missed, however this trip was all business, with a couple of other things to look at/repair as well.

The exact location and mounting method was one of the things on my list.

 

Snow, ice and the odd heavy machine (groomer) means that unless its well anchored, its very likely to move.

Snow is a strange thing, and this year they received the largest dump in 30 years, over 2m (78 inches)

Many barns and sheds around the area, caved in with the weight of the fairly wet snow dump.

 

The snow was also delivered with high winds, which meant some drifts were 6m deep, and the only access to the field was by helicopter.

 

Obviously any mounting (and what its fitted to) needs to withstand some abuse, add in some brittleness from extreme and prolonged cold, and you need to plan carefully.

 

 

imageimage

 

This pole is driven well into the ground and is solid.

It also is far enough away from the groomers when they shape the return track, as the corner is widest at that point.

 

The base of the pole has a nice area for a wooden battery box, that will withstand the elements (and the odd hit from a shovel ... if they need to dig it out).

 

The view from the location is right, and while this isn't from the RPi, gives the option of two tow lines to aim at.

(There has been very little additional snow and warm weather since that first dump, and as a conseqence a lot off trail has been lost.)

 

image

 

While I was there, I considered where the sun would be, and looked at what options there were for the solar panel.

This photo was taken at 12:46 pm and gives me a pretty good idea of the panel angle and orientation.

It can be combined with the other mount and will fit on the pole easily.

 

imageimage

 

Because I couldn't ski that day, I had to borrow one of the new Snow mobiles, which I have to say are a bit addictive.

However it wasn't a joyride as I helped deliver some fuel to the rope tow ...

 

 

Mark


  • Sign in to reply
Parents
  • Problemchild
    Problemchild over 13 years ago

    Top bannana Mark love the photos..pitty you are 1/2/ the globe away I want to go up there just from the photos.

    Is this a comercial enterprise or purely for  your entertainment pr again a bit of both ??

     

    Just did a thermal Image sequence on a RPI thought that was cool but now fancy been out and about

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to Problemchild

    John

    Thanks for the compliments.

    You get twice the NZ dollar for your pound, but you might want to wait until next year or more snow.image

     

    The field is commercial, and I started skiing there the year after they opened.

    The next year I got asked if I could fix their groomers drive card, and we've had a working relationship for 20+ years.

    I look after the electronics, and associated repairs, etc and in turn the family skis.

     

    Works out great for both.

     

    e14 were kind enought to supply the camera and the RPi, so its a win-win for everyone.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    Mostly interested in the comms link to be honest the two modules I was on about  were

    http://uk.farnell.com/jsp/search/productdetail.jsp?SKU=1348829

    and

    http://uk.farnell.com/jsp/search/productdetail.jsp?SKU=1348837

     

    The Transiever module is probably more useful for you so this is it:

    http://uk.farnell.com/radiometrix/nim2-434-650-10/rf-mod-txrx-fm-434-65mhz-10kbps/dp/1348860

     

    don't know if they stock it in NZ but there are so many RF modules it's easy to miss them image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to Problemchild

    John

    I did see these, but was hoping there were some much cheaper alternatives.

     

    They are available here, but at eye-watering prices.

    1348829 is NZ$42

    1348837 is NZ$72

    1348860 is NZ$107

     

    Unfortunately you need one at each end, so its double those figures, plus antennas, pcb, and a means to mount.

     

    For long distance they are right, but for the relatively short distance (500m) in my application, the WiFi is the better choice.

     

    In my application I would need to have additional software processes, to transfer the file via serial through the 433MHz unit, and then save the file.

    Its possible, but streaming video would not be available (a possible option that could be 'on-demand').

     

    The WiFi I choose is at the upper end of the price range, but is proven in those conditions.

    I could have used a smaller cheaper USB style device with a directional antenna at the lodge end, but I considered the second unit location, and the beamwidth angle if we fitted any more.

     

    Do you have a particular need to use these as opposed to a WiFi.?

     

    Thanks also for the insulating board suggestion.

    With the three of the other projects coming to a close, its getting close to the top of the list, after I look at the case choices.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    I had the modules for some romote telemetry then possibly a ballon launch  for which they are just what you need.I think they would serve you well if you wanted to get the  link directly down the mountain not via a hut!

    Obviously if you have those facilities then you would be daft not to use them. You are right not to use the USB units as they are far from optimal at least the little ones but they may make nice units if placed in the focus of a dish or something like that

     

    Also if you have any problems see if you can  lock the units to amuch lower bit rate so the reliability increases I'm sure you really dont need much more than 1Mbit ?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    Oh BTW i'm down at Cambridge Raspberry Jam tomorrow and Ciseco are demoing their modules ...will be nice to see what they can do.

    I had a stand next door to them at the Derby MiniMaker Faire last year and their stuff was pritty good even then !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to Problemchild

    John

    if you wanted to get the  link directly down the mountain not via a hut!

    Quite right.

    I intend to limit the power output of the WiFi (they currently do 5km) to reduce the load on the battery, and I could look at lowering the data rate if required.

    There should be no 2.4Ghz interference up there, so we should have a pretty low noise floor.

     

    re Ciseco

    Any chance of grabbing some samples?

    They have some great looking products (My mouse button was twitching over the Add+ icon)

    Slice of Pi and Slice of Pi I/O

    RFu

    XRF

    are just a few and with very reasonable shipping.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 13 years ago in reply to Problemchild

    John

    if you wanted to get the  link directly down the mountain not via a hut!

    Quite right.

    I intend to limit the power output of the WiFi (they currently do 5km) to reduce the load on the battery, and I could look at lowering the data rate if required.

    There should be no 2.4Ghz interference up there, so we should have a pretty low noise floor.

     

    re Ciseco

    Any chance of grabbing some samples?

    They have some great looking products (My mouse button was twitching over the Add+ icon)

    Slice of Pi and Slice of Pi I/O

    RFu

    XRF

    are just a few and with very reasonable shipping.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    Just been down  at the Cambridge Jam, met some mates of mine from years ago ..... we  were the greyest kids in town .... mangaged to persuade one to part with £97 for a full set of stuff from Ciseco.

    bought the same for me so will maybe able to do a review now!