Personal Blogs
  • Community Hub
  • More
Personal Blogs
Joey Thompson's Blog Quick Project: Pi Security Cam
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: screamingtiger
  • Date Created: 30 Nov 2015 4:45 PM Date Created
  • Views 1274 views
  • Likes 1 like
  • Comments 5 comments
  • pi_security
Related
Recommended

Quick Project: Pi Security Cam

screamingtiger
screamingtiger
30 Nov 2015

Ill be using the Pi NOIR CameraPi NOIR Camera which is a Pi Cam without the IR filter.  In light conditions all the color is washed out, but it is able to see in the dark even without an IR source.

Ill also be using the Motion Tool to do the heavy work for me for recording, emailing, and detecting motion

 

Requirements:

  • Video only records when motion is detected.
  • Motion detection via video feed, not a PIR sensor.
  • Ability to see in low light conditions (not completely dark).
  • Ability to limit the video length per video (1 minute at a time).
  • Videos are emailed out immediately after being taken.
  • A "safe button" which is a button I can press to turn off motion detection, the motion will auto arm after 1 hour.
  • A process to mange video files, erasing them after 2 days.
  • *Nice to have: Video view from a web browser.
  • Portable, and easy to hide.  Will be disguised as a common object that would be in a room.

 

Hardware:

Raspberry Model B

Raspberry Pi Enclosure

Pi NOIR camera

Camera EnclosureCamera Enclosure

32 GB Class 10 SD Card

1A Power supply

WiPi wireless adapterWiPi wireless adapter

 

Software:

Motion Tool for recording, emailing and detecting motion

Python for video deleting scheduled with CROND

Black Coffee cup

 

I have a larger black coffee cup that should be able to enclose the entire setup.  Its porcelain so I can drill a hold for the camera to peer out of.  A coffee cup has a stable base and some weight to it.  It also will not look out of place in my house since I routinely leave cups laying around anyways.  I will also need a hole for the power supply wire to enter.

 

I will reply with my progress to this thread.  more to come with pictures!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago +2
    This will be an interesting build. There was a similar one done a few years ago "Catch Santa Challenge" http://www.element14.com/community/roadTests/1220 Pi Cam without the IR filter. ....... but it…
  • DAB
    DAB over 10 years ago +1
    Great idea, I will be following your progress with great interest. DAB
  • screamingtiger
    screamingtiger over 10 years ago +1
    I have completed this project, but not posted details yet for a good reason. I will update my blog and then come back here and update this blog. I ended up using a USB camera instead of the Pi Cam. Slower…
Parents
  • screamingtiger
    screamingtiger over 10 years ago

    Theres nothing original about this project, pretty easy actually.  Ben heck did something similar recently.  There are free apps that will make a cell phone do the same types of things.

     

    I just chose to use a raspberry pi since I have on hand and doing it this way gives me the most control over the functionality.  The free phone apps I tried leave the videos on the phone so if a lot is going on it could run out of space.  My script will delete old videos but also ensure that if space is running out I get notified.

     

    I found with the proper settings a 1 minute video is about 5mb so a 32gb card should provide enough buffer.

     

    Its also cool the motion software will allow real time viewing via a web browser.

     

    Im placing on order to Amazon shortly to get a bunch of gifts, so the parts I need are coming from Raspberry Pi via Amazon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • screamingtiger
    screamingtiger over 10 years ago

    Theres nothing original about this project, pretty easy actually.  Ben heck did something similar recently.  There are free apps that will make a cell phone do the same types of things.

     

    I just chose to use a raspberry pi since I have on hand and doing it this way gives me the most control over the functionality.  The free phone apps I tried leave the videos on the phone so if a lot is going on it could run out of space.  My script will delete old videos but also ensure that if space is running out I get notified.

     

    I found with the proper settings a 1 minute video is about 5mb so a 32gb card should provide enough buffer.

     

    Its also cool the motion software will allow real time viewing via a web browser.

     

    Im placing on order to Amazon shortly to get a bunch of gifts, so the parts I need are coming from Raspberry Pi via Amazon.