Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog AC Optocoupler LTV 814
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 22 Feb 2020 6:21 AM Date Created
  • Views 8714 views
  • Likes 12 likes
  • Comments 4 comments
  • ac_opto_coupler
  • ltv814
Related
Recommended

AC Optocoupler LTV 814

jw0752
jw0752
22 Feb 2020

When I used to repair dental chairs it was very common to find a logic circuit communicating with a line voltage triac through an opto-coupler. The chair's actuators were typically 115 Volt AC motors. These opto couplers had an internal LED tied to a light sensitive semiconductor junction that would, when illuminated, fire the triac and allow AC line power to flow to the motor. Until a couple days ago, however, I didn't realize that opto couplers existed that would allow AC line voltage as an input and output would be information to a logic circuit.

 

I was working on a circuit board for a Midmark Sterilizer when I came across the LTV 814 Opto Coupler.

 

image

 

This Opto coupler has two opposite polarity LEDs on the input and a photo transistor on the output.

 

The sterilizer has a door switch that is in a 115 volt AC circuit as well as an over temperature cut out switch that is also part of a 115 volt AC circuit. The open or closed status of both of these switches needed to be monitored by the sterilizer's logic circuits. In this case the designer's choice had been to use the LTV814 AC opto coupler to convey the status of these switches to the logic circuits.

 

I salvaged one of the opto couplers from a scrap board and decided to experiment with it a little bit. The LEDs on the input have a voltage drop across their junctions of about 2 volts. The sterilizer board was using a 120 K Ohm 1 Watt resistor in series with the input to limit the current to the LEDs. 115 volts RMS divided by 120 K Ohms leaves us with slightly less than one milliamp of current. I had to adapt the SMD LTV 814 to through the hole for my experiment and I mounted it on a small piece of proto board. Of course the AC current would vary with time and the 1 mA was just the effective average current.

 

Here is the experimental board:

 

image

 

In order to see the effect of the whether there was AC on the input of the opto coupler or not I put together this circuit:

 

image

 

I put the photo transistor of the opto coupler in series with a 10 K resistor and connected the common point to the input of a 74HC14 Hex Schmitt Trigger IC. The Red LED is on the output of this first Schmitt Trigger. I also connected the output of this first section to the input of a second Schmitt trigger. The Green LED is on the output of the second Schmitt trigger. Since the Schmitt triggers invert we should see that the Red LED is lit when the AC power is off and the Green LED should light when the AC power is applied to the Opto Coupler. The capacitor across the 7414 is a decoupling capacitor and the other capacitor is a 10 uF ceramic that is being used to take the 120 Hz pulse out of the input to the Schmitt trigger. Since our input to the optocoupler is AC, 120 times each second the voltage on the LEDs is zero volts and this turns off the Schmitt trigger. The 10 uF capacitor stores the voltage during these off times and keeps the Schmitt trigger active. Once the power is turned off the voltage on the capacitor quickly drops due to the circuit through the 10K resistor and the Schmitt trigger goes low on the input.

 

I made a short video of the experiment in action:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This was not a very complicated experiment but it will be useful to me to know that I can use the LTV 814s, which incidentally cost about 11 cents from Farnell, to safely monitor the status of line voltage circuits. If you have applications in your builds where you need to know the status of a switch or voltage in a line voltage circuit perhaps it can be of use to you too.

 

 

 

 

John

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 6 years ago +3
    Hi John, It's great you're highlighting the usefulness of these devices. I like those versions for DC too, in case if someone connects the power the wrong way around, it will still work : )
  • ralphjy
    ralphjy over 6 years ago +2
    Had not realized that there was an AC version of optocoupler, I've used the DC versions before but didn't think of using one of these to make the input polarity insensitive as Shabaz suggested. What surprised…
  • jw0752
    jw0752 over 6 years ago in reply to ralphjy +2
    Hi Ralph, I meant to include a schematic of the test circuit but it wasn't completed until just now. I like to include the schematics so that the real engineers on the forum can spot my errors and I get…
Parents
  • ralphjy
    ralphjy over 6 years ago

    Had not realized that there was an AC version of optocoupler, I've used the DC versions before but didn't think of using one of these to make the input polarity insensitive as Shabaz suggested.

     

    What surprised me was that it was not obvious from the data sheet that this was an AC input part other than in the package diagrams(the sheet that you included).

     

    Reminds me that I need to add a detector to sense when my laser power is on.  Probably don't need an optocoupler but it would be an inexpensive buffer.

     

    Thanks for sharing.  I'm sure that one day I'll have a need to sense presence of AC voltage.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 6 years ago

    Had not realized that there was an AC version of optocoupler, I've used the DC versions before but didn't think of using one of these to make the input polarity insensitive as Shabaz suggested.

     

    What surprised me was that it was not obvious from the data sheet that this was an AC input part other than in the package diagrams(the sheet that you included).

     

    Reminds me that I need to add a detector to sense when my laser power is on.  Probably don't need an optocoupler but it would be an inexpensive buffer.

     

    Thanks for sharing.  I'm sure that one day I'll have a need to sense presence of AC voltage.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 6 years ago in reply to ralphjy

    Hi Ralph,

     

    I meant to include a schematic of the test circuit but it wasn't completed until just now. I like to include the schematics so that the real engineers on the forum can spot my errors and I get to refine my techniques and designs. The fact that there is an AC opto coupler seems obvious in hind sight but when I first realized what it was it surprised me that I hadn't seen one before. If you happen to use it in your laser ON sensor add a post to this thread.

     

    John