Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Building the DSO Shell 15001K Oscilloscope
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 25 Apr 2017 6:02 AM Date Created
  • Views 5826 views
  • Likes 12 likes
  • Comments 31 comments
  • oscilloscope_kit
Related
Recommended

Building the DSO Shell 15001K Oscilloscope

jw0752
jw0752
25 Apr 2017

If you are looking for an inexpensive kit build project that comes together nicely and works well to boot check out the DSO Shell 15001K Oscilloscope Kit.

 

https://www.banggood.com/Orignal-JYE-Tech-DS0150-15001K-DSO-SHELL-DIY-Digital-Oscilloscope-Kit-With-Housing-p-1093865.html?rmmds=myorder

 

image

 

At $22.00 including shipping from China this is a no brainer. With a 200K bandwidth (Perhaps a bit of an exaggeration) it is undersized for many applications but still is a good tool for Audio and lower frequency servicing as well as a good educational tool for the experimenter or enthusiast. This model of the unit comes with all the SMD components installed. The through the hole components, switches and connectors are left for the kit builder. Here is what comes in the package:

 

image

 

Note that while you see a probe in some of my pictures this is not included in the kit, nor is the 9 volt power supply. I found that the small wall warts that I use for the Arduinos worked well. I also put a battery pack on the back of one unit so that I have a portable model. The manufacturer cautions that 10 volts is the high limit of the power supply and damage may result if the unit is powered with a higher voltage.

 

Here are what the circuit boards look like out of the box:

 

image

 

The kit comes with 4 pages of assembly instructions, calibration, and operation manual. While it is over all adequate it takes a lot of looking close and a thorough reading to get it right the first time. I have build three so far and I still can't quite get it right. It is not that the correct procedures aren't explained or illustrated somewhere on the pages it is just that it is not a totally smooth sail and I have a tendency to use my intuition too much. Fortunately a couple redos are permitted. The solder points are very small and a little challenging so this may not be a kit for a first time builder. Better to have some soldering experience first though it is doable if someone with experience is supervising a beginner.

 

image

 

The resistors supplied are very small and 5 banded. My 68 year old eyes had a challenge with them so I just metered them and put them where they belonged. If you happen to have some of my special tungsten carbide meter probe tips you can check 1/8 watt resistors one handed like this:

 

image

 

When the main board is fully populated they have you plug it in to check for proper operation. The instructions are a little out of sequence so it is necessary to populate the board and then go back to the first instruction on the list telling you to test it. At this point all one can do it see the screen and toggle the function buttons.

 

image

 

I found that the vias did not pull the solder in quite as easily as I would have liked so a good inspection of both sides of the board after soldering allowed me to dress up a couple questionable looking joints. The Analog board is the board where the bulk of the through the hole components must be installed. Over all the instructions were good and the components easy to identify. On the first two units that I built I mounted the adjust control backwards on its board. This does not harm anything but the unit will not work properly. If the instructions are read carefully they have a small box with a red print warning not to do it the way I did. Once this error was corrected both of the first two units worked properly. Here is the small board showing the side not to mount the control on.

 

image

 

The analog board comes with two sets of header pins so that during calibration the main board can be off set to allow access to the adjustments. While in this position one can check voltages and tune the input to display a clean square wave.

 

image

 

One feature that I was really pleased with is the ability to toggle on and off a list of measurements. Usually on a meter this size and cost one is left to guess what the digital data is. Here is what the unit looks like with the measurements displayed:

 

image

 

I put a battery pack on the back of one unit to make it more portable and purchased a set of $10.00  Oscilloscope probes for the units. The probes like the oscilloscopes came with free shipping but this time the Chinese had them shipped to me from the Seychelles. The ways of the electronics world are hard to believe. I am enjoying this era of free trade and exchange of products. I wonder how long before the politicians see what is going on and screw everything up. Any how if you like to build things this was a fun little project with very little financial risk involved. Here is a picture of the back of my unit with the battery pack and a picture of a completed unit.

 

image

 

image

 

Have Fun.

 

John

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 9 years ago +7
    Final Chapter: One of the points of having a small Oscilloscope like this one is to make it portable. I went looking for a suitable battery pack for its 8V to 10V power needs. I also wanted the pack to…
  • jw0752
    jw0752 over 9 years ago in reply to mcb1 +5
    Hi Mark, Here is the bandwidth analysis in pictures. The max Horizontal sweep speed of the small scope is 10 uS/Div. so I put both scopes on this setting and stepped the frequency from 10 kHz to 240 kHz…
  • jw0752
    jw0752 over 9 years ago in reply to balearicdynamics +4
    Hi Enrico, Here is a closeup of the processor and what I believe to be the data bus to the processor. Perhaps that will tell you more about how accessible the software is. John
  • DAB
    DAB over 9 years ago in reply to jw0752

    Good build John.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago

    Final Chapter:

     

    One of the points of having a small Oscilloscope like this one is to make it portable. I went looking for a suitable battery pack for its 8V to 10V power needs. I also wanted the pack to be based on an easily available battery such as the AA. Unfortunately the only 9 volt configurations available had an open configuration with the batteries exposed. While this was functional it did not serve my aesthetic sense. Finally I settled on this 12 volt AA battery pack with a built in DC adapter plug and a power switch.

     

    image

     

    At $3.50 and free shipping from China it was a no loose choice. 12 Volts, however, is too high for the Oscilloscope which has a 10 volt max limit to its power input. My first remedy to this problem was to build a small 9 volt linear DC regulator using a 7805 regulator and a 4 volt Zener. I also put a 9.5 volt Zener across the output to clamp any voltage above that level and protect the Oscilloscope. This worked very well except for the fact that the 7805 regulator was having to dump 25% of the battery power as heat. This meant that for every set of 8 batteries that I would be using two were going to be used to heat the box. Here is a schematic of the linear regulator circuit that I was using.:

     

    image

     

    At this point I remembered that I had a bunch of the Recom R78 series devices in stock. These are switching DC to DC convertors that are great substitutes for the linear 78XX series of regulators. They, unlike the linear versions, do not waste as much power as heat. With 90% + inefficiencies one of these would be a good replacement for my linear design. I chose to use the Recom R78C9.0-1.0 which is a 9 volt 1000 mA direct convertor so I would not have to use the Zener trick on the ground lead to boost its regulated output. I will give you a link to a similar device from the Newark site. ( a 500 mA version of the 1000 mA device I am using). Unfortunately Newark doesn't stock the 9 volt device so you will have to check one of the other suppliers if you want to buy one or two of them.

     

    http://www.newark.com/recom-power/r-78e9-0-0-5/dc-dc-converter-9v-0-5a/dp/84Y3692?ost=R-78E9.0-0.5&scope=partnumberlookahead&exaMfpn=true&anyFilterApplied=false&searchref=searchlookahead&searchView=table&iscrfnonsku=false&ddkey=http%3Aen-US%2FElement14_US%2Fw%2Fsearch

     

    Here is a picture of the Recom R78C9.0 alone and also one of the device installed in the battery pack:

     

    image

     

    image

     

    I had a concern that a small ripple from the switching circuit might affect the oscilloscope so I put a 22 uF tantalum across the output. This was probably an undue concern as my past experience has been the the ripple on the output of these devices has been irrelevant for my applications. The power wire from the battery case was shortened so that it neatly wrapped around to the DC socket of the Oscilloscope.

     

    image

     

    Since the power switch on the battery pack cuts power to the R78C9.0 as well as the Oscilloscope I put a recommendation on the battery pack to used its switch as the power switch and not the Oscilloscope Power switch. While the idle draw of the R78C9.0 is very small there is no sense wasting battery power. Here are a couple pictures of the completed battery pack modification.

     

    image

     

    image

     

    John

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to michaelkellett

    I was thinking more about where you could go with hacking the kit as it is, as a kind of design challenge, rather than how you'd improve the design.

     

    Replacing the processor with a better part on the same footprint is an interesting idea, though.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jc2048

    They do have a link for upgrading firmware

    http://www.jyetech.com/Products/LcdScope/DSO138_oscilloscope_upgrade.pdf

     

    Along with the schematic

    http://www.jyetech.com/Products/LcdScope/Schematic_Shell.pdf

     

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to jw0752

    I've never, ever used an ST ARM part, so I'm genuinely a non-expert in them. I have come across 'SWD' elsewhere (I think it's probably Single-Wire Debugging, or something like that - presumably it's an ARM standard rather than something specific to ST) which is how I recognised it.

     

    I like the aliasing with the 238kHz input (it's kind of beautiful and awful at the same time) but why is the beat frequency 10kHz, or so? That would put the sampling at 250k, rather than the max 1Msps they give, wouldn't it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>