Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Christmas Vacation Project - Building a Clap Switch Light
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 27 Dec 2017 5:36 AM Date Created
  • Views 5016 views
  • Likes 14 likes
  • Comments 24 comments
  • clap_switch
  • holidayspecialch
Related
Recommended

Christmas Vacation Project - Building a Clap Switch Light

jw0752
jw0752
27 Dec 2017

Thanks to Christmas Vacation I had the opportunity to spend the day doing electronics with my 11 year old Grandson Ivan. We began with a small Chinese noise actuated clap switch.

 

https://www.ebay.com/itm/VOS-Voice-Operated-Switch-DIY-Kit-Voice-Switch-Electronic-Production-Suite/222649153280?hash=item33d6ec7700:g:1cAAAOSwnDZT5G~0

 

image

 

As you can see the kit comes with no directions other than the silk screening on the board. I had explored this kit a while back and reverse engineered a schematic so Ivan had that as a guide as well.

 

image

 

It is a simple 2 stage audio amplifier that triggers a transistor flip flop which in turn lights a small LED. It is designed to operate at 5 volts. Ivan has become very adept at building these Chinese kits and he is also knowledgeable about my shop. With few exceptions I just turn him loose and let him work. Today at one point he got too much solder on the board so that two pads were bridged. I did not realize this until I saw that he had retrieved the solder wick from the drawer and was making the proper remedy to the problem. As he worked we discussed how we could take this simple, not so practical, circuit and make something useful out of it. The idea came up that he would like a light by his bed so that when he got up at night he could just clap and have light.  I began to check for resources in the shop and found a small 2 watt 12 volt LED panel, a 12 volt linear wall wart, a project box of the right size, a nice prototyping board, and a power switch. Since we would be building the kit to integrate with the rest of the components I told Ivan to leave the microphone and power jack off the board. We would mount them to the project box when we assembled the whole unit.

 

I made a simple drawing of the support circuitry we would need to run the 12 volt LED panel and the 5 volt kit. Due to the design of the kit it would also be necessary to invert the output of the kit so that we would sync the LED panel with the small red LED on the kit board that was being driven directly from the flip flop. Since my hand drawing doesn't scan very well I have made a quick schematic.

 

image

 

As Ivan continued to work on the kit, he was decoding the color codes of the resistor at this point, I started to bread board the support circuit just to make sure it would work and also to give Ivan the layout so he could directly transfer it onto the prototype board. I love the Adafruit prototyping boards that have the same layout as a bread board and this makes simple work of transferring a layout.

 

image

 

Here was the bread board layout which seemed to work using the sample Clap Switch circuit I had built a couple weeks earlier.

 

image

 

After Ivan finished with the kit board he began to work on the support board. I helped by placing components and he soldered them in place. Since we were approaching 4 hours interrupted only by lunch I asked him if he was getting tired of electronics and he said no. I want this to be fun for him and not a job so I try to be conscious of his interest level. He stays so focused and interested I frankly forget that he is only eleven. I apologize that I did not get better pictures of the final assembly. Due to the difficulty of holding wires in place I would be the one to hold them and he continued to solder them. Here is a picture of the boards in the completed project box as well as a picture of the unit finished.

 

image

 

We had mounted the LED array and the Microphone on top of the box and the main switch was on the back where the wire from the 12 volt wall wart entered.

 

image

 

Here is a short video of Ivan demonstrating the Clap Switch Light for you.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The actual bench time for building this small project today was over 5 hours. Ivan's focus and enthusiasm made every minute a joy.

 

Happy Grandpa

John

 

 

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago in reply to genebren +5
    Still, not quite at the stage were she is interested in electronics, but here is my granddaughter holding a Pez dispenser (Snoppy) and a pair of philips screwdrivers. She kept looking for screws to turn…
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +4
    Hi Jon, The reason we didn't implement this excellent idea is that Old Grandpa thinks too linearly. This is exactly what I love about this forum and sharing with you guys. I will go back to the circuit…
  • ntewinkel
    ntewinkel over 8 years ago +4
    What a great project! And the customization makes it that much better with an even greater sense of accomplishment at the end. You can tell Ivan is really proud of the result! -Nico
Parents
  • shabaz
    shabaz over 8 years ago

    Hi John & Ivan,

     

    Excellent project and demonstration!! It works really well!

    Regarding the holding wires thing, I too have that problem, sometimes I'll use blu-tack (temporary putty) to hold things in place while I solder. It softens slightly admittedly when the heat reaches it, so I still have to be quick to complete the join, but it seems to hold for long enough.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 8 years ago in reply to shabaz

    Holding stuff in place while it gets attached or soldered is a universal problem. I have at least 5 vices on my workbench plus 2 multi-clip third hands plus about 5 pucks that I hold things down with, plus I have a couple of small visegrips. The alligator clip third hands often need paper in the jaws to prevent damage to the object being held and I put duct tape in the jaws of the steel vices. 2 of the vices have full ball joints for arbitrary positioning and rubber jaws. Still trying to come up with better ways to hold and feed solder....

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to dougw

    dougw  wrote:

     

    Holding stuff in place while it gets attached or soldered is a universal problem...

    smd image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 8 years ago in reply to Jan Cumps

    My SMD methods are all manual - many tweezers and a useless suction placer. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 8 years ago in reply to Jan Cumps

    My SMD methods are all manual - many tweezers and a useless suction placer. image