Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Christmas Vacation Project - Building a Clap Switch Light
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 27 Dec 2017 5:36 AM Date Created
  • Views 5010 views
  • Likes 14 likes
  • Comments 24 comments
  • clap_switch
  • holidayspecialch
Related
Recommended

Christmas Vacation Project - Building a Clap Switch Light

jw0752
jw0752
27 Dec 2017

Thanks to Christmas Vacation I had the opportunity to spend the day doing electronics with my 11 year old Grandson Ivan. We began with a small Chinese noise actuated clap switch.

 

https://www.ebay.com/itm/VOS-Voice-Operated-Switch-DIY-Kit-Voice-Switch-Electronic-Production-Suite/222649153280?hash=item33d6ec7700:g:1cAAAOSwnDZT5G~0

 

image

 

As you can see the kit comes with no directions other than the silk screening on the board. I had explored this kit a while back and reverse engineered a schematic so Ivan had that as a guide as well.

 

image

 

It is a simple 2 stage audio amplifier that triggers a transistor flip flop which in turn lights a small LED. It is designed to operate at 5 volts. Ivan has become very adept at building these Chinese kits and he is also knowledgeable about my shop. With few exceptions I just turn him loose and let him work. Today at one point he got too much solder on the board so that two pads were bridged. I did not realize this until I saw that he had retrieved the solder wick from the drawer and was making the proper remedy to the problem. As he worked we discussed how we could take this simple, not so practical, circuit and make something useful out of it. The idea came up that he would like a light by his bed so that when he got up at night he could just clap and have light.  I began to check for resources in the shop and found a small 2 watt 12 volt LED panel, a 12 volt linear wall wart, a project box of the right size, a nice prototyping board, and a power switch. Since we would be building the kit to integrate with the rest of the components I told Ivan to leave the microphone and power jack off the board. We would mount them to the project box when we assembled the whole unit.

 

I made a simple drawing of the support circuitry we would need to run the 12 volt LED panel and the 5 volt kit. Due to the design of the kit it would also be necessary to invert the output of the kit so that we would sync the LED panel with the small red LED on the kit board that was being driven directly from the flip flop. Since my hand drawing doesn't scan very well I have made a quick schematic.

 

image

 

As Ivan continued to work on the kit, he was decoding the color codes of the resistor at this point, I started to bread board the support circuit just to make sure it would work and also to give Ivan the layout so he could directly transfer it onto the prototype board. I love the Adafruit prototyping boards that have the same layout as a bread board and this makes simple work of transferring a layout.

 

image

 

Here was the bread board layout which seemed to work using the sample Clap Switch circuit I had built a couple weeks earlier.

 

image

 

After Ivan finished with the kit board he began to work on the support board. I helped by placing components and he soldered them in place. Since we were approaching 4 hours interrupted only by lunch I asked him if he was getting tired of electronics and he said no. I want this to be fun for him and not a job so I try to be conscious of his interest level. He stays so focused and interested I frankly forget that he is only eleven. I apologize that I did not get better pictures of the final assembly. Due to the difficulty of holding wires in place I would be the one to hold them and he continued to solder them. Here is a picture of the boards in the completed project box as well as a picture of the unit finished.

 

image

 

We had mounted the LED array and the Microphone on top of the box and the main switch was on the back where the wire from the 12 volt wall wart entered.

 

image

 

Here is a short video of Ivan demonstrating the Clap Switch Light for you.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The actual bench time for building this small project today was over 5 hours. Ivan's focus and enthusiasm made every minute a joy.

 

Happy Grandpa

John

 

 

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago in reply to genebren +5
    Still, not quite at the stage were she is interested in electronics, but here is my granddaughter holding a Pez dispenser (Snoppy) and a pair of philips screwdrivers. She kept looking for screws to turn…
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +4
    Hi Jon, The reason we didn't implement this excellent idea is that Old Grandpa thinks too linearly. This is exactly what I love about this forum and sharing with you guys. I will go back to the circuit…
  • ntewinkel
    ntewinkel over 8 years ago +4
    What a great project! And the customization makes it that much better with an even greater sense of accomplishment at the end. You can tell Ivan is really proud of the result! -Nico
Parents
  • jc2048
    jc2048 over 8 years ago

    "It is a simple 2 stage audio amplifier ..."

     

    Except that it isn't. I'd have said the same at a quick glance, because it does look like the kind of circuit shape an amplifier would have, but in reality the first two transistors are a monostable with a very fine trigger. The first transistor is biased so that it normally conducts and it holds off the second transistor. A signal from the microphone starts to turn it off, the second transistor turns on and the collector voltage falling is coupled to the input by the 1uF cap, massively reinforcing the original trigger.

     

    Then it's a matter of waiting until the 1uF capacitor charges to the point where the first transistor will turn on again, returning the second transistor to its normally off state.

     

    Try looking at the collector of Q2 with a scope and you'll see what it does each time you clap. The collector goes low for longer than the clap lasts (that avoids multiple triggering of the output bistable). The output bistable is toggled by the negative going edge of that collector waveform, which you'll see if you compare the two.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 8 years ago

    "It is a simple 2 stage audio amplifier ..."

     

    Except that it isn't. I'd have said the same at a quick glance, because it does look like the kind of circuit shape an amplifier would have, but in reality the first two transistors are a monostable with a very fine trigger. The first transistor is biased so that it normally conducts and it holds off the second transistor. A signal from the microphone starts to turn it off, the second transistor turns on and the collector voltage falling is coupled to the input by the 1uF cap, massively reinforcing the original trigger.

     

    Then it's a matter of waiting until the 1uF capacitor charges to the point where the first transistor will turn on again, returning the second transistor to its normally off state.

     

    Try looking at the collector of Q2 with a scope and you'll see what it does each time you clap. The collector goes low for longer than the clap lasts (that avoids multiple triggering of the output bistable). The output bistable is toggled by the negative going edge of that collector waveform, which you'll see if you compare the two.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 8 years ago in reply to jc2048

    Hi Jon,

    Thank you very much for your in depth analysis of my schematic. You are correct, of course, the R-13 was missplaced. After looking at these little circuits and trying to turn them back into schematics I sometimes go cross-eyed. Here is a corrected schematic. I did not redraw the bistable but I agree it would have been much better represented in a conventional configuration. The next time I see this arrangement on a board I will try to be more conventional. Here is the revised schematic and hopefully there aren't any more mistakes.

     

    image

     

    I have copied your comments and added them to the sparse literature I have been able to gather and generate on this circuit so that I am better prepared to use it in the future. Thanks again for taking the time to really look at my presentation and catching the mistakes and incorrect description of the front end of the circuit.

     

    John and Ivan

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to jc2048

    Hi Jon,

     

    Here is the waveform of the collector of Q2 as it triggers the bi-stable. It is exactly as you described with a pulse duration of 400 ms. Thanks for your insights and guidance. Next time Ivan is over I have some explaining to do. He already knows that you guys explain things to me just like I try to explain things to him. Everyone is a teacher and everyone is a student.

     

    John

     

    image

    • Cancel
    • Vote Up +4 Vote Down