Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog DC Load Unit "La Carga" Episode I
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 2 Aug 2015 12:25 AM Date Created
  • Views 1629 views
  • Likes 4 likes
  • Comments 13 comments
  • test_equipment
  • dc_load
Related
Recommended

DC Load Unit "La Carga" Episode I

jw0752
jw0752
2 Aug 2015

In January of this year, inspired by some of Robert Peter Oakes 's excellent tutorials I decided to begin to design and construct a DC load. I have been learning and improving my electronics ever since joining E-14 about two years ago. Those of you who are familiar with me know that I tend to be a little retro and basic in my approach to problems and projects. This DC Load unit which I have dubbed " La Carga " (named chosen by 4ringfan) will be no exception. Up until now I have always been satisfied to grab what I called a "LOAD BULB" every time I wanted to load a circuit.

 

image

 

 

While these have served my needs in simple experiments the progress of the last couple years has put me in a position where I want a little more precision and control of the load in my experiments.

 

As I mentioned I began in January to draw rough schematics and plans for the DC Load unit. Thanks to the inspiration offered by my friend D_Hersey I have put some effort into learning the basics of SPICE IV. For the first time in my life I am able to run simulations of many of my prototype circuits prior to bread boarding them. I also am planning so that the power supply and other circuitry is more appropriately sized to the job they are intended to do. When one is not very good at electronics there is a tendency to over build. This is why over the years many of my creations are "TANKS" when they should have been sports cars. As you will see I did not completely escape this tendency but I hopefully have made some improvements.

 

The plan is to use that same style enclosure that I used when I built my power supply in September of 2014.

 

      imageimage

 

This Case and Chasis was from a 40 year old piece of Dental Equipment called a Cavitron. Above you can see the before and after pictures of the power supply. If you have an interest in that build here is a link to the blog post:  http://www.element14.com/community/people/jw0752/blog/2014/09/21/a-new-power-supply-for-john

 

Circuit Over View:

 

My plan is to build a DC Load that will cover the voltage range of 3 Volts to 35 Volts and be capable of 6 amps with a max wattage of 210 Watts. I want to have the unit sense the voltage and add or remove series current limiting resistors so that my control device, a salvaged IGBT, (Isolated Gate Bipolar Transistor) will never have to dissipate more than about 40 watts itself. I have decided to use digital LCD meters on this build so the unit will not be quite so retro, though no one will argue that I am completely out of the retro mode by any means. Something else that is new for me is that I have been inspired by waelect and I am going to blog about this build as I am doing it. Up until now I have wanted to have a finished functional unit before putting my neck out. This will give everyone better insights into some of the mistakes and wrong paths that I take while building. I do reserve the right to not talk about the really dumb mistakes.

 

In Episode II , a couple days from now, I will publish my schematics for the build and show pictures of some of the major components.

 

John

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 11 years ago +2
    Here's an app note from IR - you are wondering into unknown territory using the IGBT as a linear device but it may work - which part do you have ? www.irf.com/technical-info/appnotes/an-983.pdf MK
  • jw0752
    jw0752 over 11 years ago in reply to michaelkellett +2
    Hi Michael, After reviewing the application notes and data sheet I did some bench experiments and of course you were correct. The IGBT was not the best choice for this application. I have a MOSFET IRFPC60LC…
  • shabaz
    shabaz over 11 years ago in reply to jw0752 +2
    I know little about IGBT devices too : ( Common adoption of them did not occur at the time I was studying, and it seems more popular now. I'll have to study and experiment with them sometime!
Parents
  • michaelkellett
    michaelkellett over 11 years ago

    Here's an app note from IR - you are wondering into unknown territory using the IGBT as a linear device but it may work - which part do you have ?

     

     

     

    www.irf.com/technical-info/appnotes/an-983.pdf

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to michaelkellett

    Hi Michael,

    After reviewing the application notes and data sheet I did some bench experiments and of course you were correct. The IGBT was not the best choice for this application. I have a MOSFET IRFPC60LC which seems to be a much better choice. In the voltage range of my application the IGBT had a Vce of 1.35V and it basically stopped working when Vcc dropped below 6 volts. The IRFPC60LC had a Vds of 0.48 volts in the same voltage range and did not start to drop out until Vss was below 3.5V. The upside is that my mistake has given me an opportunity, thanks to you, to learn more about the IGBT. Your watchful presence is always appreciated.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to jw0752

    I know little about IGBT devices too : ( Common adoption of them did not occur at the time I was studying, and it seems more popular now. I'll have to study and experiment with them sometime!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 11 years ago in reply to jw0752

    I know little about IGBT devices too : ( Common adoption of them did not occur at the time I was studying, and it seems more popular now. I'll have to study and experiment with them sometime!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 11 years ago in reply to shabaz

    Hi Shabaz,

    Check out the great App Note that MK posted as it has some great information on IGBTs and how they relate to MOSFETS.

     

    http://www.irf.com/technical-info/appnotes/an-983.pdf

     

    John