Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Dental Electrosurgery Unit - A Peek Inside
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 7 Jun 2016 6:25 AM Date Created
  • Views 1395 views
  • Likes 6 likes
  • Comments 4 comments
  • electro_surgery_unit
Related
Recommended

Dental Electrosurgery Unit - A Peek Inside

jw0752
jw0752
7 Jun 2016

image

 

Tonight an older Dental Electro-surgery Unit was sent to me for repair. The dentist uses an Electro-Surgery unit like a scalpel to remove growths from inside the mouth and also to cauterize areas of tissue. The hand piece has a chuck and will accommodate different size and shape ends to suit different types of lesions. When I was more active in the dental repair business I would keep a piece of meat in the refrigerator so that I could test the repaired units by cutting out small pieces of meat and cauterizing patterns on the face of the steak.

 

If you would like more details on how the process works here is a link that explains Electro-Surgery in more detail:

 

https://en.wikipedia.org/wiki/Electrosurgery

 

The Electrosurgery unit works by providing a high frequency, in this case about 2.8 MHz, current that is used to cut and coagulate as needed in minor surgeries. This particular unit is a Cameron Miller Model 26-230 and was manufactured a few years ago. I know that it was a few years ago as the circuit uses Vacuum Tube technology and the company address on the unit lacks a ZIP code. I wanted to share the design and construction of it with you as it is a good example of a nice simple design that was built to last.

 

Here is a picture of the insides:

 

image

 

The vacuum tube is a 6GJ5 Beam Power Tube that was more typically used in the Horizontal Deflection Amplifier circuit of 1950s and 1960s area TV Sets. For those of you accustomed to working on transistor based technology the big difference between transistor technology and tube technology is the 1000 Volts on the red wire going to the plate of the tube. In this case the plate connection is the silver button on the top of the tube. The circuit is just an oscillator whose output is coupled to the CUT (Black) output on the front panel through the variable capacitor. The more the capacitance is increased the more current that is available for cutting. The Coagulate ( Red) output is linked to the Cut Output with a 0.001 1000VDC capacitor. This serves to reduce and limit the current of the Coagulate terminal which is used for procedures where cutting is not needed.

 

image

 

The power supply is a transformer with a 6 volt secondary that is used for the filament of the 6GJ5 tube and a 750 Volt secondary that goes to a full wave bridge rectifier. The bridge diodes are actually silicon types of similar appearance to 1N4007s. The designer of the circuit did not bother to filter the DC output of the bridge leaving it to pulse at 120 Hz. The effect of this is to create an output the has 2.8 MHz pulses with a frequency of 120 Hz.

 

image

 

Here is another view inside the unit. The Green Output terminal in the left foreground is marked PATIENT. Yes they have a ground wire that goes out to the patient. It is terminated with an insulated plate 12 cm X 9 cm that is placed under the patient's leg or bottom, outside the clothing. This plate makes a capacitive coupling to the patient and works very well at 2.8 MHz. Here is a picture of the Plate and cable.

 

image

 

You may at this point be asking yourself, "He said it came in for repair so what was wrong with it?" Well, there was nothing wrong with the unit. In 30 years I have never had to fix a single one of these units and I have never had to replace a tube in one of them. The only things I have ever had to work on are the cords that go to the cutting handpiece and the Patient plate. In this case the cord to the handpiece had broken wires where the cord entered the back of the handpiece. I replaced the cord on the handpiece and installed a new banana plug on the end and everything was good as new.

 

John

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago +2
    Interesting device. I had no idea such devices existed. There is a computer museum here and I got the chance to take some photos over the weekend, I liked this one of valves/tubes:
  • jw0752
    jw0752 over 10 years ago in reply to shabaz +2
    Hi Shabaz, When I was 19 I had a collection of over 1000 new and used Vacuum tubes (Valves). Unfortunately my places to live in the ensuing years have not always accommodated my collections. Somewhere…
  • DAB
    DAB over 10 years ago +1
    Nice post John. Those of us who have worked with high power RF well know the capability for this device to burn off human flesh with a small electrode. RF burns were like a badge of honor when working…
Parents
  • DAB
    DAB over 10 years ago

    Nice post John.

     

    Those of us who have worked with high power RF well know the capability for this device to burn off human flesh with a small electrode.

     

    RF burns were like a badge of honor when working with some of these devices.

     

    The US Navy did a study and found that 50% off all unit failures were due to connector or cabling issues.

    I think your experience with this device proves the point that users should always check their cables and connections before assuming that the device has failed.

     

    It is sort of like the Windows reboot sequence.  Whenever Windows failed to work correctly, a system reboot solved about 90% of the problems.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to DAB

    Hi DAB,

    I wish I had your depth of experience and insight. II always appreciate your comments.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago in reply to DAB

    Hi DAB,

    I wish I had your depth of experience and insight. II always appreciate your comments.

    John