Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Dental Sterilizer Power Supply Board Repair
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 3 Dec 2015 6:38 AM Date Created
  • Views 963 views
  • Likes 5 likes
  • Comments 7 comments
  • service_techniques
  • circuit_board_repair
Related
Recommended

Dental Sterilizer Power Supply Board Repair

jw0752
jw0752
3 Dec 2015

Tonight I have been involved in the diagnosis and repair of a Hybrid Switching/Linear power supply board from a Pelton Crane Validator Plus dental instrument sterilizer. Due to a design flaw in this model sterilizer this is not the first time I have seen this problem. The board is positioned in the sterilizer directly under the water reservoir. If the person filling the water reservoir is careless water drips down onto the board. There is some protection afforded the board by an aluminum plate but experience has shown this protection to be ineffective over time. Here is a picture of the failed power supply board:


image


As an overview I will tell you that the 115 VAC attaches to the board on the 2 pin connector in the lower right. The power conversion then progresses in a clockwise direction around the board until the output exits the board on the three white 4 pin angle headers on the right edge. When working properly the board produces +5 volts, +12 volts, and -12 volts with a common ground. This is an OEM board and no information or specifications are provided. It is considered unrepairable by the manufacturer who really wants to sell very expensive replacement boards instead of repairing the ones that fail.


I begin my repair with a very thorough inspection of the board, both top and bottom. During this inspection I am logging anything suspicious that may be part of the problem. This includes any burns to the components or the board, any cracks or hazing to the solder joints, and any signs of previous repair. I will usually do this with a jewelry loupe and a small analog meter with which I can make quick checks on diodes, transistors, and resistors. At the same time as the inspection I am attempting to understand the design of the board and how it might work. There is always a lot of guess work involved in this as I am not an engineer but slowly over the years I have gotten a little better at it. As I mentioned this board has been subjected to water falling on it occasionally over a long period of time. This was evidenced by crystal deposits on the end of the board where the 3 white angle headers are. Here are a couple pictures of the damaged area:


     imageimage


The good news was that the water damage was restricted to the low voltage output end of the board. The solder side of the board was in pristine condition with no signs of water damage. Visual inspection showed that a couple jumper buss wires had been badly corroded and one was open completely. Water had apparently capillaried under two decoupling capacitors in the damage area and they would have to be removed for inspection. This board was able to continue working, probably for years, despite the occasional water contamination because the water was isolated to the low voltage area. If you mix low voltage with water and metal you will get an effect that slowly destroys and eats away the electrode that is at a more positive potential. The small additional current load produced by the resistance in the water and this reaction were never enough to cause a failure. It wasn't until a buss wire became totally broken that the board failed. I began the repair process by removing all components and headers in the water damage area.  The headers were cleaned and showed no permanent damage. The positive leads on both of the capacitors were each eaten away and the capacitors would have to be replaced. I was able to find an exact replacement for the 47 uF 50 volt cap but the 1200 uF 16 volt had to be replaced with another value. My options were 1000 uF or 2200 uF. I chose the 2200 uF at 16 volt as I felt it would allow me to err on the side of caution.  Here is what the board looked like with the components removed:


image



image


One can clearly see the damage to the buss jumpers and incidentally the green color on the component side of the board is a clear indication of the electrolysis of copper from the wires. The board was cleaned with a wire brush and some solvents. New buss wire was then installed along with the replacement components. With everything installed and looking like new it is time to test the board. To this point I had applied no power to the board so all my work might be in vain if something is wrong with the switching circuitry. I hooked the board up so that my little bread board meters were on the +5 volt and +12 volt outputs. I put an automotive tail light bulb with 500 mA draw at 12 volts across  the -12 volt output. The board was then connected to my variac isolated AC supply and the voltage slowly brought up to 115 VAC. Here is what the test setup looked like:


image


Sorry my shutter was too fast for the LED displays to look good. The power supply board was allowed to run for about an hour. Since I had no specs on the output of the board it was not practical to load up the outputs as I did not want to take the chance of overloading them and damaging the board needlessly. The board was labeled as having been repaired and will be returned to be used in the next Validator Plus sterilizer that comes into the shop with this same problem.


John

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 10 years ago in reply to pettitda +3
    Hi David, My variac is part of a power supply that I built 40 years ago and it has become an integral part of my lab. Variacs are of course inherently dangerous as there is no isolation from the mains…
  • mcb1
    mcb1 over 10 years ago +1
    Brilliant writeup John. It does show how experience, knowledge and careful observation can determine the likely causes, and make a repair. I struggled with convincing some co-workers the importance of…
Parents
  • pettitda
    pettitda over 10 years ago

    Nice write-up John!  I've heard a lot of differing opinions on the use of a variac to power up a board that's been out of use for a while.  In your case, why did you choose to use a variac?  I've not personally used a variac, however I have several old radios that I intend to restore at some point.  So, I may need to invest in one. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to pettitda

    Hi David,

     

    image

     

    My variac is part of a power supply that I built 40 years ago and it has become an integral part of my lab. Variacs are of course inherently dangerous as there is no isolation from the mains. If they have been wired by inexperienced people it is easy to get a live main connection on the common of the variac. Many years ago I was a beneficiary of a good jolt of mains juice from a variac so I have a lot of respect for it. I have my variac connected to the mains through a 1:1 isolation transformer that removes some of the danger. That being said, I find the variac very useful for a number of activities in my lab. For one I use it to spec out unknown transformers. I can start at low voltages and slowly increase the primary voltage all the while monitoring the secondary. Another useful application is to spec out MOVs and other transient supression devices. I can never find any specs or listings to identify these devices so the MOV is put in series with a resistor and the voltage is increased until I get a stable voltage reading across the MOV. If the MOV is in excess of the 150 volt output of the variac I will use a step up transformer to give me the range that I need. In response to your direct question I like to use the variac to slowly apply a voltage to questionable power supply boards. By monitoring the current I can see a short or other problem before I have reached a smoke and burn situation. This gives me a chance to go back and try to further troubleshoot the problem. The variac is a great tool for the shop but I would not use one without the isolation transformer to drive it.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago in reply to pettitda

    Hi David,

     

    image

     

    My variac is part of a power supply that I built 40 years ago and it has become an integral part of my lab. Variacs are of course inherently dangerous as there is no isolation from the mains. If they have been wired by inexperienced people it is easy to get a live main connection on the common of the variac. Many years ago I was a beneficiary of a good jolt of mains juice from a variac so I have a lot of respect for it. I have my variac connected to the mains through a 1:1 isolation transformer that removes some of the danger. That being said, I find the variac very useful for a number of activities in my lab. For one I use it to spec out unknown transformers. I can start at low voltages and slowly increase the primary voltage all the while monitoring the secondary. Another useful application is to spec out MOVs and other transient supression devices. I can never find any specs or listings to identify these devices so the MOV is put in series with a resistor and the voltage is increased until I get a stable voltage reading across the MOV. If the MOV is in excess of the 150 volt output of the variac I will use a step up transformer to give me the range that I need. In response to your direct question I like to use the variac to slowly apply a voltage to questionable power supply boards. By monitoring the current I can see a short or other problem before I have reached a smoke and burn situation. This gives me a chance to go back and try to further troubleshoot the problem. The variac is a great tool for the shop but I would not use one without the isolation transformer to drive it.

    John

    • Cancel
    • Vote Up +3 Vote Down